2.0.0
ST Edge AI Core - Command-line Interface


ST Edge AI Core

ST Edge AI Core - Command-line Interface


ST Edge AI Core Technology 2.0.0



r8.0

Overview

The 'stedgeai' application is a console utility. It provides a complete and unified Command Line Interface (CLI) for compiling a pretrained deep learning (DL) or machine learning (ML) model into an optimized library. This library can run on an ST device/target enabling edge AI on microcontrollers (MCUs) with or without ST Neural ART NPU, microprocessors (MPUs), and smart sensors. It consists of three main commands: analyze, validate and generate. Each command can be used independently of the other with the same set of common options (model files, compression factor, output directory…) and specific options. The supported-ops command lists the supported operators and associated constraints for a given deep learning framework.

Supported ST device/target

target description
stm32[xx] The STM32 family of 32-bit microcontrollers based on the Arm Cortex®-M processor. 'stm32xx' is requested to define a specific stm32 series (see the “Supported STM32 series” section) else 'stm32h7' is used.
stellar-e Series of MCUs tailored for the specific requirements of electrified vehicles, ensuring efficient actuation of power conversion and e-drive train applications
stellar-pg Series of MCUs (P and G families), based on the same backbone architecture, tailored for/to their application domains to offer optimized and rational solutions to meet the needs for the next generation of vehicles. 'Stellar P', designed to meet the demands of integrating the next generation of drivetrains, electrification solutions and domain-oriented systems, delivers a new level of real-time performance, safety, and determinism. 'Stellar G', addressing the key challenges of next-generation body integration and zone-oriented vehicle architectures, ensures performance, safety, and power efficiency combined with wide connectivity and high security.
ispu A new generation of MEMS sensors featuring an embedded intelligent sensor processing unit (ISPU)
mlc MEMS sensors embedding the machine learning core (MLC)
stm32mp The STM32 family of general-purpose 32-bit microprocessors (MPUs) provides developers with greater design flexibility. They are based on single or dual Arm Cortex®-A cores, combined with a Cortex®-M core. 'stm32mpxx' is requested to define a specific stm32mpu series (see the “Supported STM32MPU series” section)

Synopsis

usage: stedgeai --model FILE --target stm32|stellar-e|stellar-pg|ispu|mlc [--type keras|onnx|tflite] [--name STR]
                [--compression none|lossless|low|medium|high] [--allocate-inputs] [--allocate-outputs] [--no-inputs-allocation]
                [--no-outputs-allocation] [--input-memory-alignment INT] [--output-memory-alignment INT] [--workspace DIR] [--output DIR]
                [--split-weights] [--optimization OBJ] [--memory-pool FILE] [--no-onnx-optimizer] [--input-data-type float32|int8|uint8]
                [--output-data-type float32|int8|uint8] [--inputs-ch-position {chfirst,chlast}] [--outputs-ch-position {chfirst,chlast}]
                [--prefetch-compressed-weights] [--custom FILE] [--c-api st-ai|legacy] [--allocate-activations] [--allocate-states]
                [--st-neural-art [ST_NEURAL_ART]] [--quantize [FILE]] [--binary] [--dll] [--ihex] [--address ADDR] [--copy-weights-at ADDR]
                [--relocatable] [--lib DIR] [--no-c-files] [--entropy ENTROPY] [--batch-size INT] [--mode MODE] [--desc DESC]
                [--valinput FILE [FILE ...]] [--valoutput FILE [FILE ...]] [--range RANGE [RANGE ...]] [--full] [--io-only] [--save-csv]
                [--classifier] [--no-check] [--no-exec-model] [--seed SEED] [--ucf FILE] [--with-report] [--no-report] [--no-workspace] [-h]
                [--version] [--tools-version] [--verbosity [{0,1,2,3}]] [--quiet]
                analyze|generate|validate|supported-ops

A short description of the options can be displayed with the following command:

$ stedgeai --help
...

To know the versions of the main Python modules which are used:

$ stedgeai --tools-version
stedgeai - ST Edge AI Core v2.0.0
- Python version   : 3.9.12
- Numpy version    : 1.23.5
- TF version       : 2.15.1
- TF Keras version : 2.15.0
- ONNX version     : 1.15.0
- ONNX RT version  : 1.18.1

Options for a given target

The 'target' option can be specified to know the options which are available for a given target.

$ stedgeai --target mlc --help
usage: stedgeai [--target STR] [--output DIR] --device DEVICE [--script FILE]
                [--json FILE] [--type {arff,ucf}] [--port COM] [--ucf FILE]
                [--logs FILE | DIR] [--ignore-zero] [--tree FILE] [--arff FILE]
                [--meta FILE] [--no-report] [--help] [--version] [--tools-version]
                [--verbosity [{0,1}]]
                generate|validate|analyze

ST Edge AI Core v1.0.0 (MLC 1.0.0)
...

Command workflow

For each command, the same preliminary steps are applied. A report (txt file) is systematically created and fully or partially displayed. Additional JSON files (dictionary based) are generated in the workspace directory to be parsed by the external tools/script to retrieve the results. Note that they can also be used by a nonregression environment. The format of these files is out of the scope of this document.

<workspace-directory-path>\<name>_c_info.json
<output-directory-path>\<name>_<cmd_name>_report.txt
  • 'analyze' workflow
    • import the model
    • map, render, and optimize internally the model
    • log and display a report
  • 'validate' workflow
    • import the model
    • map, render, and optimize internally the model
    • execute the generated C-model (on the desktop or on the board)
    • execute the original model using the original deep learning runtime framework for x86
    • evaluate the metrics
    • log and display a report
  • 'generate' workflow
    • import the model
    • map, render, and optimize internally the model
    • export the specialized C-files
    • log and display a report

Enable AutoML pipeline for resource-constrained environment

The CLI can be integrated into an automatic or manual pipeline. It allows to design a deployable, and effective neural network architecture for a resource-constrained environment (that is, with low memory/computational resources and/or critical power consumption budgets). The main loop can be extended with a post-analyzing/validating step of the pretrained models. The candidates are checked according to the end-user target constraints thanks to the respective analyze and validate commands.

  • Checking of the budgeted memory (ROM/RAM) can be done in the inner loop (topology selection/definition) before the time-consuming training process (or retraining process) to preconstraint the choices of the neural network architecture according to the memory budgets.
  • Note that the “analyze” and “host validate” step can be merged, “analyze” information are also available in the “validate” reports.

Error handling

During the execution of a given command, after the parsing of the arguments if an error is raised, the stedgeai application returns -1 (else 0 is returned).

A category and a short description prefix an error message.

category description
CLI ERROR specific CLI error
LOAD ERROR error during the load/import of the model or the connection with the board - OSError, IOError
NOT IMPLEMENTED expected feature is not implemented - NotImplementedError
INTERRUPT indicates that the execution of the command has been interrupted (CTRL-C or kill system signal) - KeyboardInterrupt, SystemExit
TOOLS ERROR, INTERNAL ERROR internal error - ImportError, RuntimeError, ValueError

Note

There is a specific attention to have explicit and relevant short description of the error messages. Unfortunately, this is not always the case, do not hesitate to contact the local support or to use the product ST Community channel/forum, “Edge AI”.

Example of specific error

$ stedgeai validate model.tflite --target ispu -t keras
...
E102(CliArgumentError): Wrong model files for 'keras'

Analyze command

Description

The 'analyze' command is the primary command to import, parse, and check an uploaded pretrained model. A detailed report provides the main metrics to know if the generated code can be deployed on the targeted device. It also includes the rendering information by layer or/and operator (see “C-graph description” section). It provides the size of the requested RT memory size to store the kernel and specific network binary objects. After completion, the user can be fully confident in the imported model in term of supported layers/operators.

Examples

  • Analyze a model

    $ stedgeai analyze -m <model_file_path> --target <target>
  • Analyze Keras model saved in two separated files: model.json + model.hdf5

    $ stedgeai analyze -m <model_file_path>.json -m <model_file_path>.hdf5 --target <target>
  • Analyze a 32b float model with compression request

    $ stedgeai analyze -m <model_file_path> -c low --target <target>
  • Analyze a model with the input tensors placed in the activations buffer

    $ stedgeai analyze -m <model_file_path> --allocate-inputs --target <target>

Common options

This section describes the common options for the analyze, validate, and generate commands. The specific options are described in the respective command section.

-m/--model FILE

Path of the model files (see “Deep Learning (DL) framework detection” section). Note that the same -m argument should be also used to indicate the weights file if necessary - Mandatory

Details

Deep Learning (DL) framework detection

Extensions of the model files are used to identify the DL framework which should be used to import the model. If the autodetection is ambiguous, the '--type/-t' option should be used to define the correct framework.

DL framework type (–type/-t) file extension
Keras keras .h5 or .hdf5 and .json
TensorFlow lite tflite .tflite
ONNX onnx .onnx

--target STR

Set the targeted device - Mandatory

-t/--type STR

Indicate the type of the original DL framework when the extension of the model files does not allow inference (see “DL framework detection” section) - Optional

-w/--workspace DIR

Indicate a working/temporary directory for the intermediate/temporary files (default:"./st_ai_ws/" directory) - Optional

-o/--output DIR

Indicate the output directory for the generated C-files and report files (default:"./st_ai_output/"directory) - Optional

-n/--name STR

Indicate the C-name (C-string type) for the imported model. This name id used to prefix the name of specialized NN C-files and the API functions. It is also used for the temporary files, allowing you to use the same workspace/output directories for different models (default: "network"). - Optional

-c/--compression STR

  • supported target: stm32xx, stellar-e, stellar-pg
  • unsupported target: stm32n6 with NPU, mlc, ìspu, stm32mp

Indicate the expected compression level applied on the different operators. Supported values: none|lossless|low|medium|high (Default: lossless) to apply the same level for all operators, or a simple json file to define a compression level by operator. - Optional

Details

During the optimization passes of the imported model, different compression level can be applied. Underlying applied compression algorithms depend on the selected level and the configuration of the operator/layer itself.

level description
none no compression
lossless applied algorithms ensuring the accuracy (structural compression)
low applied algorithms trying to reduce the size of the parameters with a minimum of accuracy loss
medium more aggressive algorithms, the final accuracy loss can be more important
high extreme aggressive algorithms (not used)

Supported compressions by operator

  • Floating-point dense or fully connected layers: 'low/medium/high' enables the compression of weights or/and bias. With 'low', a targeted compression factor of '4' is applied while with 'medium\high' the targeted compression factor is‘8’`.

  • ONNX-ML TreeEnsembleClassifier operator: With 'none' level, no compression or optimization is applied. 'lossless' enables a first level of compression w/o loss of accuracy. 'low','medium','high' enable compression weights.

Warning

Only float32 (or float) are supported by the code generator, this implies that during the import of the operator, the float64 (or double) values are converted in float32.

Specify a compression level by operator

By default, the compression process tries to apply globally the same compression level for all eligible operators. If the global accuracy is too much impacted or to force the compression, the user has the possibility to refine the expected compression level layer-by-layer.

A JSON file must be defined to indicate what is the compression level which must be applied for a given layer. The original name specifies the name of the layer.

{
    "layers": {
        "dense_2": {"factor": "high"},
    }
}

The option -c/--compression can be used to pass the configuration file.

$ stedgeai analyze -m <model_file> --target stm32 -c <conf_file>.json

Note

Be aware that a specific layer could not be compressed if the gain of weight size is not enough.

--no-inputs-allocation

If defined, this flag indicates that no space is reserved in the “activations” buffer to store the input buffers. The application should allocate them separately in the user memory space and provide them to the execution engine before performing the inference. Refer to “IO buffers into activations buffer” section. - Optional

--no-outputs-allocation

If defined, this flag indicates that no space is reserved in the “activations” buffer to store the output buffers. The application should allocate them separately in the user memory space and provide them to the execution engine before performing the inference. Refer to “I/O buffers into activations buffer” section. - Optional

--input-memory-alignment INT

If defined, set the memory-alignment constraint in bytes (multiple of 2) to allocate the input buffer inside the “activations” buffer. By default 4 (or 8 bytes dependent of system bus-width) are used. Refer to the “I/O buffers into activations buffer” section. - Optional

--output-memory-alignment INT

If defined, set the memory-alignment constraint in bytes (multiple of 2) to allocate the output buffer inside the “activations” buffer. By default 4 (or 8 bytes dependent of system bus-width) are used. Refer to “I/O buffers into activations buffer” section. - Optional

--allocate-inputs

DEPRECATED (enabled by default) - If defined, this flag indicates that a space is reserved in the “activations” buffer to store the input buffers. Otherwise, they should be allocated separately in the user memory space. Depending on the size of the input data, the “activations” buffer may be bigger but overall less than the sum of the activation buffer plus the input buffer. To retrieve the address of the associated input buffers refer to the “I/O buffers into activations buffer” section. - Optional

--allocate-outputs

DEPRECATED (enabled by default) - If defined, this flag indicates that a space is reserved in the “activations” buffer to store the output buffers. Otherwise, they should be allocated separately in the user memory space. (Refer to “I/O buffers into activations buffer” section). - Optional

--memory-pool FILE

Indicate the file path of the memory pool descriptor file. It allows to describe the memory regions allowing to support the multiheap use-case.- Optional

Details

Description of the Memory pools

For advanced use-cases, the user has the possibility to pass (through the '--memory-pool' option), a text file (JSON file format) allowing to specify some properties of the targeted device. The “1.0” JSON version allows only to provide the descriptions of the memory pools.

{
    "version": "1.0",
    "memory": {
        "mempools": [
            {
                "name": "sram",
                "size": "128KB",
                "usable_size": "96KB"
            }
        ]
    }
}
key description
"version" version/format of the JSON file. Only "1.0" value is supported - mandatory
"memory" key to describe the memory properties (dict) - optional
"mempools" key to describe the memory pool (list of dict) - optional

Memory pool description ("mempools" item)

key description
"name" user name, if not defined a generic name is generated: pool_{pos} - optional
"size" indicate the total size - mandatory
"usable_size" indicate the maximum size which can be used - if not defined, size is used - optional
"address" indicate the base @ of memory pool (ex. 0x2000000) - optional
  • value is defined as a string, "B,KB,MB" can be used to indicate the size. "0x" prefix indicates value in hexadecimal.
  • no target device database is embedded in the CLI to check that the provided memory pool descriptors are valid.
  • Note that if "address" attribute is defined and if the associated memory pool is used, the value is used as-is to define the default address of the activations buffer by the generated code (see generated <network>_data.c file).

A typical example of JSON file indicates that two budgeted memory pools can be used to place the activations buffer. "dtcm" memory pool is privileged to place the critical buffers.

{
    "version": "1.0",
    "memory": {
        "mempools": [
            {
                "name": "dtcm",
                "size": "128KB",
                "usable_size": "64KB"
            },
            {
                "name": "ram_d1",
                "size": "512KB",
                "usable_size": "256KB"
            },
            {
                "name": "default"
            }
        ]
    }
}

--split-weights

If defined, this flag indicates that one c-array is generated per weights/bias data tensor instead to have a unique C-array (“weights” buffer) for the whole model (default: disabled), (refer to “Split weights buffer” section) - Optional

-O/--optimization STR

Indicate the objective of the applied optimization passes - Optional

Details

Optimization objectives

The '-O/--optimization' option is used to indicate the objective of the optimization passes which are applied to deploy the c-model. Note that the accuracy/precision of the generated model is not impacted. By default (w/o option), a trade-off (that is, balanced) is considered.

objective description
time apply the optimization passes to reduce the inference time (or latency). In this case, the size of the used RAM (activations buffer) can be impacted.
ram apply the optimization passes to reduce the RAM used for the activations. In this case, the inference time can be impacted.
balanced trade-off between the 'time' and the 'ram' objectives. Reduces RAM usage yet minimizing impact on inference time

The following figure illustrates the usage of the optimization option. It is based on the 'Nucleo-H743ZI@480MHz' board with the small MLPerf Tiny quantized models from https://github.com/mlcommons/tiny/tree/master/benchmark/training.

--c-api STR

Select the generated embedded c-api: 'legacy' or 'st-ai'. 'legacy' is the c-api supported by default on target STM32 and Stellar (refer to “Embedded Inference Client API” and “Embedded Inference Client ST Edge AI API” articles for details) - Optional

--allocate-activations

(Experimental) Supported only with the st-ai c-api, this option indicates that the runtime space must allocate the memory buffers to store the activations. Otherwise, the application must provide them (default behavior) - Optional

--allocate-states

(Experimental) Supported only with the st-ai c-api, this option indicates that the runtime space must allocate the memory buffers to store the states. Otherwise, the application must provide them (default behavior) - Optional

--input-data-type

For the quantized models, indicates the expected inputs data type of generated implementation. Multiple inputs definition is supported: in_data_type_1,in_data_type_2,… If one data type is given, it will be applied for all inputs (possible values: float32|int8|uint8) - Optional

Details
model type supported options
Keras (float) int8 and uint8 data type are not supported. float32 can be used but the original data type is unchanged.
ONNX (float) int8 and uint8 data type are not supported. float32 can be used but the original data type is unchanged.
TFlite (float) int8 and uint8 data type are not supported. float32 can be used but the original data type is unchanged.
TFlite (quantized) int8, uint8 and float32 are supported. According the original data types a converter is inserted.
ONNX (quantized)* int8, uint8 and float32 are supported. According the original data types a converter is inserted.

(*) by default for this type of model, the original I/O data type (float32) is converted to int8 data type to feed directly the int8 kernels allowing to support efficiently the deployed ONNX QDQ models (see “QDQ format deployment” section).

--output-data-type

For the quantized models, indicates the expected outputs data type of generated implementation. Multiple outputs definition is supported: out_data_type_1,out_data_type_2,… If one data type is given, it is applied for all outputs (possible values: float32|int8|uint8) - Optional

--cut-input-tensors

A single tensor or a list of tensor by which to cut the input model

--cut-output-tensors

A single tensor or a list of tensor by which to cut the output model

--cut-input-layers

A single layer or a list of layer by which to cut the input model

--cut-output-layers

A single layer or a list of layer by which to cut the output model

--inputs-ch-position

Indicate the expected NCHW (channel first) or NHWC (channel last) data layout for the inputs (refer to “How to change the I/O data type or layout (NHWC vs NCHW)” article for more details). Note that this option is applied for all inputs if multiple inputs - possible values: chfirst|chlast - Optional

--outputs-ch-position

Indicate the expected NCHW (channel first) or NHWC (channel last) data layout for the outputs (refer to “How to change the I/O data type or layout (NHWC vs NCHW)” article for more details). Note that this option is applied for all outputs if multiple outputs - possible values: chfirst|chlast - Optional

--no-onnx-optimizer

Disable the ONNX optimizer pass before to import the ONNX model - Optional

-q/--quantize FILE

Path of the configuration file (JSON file) to define the tensor format configuration.

--st-neural-art STR

supported target: stm32n6 with ST Neural-ART NPU

Set the selected profile (including the ST Neural-ART compiler options, refer to “ST Neural ART compiler primer” article) from a well-defined configuration file.

--custom FILE

Path of the configuration file (JSON file) to support the custom layers (refer to “Keras Lambda/custom layer support” article) - Optional

-v/--verbosity {0,1,2,3}

Set the level of verbosity (or level of displayed information). Supported values: 0,1,2 (default:1) - Optional

--quiet

Disable the display of the progress bar during the execution of the command - Optional

Out-of-the-box information

The first part of the log shows the used arguments and the main metrics of the C implementation.

$ stedgeai analyze -m ds_cnn.h5 --target stm32
..
 Exec/report summary (analyze)
 -------------------------------------------------------------------------------------------
 model file         :   <model-path>\ds_cnn.h5
 type               :   keras
 c_name             :   network
 compression        :   lossless
 optimization       :   balanced
 target/series      :   stm32h7
 workspace dir      :   <workspace-directory-path>
 output dir         :   <output-directory-path>
 model_fmt          :   float
 model_name         :   ds_cnn
 model_hash         :   0xb773f449281f9d970d5b982fb57db61f
 params #           :   40,140 items (156.80 KiB)
 -------------------------------------------------------------------------------------------
 input 1/1          :   'input_0', f32(1x49x10x1), 1.91 KBytes, user
 output 1/1         :   'dense_1', f32(1x12), 48 Bytes, user
 macc               :   4,833,792
 weights (ro)       :   158,768 B (155.05 KiB) (1 segment) / -1,792(-1.1%) vs float model
 activations (rw)   :   55,552 B (54.25 KiB) (1 segment)
 ram (total)        :   57,560 B (56.21 KiB) = 55,552 + 1,960 + 48
 -------------------------------------------------------------------------------------------
...

The initial subsection recalls the CLI arguments. Note that the full raw command line is saved at the beginning of the generated report file: <output-directory-path>\network_<cmd>_report.txt

field description
model file reports the full-path of the original model files (-m/--model). If multiple files, there is one line by file.
type reports the -t/--type value or inferred DL framework type
c_name reports the expected C-name for the generated C-model (-n/--name)
compression reports the applied compression level (-c/--compression)
optimization reports the selected objective: balanced (default), ram or time, (-O/--optimization)
target/series reports the selected target/series (--target)
workspace dir full-path of the workspace directory (-w/--workspace)
output dir full-path of the output directory (-o/--output)

The second part shows the results of the importing and rendering stages.

field description
model_fmt designates the main format of the generated model: float, ss/sa, dqnn,..
model_name designates the name of the provided model. This is generally the name of the model file.
model_hash provides the computed MD5 signature of the imported model files.
input indicates the name, the format, the shape, and the size in bytes of an input tensor. There is one line by input. 'inputs (total)' field indicates the total size (in bytes) of the inputs.
output indicates the name, the format, the shape, and the size of the output tensor. There is one line by output. outputs (total) field indicates the total size (in bytes) of the outputs.
params # indicates the total number of parameters of the original model and its associated size in bytes.
macc indicates the whole computational complexity of the original model. Value is defined in MACC operations: Multiply ACCumulated operations, refer to “Computational complexity: MACC and cycles/MACC”
weights (ro) indicates the requested size (in bytes) for the generated constant RO parameters (weights and bias tensors). The size is 4 bytes aligned. If the value is different from the original model files, the ratio is also reported. (refer to “Memory-related metrics” section)
activations (rw) indicates the requested size (in bytes) for the working RW memory buffer (also called activations buffer). It is mainly used as an internal heap for the activations and temporary results. (refer to “Memory-related metrics” section)
ram (total) indicates the requested total size (in bytes) for the RAM including the input and output buffers.

Note that when the --memory-pool is passed, the next part 'Memory-pools summary' summarizes the usage of the memory pools.

  Memory-pools summary (activations/ domain)
  --------------------------- ---- -------------------------- ---------
  name                        id   used                       buffer#
  --------------------------- ---- -------------------------- ---------
  sram                        0    54.25 KiB (10.8%)          34
  weights_array               1    155.05 KiB (15876800.0%)   35
  input_0_output_array_pool   2    1.91 KiB (196000.0%)       1
  dense_1_output_array_pool   3    48 B (4800.0%)             1
  --------------------------- ---- -------------------------- ---------

IR graph description

The outlined “graph” section (table form) provides a summary of the topology of the network which is considered before the optimization, render, and generation stages. The 'id' column indicates the index of the operator from the original graph. It is generated by the importer. The described graph is an internal platform-independent representation (or IR) created during the import of the model. Only training operators are ignored. Note that if no input operator is defined, an “input” layer is added and the nonlinearity functions are unfused.

field description
id indicates the layer/operator index in the original model.
layer (type) designates the name and type of the operator. The name is inferred from the original name. In the case where a nonlinearity function is unfused, the new IR-node is created with the original name suffixed with '_nl' (see next figure with the first layer)
shape indicates the output shape of the layer. Follow the “HWC” layout or channel last representation (refer to “I/O tensor” section)
param/size indicates the number of parameters and their sizes in bytes (4 bytes aligned)
macc designates the complexity in multiply-accumulated operations, refer to “Computational complexity: MACC and cycles/MACC”
connected to designates the name of the incoming operators/layers

The right side of the table ('c_*' columns) reports generated C-object after optimization and rendering stages.

field description
c_size indicates the difference in bytes of the size for the implemented weights/params tensors. If nothing is indicated, the size is unchanged compared to the original size ('-/size' field)
c_macc indicates the difference in MACC. If nothing is displayed, the final complexity of the C-operator is comparable to the complexity of the original layer/operator ('macc' field).
c_type indicates the type of the c-operator. The value between square is the index in the c-graph. The value between parenthesis is the data type: '()' indicates a float32 type, '(i)' for integer type, '(c4, c8)' for the compressed floating-point layer (size includes also the associated dictionary). Multiple c-operators can be generated for an original operator.

Footer summarizes the differences for the whole model including the requested RAM size for the activations buffer and for the I/O tensors.

model/c-model: macc=369,672/369,688 +16(+0.0%) weights=18,288/18,288
           activations=--/6,032 io=--/2,111

In the case where the optimizer engine has folded or/and fused the IR nodes, the 'c_type' is empty.

The following figure is an example of an IR graph with a residual neural network. As for the multiple branches, no specific information is added, 'connected to' column allows to know the connections.

Warning

For a compressed or quantized model, the MACC values (by layer or globally) are unchanged since the number of operations is always the same. Only the associated number of CPU cycles by MACC is changed. In particular, for the quantized models.

Number of operations per c-layer

Number of operations by generated C-layer ('c_id') according to the type of data is provided. With the synthesis by types of operations for the entire model, this information makes it possible to know the partitioning of the operations in relation with the types of data.

 Number of operations per c-layer
 ----------------------------------------------------------------------------------------------
 c_id    m_id   name (type)                                     #op (type)
 ----------------------------------------------------------------------------------------------
 0       1      quant_conv2d_conv2d (conv2d_dqnn)                       230,416 (smul_s8_s8)
 1       3      quant_conv2d_1_conv2d (conv2d_dqnn)                   1,843,200 (sxor_s1_s1)
 ...
 14      25     quant_depthwise_conv2d_3_conv2d (conv2d_dqnn)            28,800 (sxor_s1_s1)
 ...
 16      28     quant_conv2d_7_conv2d (conv2d_dqnn)                   1,638,400 (sxor_s1_s1)
 17      30     activation (nl)                                           6,400 (op_f32_f32)
 18      32     conv2d_conv2d (conv2d)                                   76,812 (smul_f32_f32)
 ----------------------------------------------------------------------------------------------
 total                                                               10,067,228

   Number of operation types
   ---------------------------------------------
   smul_s8_s8               230,416        2.3%
   sxor_s1_s1             9,740,800       96.8%
   op_s1_s1                  12,800        0.1%
   op_f32_f32                 6,400        0.1%
   smul_f32_f32              76,812        0.8%
operation description
smul_f32_f32 floating-point macc-type operation
smul_s8_s8 8-bit signed integer macc-type operation
op_f32_f32 Floating point operation (nonlinearity, elemtwise op…)
conv_s8_f32 converter operation; s8 -> f32
xor_s1_s1 binary operation (~macc)

Complexity report per layer

The last part of the report summarizes the relative network complexity in term of MACC and associated ROM size by layer. Note that only the operators which contribute to the global 'c_macc' and 'c_rom' metrics are reported. 'c_id' indicates the index of the associated c-node.

 Complexity report per layer - macc=18,752,688 weights=7,552 act=3,097,600 ram_io=602,184
 ---------------------------------------------------------------------------------------------------
 id   name                             c_macc                    c_rom                     c_id
 ---------------------------------------------------------------------------------------------------
 1    separable_conv1                  ||                 1.8%   ||                 1.6%   [0]
 1    separable_conv1_conv2d           |||                3.2%   ||||               3.4%   [1]
 2    depthwise_conv2d_1               |||||||||         10.3%   ||||||||           8.5%   [2]
 3    conv2d_1                         ||||||||||||||||  17.6%   ||||||||||||||    14.4%   [3]
 5    dw_conv_branch1                  ||||||||           9.3%   ||||||||           8.5%   [7]
 6    pw_branch1                       ||||||||||||||||  17.6%   ||||||||||||||    14.4%   [8]
 7    dw_conv_branch0                  ||||||||           9.3%   ||||||||           8.5%   [6]
 8    batch_normalization_1            ||                 2.1%   ||                 1.7%   [9]
 9    separable_conv1_branch2          ||||||||           9.3%   ||||||||           8.5%   [4]
 9    separable_conv1_branch2_conv2d   |||||||||||||||   16.5%   ||||||||||||||    14.4%   [5]
 10   add_1                            ||                 2.1%   |                  0.0%   [10, 11]
 11   global_average_pooling2d_1       |                  1.0%   |                  0.0%   [12]
 12   dense_1                          |                  0.0%   ||||||||||||||||  16.2%   [13]
 12   dense_1_nl                       |                  0.0%   |                  0.0%   [14]

C-graph description

Additional “Generated C-graph summary” section is included in the report (also displayed with '-v 2' argument). It summarizes the main computational and associated elements (c-objects) used by the C-inference engine (runtime library). It is based on the c-structures generated inside the '<name>.c' file. A complete graphic representation is available through the UI (refer to [UM]).

The first part recalls the main structural elements: c-name, number of c-nodes, number of C-array for the data storage of the associated tensors. Input and output name of the I/O tensors.

Generated C-graph summary
---------------------------------------------------------------------------------------------------
model name         : microspeech_01
c-name             : network
c-node #           : 5
c-array #          : 11
activations size   : 4352
weights size       : 16688
macc               : 336084
inputs             : ['Reshape_1_output_array']
outputs            : ['nl_2_fmt_output_array']

As illustrated in the following figure, the implemented c-graph (legacy API) can be considered as a sequential graph, managed as a simple linked list. Fixed-executing order is defined by the C-code optimizer according to two main criteria: data-path dependencies (or tensor dependencies) and the minimization of the RAM memory peak usage.

Each computational c-node is entirely defined by:

C-Arrays table

'C-Arrays' table lists the objects allowing to handle the base address, size, and metadata of the data memory segments for the different tensors. For each item, number of items, size in byte ('item/size'), memory segment location ('mem-pool'), type ('c-type') and short format description ('fmt') are reported.

C-Arrays (11)
---------------------------------------------------------------------------------------------------
c_id  name (*_array)      item/size           mem-pool     c-type         fmt         comment 
---------------------------------------------------------------------------------------------------
0     conv2d_0_scratch0   352/352             activations  uint8_t        ua8          
1     dense_1_bias        4/16                weights      const int32_t  ss32                   
2     dense_1_weights     16000/16000         weights      const uint8_t  ua8                  
3     conv2d_0_bias       8/32                weights      const int32_t  ss32                  
4     conv2d_0_weights    640/640             weights      const uint8_t  ua8                 
5     Reshape_1_output    1960/1960           user         uint8_t        ua8         /input     
6     conv2d_0_output     4000/4000           activations  uint8_t        ua8                 
7     dense_1_output      4/4                 activations  uint8_t        ua8                 
8     dense_1_fmt_output  4/16                activations  float          float                    
9     nl_2_output         4/16                activations  float          float                  
10    nl_2_fmt_output     4/4                 user         uint8_t        ua8         /output    
---------------------------------------------------------------------------------------------------
mem_pool description
activations part of the activations buffer
weights part of a ROM segment
user part of a memory segment owned by the user (client application level)
fmt format description
float 32b float numbers
s1/packed binary format
bool boolean format
c4/c8 compressed 32b float numbers. The size includes the dictionary.
s, u, ua, ss, sa integer or/and quantized format (refer to [“Quantized models support”]]STAI_CORE_QUANT article). '/ch(n)' indicates that per-channel scheme is used (else per-tensor).

C-Layers table

'C-Layers' table lists the c-nodes. For each node, the c-name (name), type, macc, rom and associated tensors (with the shape for the I/O tensors) are reported. Associated c-array can be found with its name (or array id).

C-Layers (5)
---------------------------------------------------------------------------------------------------
c_id  name (*_layer)  id  type    macc        rom         tensors                shape (array id) 
---------------------------------------------------------------------------------------------------
0     conv2d_0        0   conv2d  320008      672         I: Reshape_1_output    [1, 49, 40, 1] (5)
                                                          S: conv2d_0_scratch0                     
                                                          W: conv2d_0_weights                      
                                                          W: conv2d_0_bias                         
                                                          O: conv2d_0_output     [1, 25, 20, 8] (6)
---------------------------------------------------------------------------------------------------
1     dense_1         1   dense   16000       16016       I: conv2d_0_output0    [1, 1, 1, 4000] (6)
                                                          W: dense_1_weights                      
                                                          W: dense_1_bias                      
                                                          O: dense_1_output      [1, 1, 1, 4] (7) 
---------------------------------------------------------------------------------------------------
2     dense_1_fmt     1   nl      8           0           I: dense_1_output      [1, 1, 1, 4] (7) 
                                                          O: dense_1_fmt_output  [1, 1, 1, 4] (8) 
---------------------------------------------------------------------------------------------------
3     nl_2            2   nl      60          0           I: dense_1_fmt_output  [1, 1, 1, 4] (8) 
                                                          O: nl_2_output         [1, 1, 1, 4] (9) 
---------------------------------------------------------------------------------------------------
4     nl_2_fmt        2   nl      8           0           I: nl_2_output         [1, 1, 1, 4] (9)
                                                          O: nl_2_fmt_output     [1, 1, 1, 4] (10)
---------------------------------------------------------------------------------------------------
  • 'id' designates the layer/operator index from the original model allowing to retrieve the link with the implemented node ('c_id').

The following figure illustrates a quantized model where the softmax operator is implemented in float requesting to insert two converters. Note that this is just an example, the softmax operator is fully supported in int8.

Runtime memory size

“Runtime” identifies all involved kernel objects (software components) which are requested to execute the deployed c-model on a given device (also called runtime AI-stack). To compute these information, the '--target' option is used to know the targeted device and an embedded gcc-based compiler application should be available in the PATH.

The first part indicates the final contribution by module (generated c-file or library) and by type of memory segment. 'RT total' line sum-ups the different contributors. 'lib (toolchain)' indicates the contribution of the used toolchain objects (including typically the low-level floating point operations from the libm/libgcc libraries). The extra lines weights/activations/io recalls the requested size for respectively the weights, the activations buffer and the payload for the input/output tensors (refer to “memory-related metrics” section from “Evaluation report and metrics” article).

segment description
text size in bytes for the code
rodata size in bytes for the const data (usually stored in nonvolatile memory device, FLASH type, except for ISPU)
data size in bytes for the initialized data (stored in volatile memory device like embedded RAM, initial values is stored in FLASH, except for ISPU)
bss size in bytes for the zero-initialized data (stored in RAM)
$ stedgeai analyze -m <model_path> --target stm32h7 --c-api legacy
...
 Requested memory size by section - "stm32h7" target
 ----------------------------- -------- -------- ------- --------
 module                            text   rodata    data      bss
 ----------------------------- -------- -------- ------- --------
 NetworkRuntime910_CM7_GCC.a     19,100        0       0        0
 network.o                          482      213   1,520      116
 network_data.o                      48       16      88        0
 lib (toolchain)*                   104        0       0        0
 ----------------------------- -------- -------- ------- --------
 RT total**                      19,734      229   1,608      116
 ----------------------------- -------- -------- ------- --------
 weights                              0   16,688       0        0
 activations                          0        0       0   12,004
 io                                   0        0       0    1,964
 ----------------------------- -------- -------- ------- --------
 TOTAL                           19,734   16,917   1,608   14,084
 ----------------------------- -------- -------- ------- --------
 *  toolchain objects (libm/libgcc*)
 ** RT AI runtime objects (kernels+infrastructure)
module description
NetworkRuntime910_CM7_GCC.a kernel objects implementing the requested operators
network.o specialized code/data to manage the c-model
network_data.o specialized code/data to manage the weight/activation buffers

Note that the '<network>_params_data.o' file does not appear in the table, because it contains only the values of the weights (c-array form) which is represented by the '*weights*’ extra line.

The last part summarizes the whole requested memory size per type of memory. It also illustrates the breakdown between the RT objects and the main dimensioning memory-related metrics of the deployed c-model (that is, ROM/RAM metrics).

  Summary - "stm32h7" target
  ---------------------------------------------------
               FLASH (ro)      %*   RAM (rw)       %
  ---------------------------------------------------
  RT total         21,571   56.4%      1,724   11.0%
  ---------------------------------------------------
  TOTAL            38,259             15,692
  ---------------------------------------------------
  *  rt/total

ISPU example

The following log illustrates an example for the 'ispu' target. In the final summary, as the firmware is loaded in the internal RAM through a serial interface by a host processor, the requested size to store the initialized value of the .data section is not considered.

$ stedgeai analyze -m <model_path> --target ispu --c-api stai
...
 Requested memory size by section - "ispu" target
 ------------------- -------- -------- ------ --------
 module                  text   rodata   data      bss
 ------------------- -------- -------- ------ --------
 network_runtime.a     10,970        0      4        0
 network.o              1,968       80      0        0
 lib (toolchain)*       1,844      428      0        0
 ------------------- -------- -------- ------ --------
 RT total**            14,782      508      4        0
 ------------------- -------- -------- ------ --------
 weights                    0   16,688      0        0
 activations                0        0      0   12,004
 states                     0        0      0        0
 io                         0        0      0    1,964
 ------------------- -------- -------- ------ --------
 TOTAL                 14,782   17,196      4   13,968
 ------------------- -------- -------- ------ --------
 *  toolchain objects (libm/libgcc*)
 ** RT AI runtime objects (kernels+infrastructure)

  Summary - "ispu" target
  ----------------------------------------------------------
               Code RAM (ro)      %*   Data RAM (rw)      %
  ----------------------------------------------------------
  RT total            15,290   47.8%               4   0.0%
  ----------------------------------------------------------
  TOTAL               31,978                  13,972
  ----------------------------------------------------------
  *  rt/total

Validate command

Description

The 'validate' command allows validating the generated/deployed model. Two modes (--mode option) are considered: host and target. The detailed descriptions of the used metrics are described in the “Evaluation report and metrics” article.

Validation on host

Option: '--mode host' (Default)

The specialized NN generated c-files are compiled on the host and linked with a specific network-runtime library implementing the reference C-kernels closed to the target implementation.

Validation on target

Option: '--mode target -d <desc>'

This mode allows validating the deployed model on the associated board. Before to execute the 'validate' command, the board should be flashed with a specific validation firmware including a specific COM stack and the deployed C-model. For each target the way to deploy the model on the associate development board can be specific.

When the board is flashed and started, the same validation process is applied, only the execution of the deployed c-model is delegated to the target.

Examples

  • Minimal command to validate a 32b float model with the self-generated random input data (“Validation on desktop”).

    $ stedgeai validate -m <model_f32p_file_path> --target stm32
  • To report the “L2r error” and relative execution time by layer (“Validation on desktop”).

    $ stedgeai validate -m <model_f32p_file_path> --full --target stm32
  • Minimal command to validate a 32b float model on STM32 target. Note that a complete profiling report including execution time by layer is generated by default.

    $ stedgeai validate -m <model_f32p_file_path> --mode target --target stm32
  • Validation of a 32b float model with compression factor (“Validation on desktop”)

    $ stedgeai validate -m <model_f32p_file_path> -c medium --target stm32
  • Validate a model with a custom dataset

    $ stedgeai validate -m <model_file_path> -vi test_data.csv --target stm32
  • Validate a model with only 20 randomly selected samples from a large custom dataset

Specific options

--mode

Indicates the mode of validation - Optional

mode description
'host' default value - Performs a validation on the host.
'target' Perform a validation on target.
'host-io-only' alias equivalent to ‘–mode host –io-only’ - deprecated - default behavior
'target-io-only' alias equivalent to ‘–mode target –io-only’

-vi/--valinput

Indicates the custom test dataset which must be used. If not defined an internal self-generated random dataset is used (refer to “Input validation files” section) - Optional

-vo/--valoutput

Indicates the expected custom output values. If the data are already provided in a simple file ('*.npz') through the '-vi' option this argument is skipped - Optional

-b/--batches

Indicates how many random data samples is generated (default: '10') or how many custom test data are used (default: all) - Optional

-d/--desc

Describes the protocol and associated parameters to communicate with the deployed c-model. Syntax: '<driver>[:parameters]'. This option is required if the --mode target is specified.

Describes the COM port which is used to communicate with a target board (see “Serial COM port configuration” section) - Optional

--full

supported target: stm32xx, stellar-e, stellar-pg

Apply an extended validation process to report the L2r error layer-by-layer (Only supported for the floating-point Keras model, experimental for the other models). Else only the L2r is evaluated on the last or output layers. - Optional

--io-only

Force the execution of the deployed model without instrumentation to retrieve the intermediate data (alias to 'host-io-only' and 'target-io-only' mode) - Optional

--classifier

Consider the provided model as a classifier. This implies that the computation of the 'CM' and 'ACC' metrics are evaluated, else an autodetection mechanism is used to evaluate if the model is a classifier or not. - Optional

--no-check

Combined with the 'target' mode, reduce for debug purpose the full preliminary check-list to make sure that the flashed target C-model has been generated with the same tools and options. Only the c-name and network I/O shape/format are checked. - Optional

--no-exec-model

Do not execute the original model on the host with a deep learning framework runtime. Only the generated c-model is executed (see “Evaluation report and metrics” article)- Optional

--range

Indicates the min and max values (in float) for the generated random data, default is '[0.0, 1.0['. To generate randomly and uniformly the data between '-1.0' and '1.0', following parameters should be passed: '--range -1 1' (Refer to “Random data generation” section)- Optional

--seed

Define the seed which is used to initialize the pseudorandom number generator for the random data generation. Else a fixed seed is used - Optional

--save-csv

Save the whole data in the respective '*.csv' files. By default, for performance reasons, only a limited part are saved. - Optional

For 'ispu' target an additional option is defined to specify the file needed to load the ISPU program (see the “Validate command extension” section of the ISPU specific documentation).

At the end of the process, results are summarized in a simple table (see “Evaluation report and metrics” for a detailed description of the results).

Evaluation report (summary)
----------------------------------------------------------------------------------------------------------
Mode                 acc      rmse      mae       l2r       tensor
----------------------------------------------------------------------------------------------------------
x86 C-model #1       92.68%   0.053623  0.005785  0.340042  dense_4_nl [ai_float, [(1, 1, 36)], m_id=[10]]
original model #1    92.68%   0.053623  0.005785  0.340042  dense_4_nl [ai_float, [(1, 1, 36)], m_id=[10]]
X-cross #1           100.00%  0.000000  0.000000  0.000000  dense_4_nl [ai_float, [(1, 1, 36)], m_id=[10]]
----------------------------------------------------------------------------------------------------------

Serial COM port configuration

The '-d/--desc' option should be used to indicate how to configure the serial COM driver to access the board.

By default, an autodetection mechanism is applied to discover a connected board at 115200 (default value: default:115200) or 921600 for ISPU

  • Set the baud rate to 921600

    $ stedgeai validate -m <model_file_path> --target stm32 --mode target -d serial:921600
  • Set the COM port to COM16 (Windows case) or /dev/ttyACM0 (Linux case)

    $ stedgeai validate -m <model_file_path> --target stm32 --mode target -d serial:COM16
    $ stedgeai validate -m <model_file_path> --target stm32 --mode target -d serial:/dev/ttyACM0
  • Set the COM port to COM16 and the baud rate to 921600

    $ stedgeai validate -m <model_file_path> --target stm32 --mode target -d serial:COM16:921600

Extended complexity report per layer

If '-v 2' option is used, the “Complexity report per layer” table is extended with a specific column to report the metric according the data type: 'l2r' for the floating-point models and 'rmse' for the integer or quantized models. By default, the metric is computed only on the last layers (outputs of the model), however for the Keras floating-point model, the '--full' option allows computing this error layer-by-layer.

* indicates the max value

$ stedgeai validate -m <model_f32p_file_path> --target stm32 -v 2
...
 Complexity report per layer - macc=4,013 weights=15,560 act=192 ram_io=416
 ---------------------------------------------------------------------------------------------------------
 id   name           c_macc                    c_rom                     c_id   c_dur    l2r (X-CROSS)
 ---------------------------------------------------------------------------------------------------------
 0    dense_1        ||||||||||||||||  82.2%   ||||||||||||||||  84.8%   [0]     11.3%
 1    activation_1   |                  0.8%   |                  0.0%   [1]     13.3%
 2    dense_2        |||               12.7%   |||               13.1%   [2]     16.5%
 3    activation_2   |                  0.4%   |                  0.0%   [3]     17.7%
 4    dense_3        |                  2.0%   |                  2.1%   [4]     19.4%
 5    activation_3   |                  1.9%   |                  0.0%   [5]     21.9%   3.95458301e-07 *
...
$ stedgeai validate -m <model_f32p_file_path> --target stm32 --full
...
 Complexity report per layer - macc=4,013 weights=15,560 act=192 ram_io=416
 ---------------------------------------------------------------------------------------------------------
 id   name           c_macc                    c_rom                     c_id   c_dur    l2r (X-CROSS)
 ---------------------------------------------------------------------------------------------------------
 0    dense_1        ||||||||||||||||  82.2%   ||||||||||||||||  84.8%   [0]     11.0%   5.62010030e-08
 1    activation_1   |                  0.8%   |                  0.0%   [1]     13.3%   5.57235715e-08
 2    dense_2        |||               12.7%   |||               13.1%   [2]     16.3%   8.20674515e-08
 3    activation_2   |                  0.4%   |                  0.0%   [3]     18.0%   8.00048383e-08
 4    dense_3        |                  2.0%   |                  2.1%   [4]     19.6%   1.32168850e-07
 5    activation_3   |                  1.9%   |                  0.0%   [5]     21.9%   3.95458301e-07 *
...

Warning

'--full' option can be also used for validation on target ('--mode target'), to report the L2r error per layer, however, be aware that the validation time is significantly increased due to the download of the intermediate results.

Execution time per layer

Validation on target

The validation on target allows to have a full and accurate profiling report including:

  • inference-time
  • number of CPU cycles by MACC
  • execution time per layer
  • Device HW settings/configurations (clock frequency, memory configuration)
...
Running the ST.AI c-model (AI RUNNER)...(name=network, mode=TARGET)

 Proto-buffer driver v2.0 (msg v3.1) (Serial driver v1.0 - COM4:115200) ['network']

  Summary 'network' - ['network']
  -----------------------------------------------------------------------------------
  I[1/1] 'input_1'    :   int8[1,1,28,28], 784 Bytes, QLinear(0.012722839,-95,int8),
                          activations
  O[1/1] 'output_1'   :   f32[1,10], 40 Bytes,
                          activations
  n_nodes             :   9
  activations         :   32640
  weights             :   1200584
  macc                :   12052856
  hash                :   0x00f1e2478590bea3e6ed23bba954f39f
  compile_datetime    :   Nov 5 2024 11:58:56
  -----------------------------------------------------------------------------------
  protocol            :   Proto-buffer driver v2.0 (msg v3.1)
                          (Serial driver v1.0 - COM4:115200)
  tools               :   ST.AI (st-ai api) v2.0.0
  runtime lib         :   v10.0.0-9a75ee0c compiled with GCC 12.3.1 (GCC)
  capabilities        :   IO_ONLY, PER_LAYER, PER_LAYER_WITH_DATA, SELF_TEST
  device.desc         :   stm32 family - 0x450 - STM32H743/53/50xx and
                          STM32H745/55/47/57xx @480/240MHz
  device.attrs        :   fpu,art_lat=4,core_icache,core_dcache
  -----------------------------------------------------------------------------------

  ST.AI Profiling results v2.0 - "network"
  ---------------------------------------------------------------
  nb sample(s)   :   10
  duration       :   28.016 ms by sample (28.010/28.023/0.004)
  macc           :   12052856
  cycles/MACC    :   1.12
  CPU cycles     :   [13,447,454]
  ---------------------------------------------------------------

   Inference time per node
   ----------------------------------------------------------------------------------------------
   c_id    m_id   type                   dur (ms)       %    cumul  CPU cycles       name
   ----------------------------------------------------------------------------------------------
   0       11     Conv2D (0x103)            1.255    4.5%     4.5%  [    602,299 ]   ai_node_0
   1       17     Conv2dPool (0x109)       20.223   72.2%    76.7%  [  9,707,063 ]   ai_node_1
   2       20     Transpose (0x10a)         0.795    2.8%    79.5%  [    381,426 ]   ai_node_2
   3       20     NL (0x107)                0.580    2.1%    81.6%  [    278,565 ]   ai_node_3
   4       23     Dense (0x104)             5.147   18.4%    99.9%  [  2,470,516 ]   ai_node_4
   5       26     Dense (0x104)             0.009    0.0%   100.0%  [      4,214 ]   ai_node_5
   6       26     NL (0x107)                0.001    0.0%   100.0%  [        292 ]   ai_node_6
   7       29     Softmax (0x10c)           0.003    0.0%   100.0%  [      1,652 ]   ai_node_7
   8       30     NL (0x107)                0.003    0.0%   100.0%  [      1,427 ]   ai_node_8
   ----------------------------------------------------------------------------------------------
   n/a     n/a    Inter-nodal               0.000    0.0%   100.0%                   n/a
   ----------------------------------------------------------------------------------------------
   total                                   28.016                   [ 13,447,454 ]
   ----------------------------------------------------------------------------------------------

   Statistic per tensor
   ----------------------------------------------------------------------------------
   tensor   #    type[shape]:size         min      max     mean      std  name
   ----------------------------------------------------------------------------------
   I.0      10   i8[1,1,28,28]:784       -128      127   -1.681   73.679  input_1
   O.0      10   f32[1,10]:40          -7.937   -0.033   -4.356    1.900  output_1
   ----------------------------------------------------------------------------------
...

This report can be used to identify the main contributors in terms of inference time and to re-fine the model accordingly. 'c_id' column references the index of the c-node (see “C-graph description” section) and the 'm_id' identifies the index from the original model.

out-of-the-box execution

When 'target-io-only' mode or --io-only options are used, the deployed model is only executed out-of-the-box. Executing time or l2r per layer are no more computed. This can be used to limit the traffic between the host and the target reducing the validation time.

...
  ST.AI Profiling results v2.0 - "network"
  ------------------------------------------------------------------
  nb sample(s)      :   10
  duration          :   28.016 ms by sample (28.007/28.044/0.010)
  macc              :   12052856
  cycles/MACC       :   1.12
  CPU cycles        :   [13,447,610]
  used stack/heap   :   1300/0 bytes
  ------------------------------------------------------------------

   Statistic per tensor
   ----------------------------------------------------------------------------------
   tensor   #    type[shape]:size         min      max     mean      std  name
   ----------------------------------------------------------------------------------
   I.0      10   i8[1,1,28,28]:784       -128      127   -1.681   73.679  input_1
   O.0      10   f32[1,10]:40          -7.937   -0.033   -4.356    1.900  output_1
   ----------------------------------------------------------------------------------
...

Validation on host

For validation on host, the relative execution time per layer is not reported by default; the '-v 2' option should be used to display them. Nevertheless, it is important to note that these values are only indicators. They depend on the implementation of the kernels, which are not optimized, and the workload of the desktop/host machine (see device.desc field). This contrasts with the reported inference times for validation on the target.

$ stedgeai validate -m <model_file_path> --target stm32 -v 2 [--mode host]
...
Running the ST.AI c-model (AI RUNNER)...(name=network, mode=HOST)

 DLL Driver v2.0 - Direct Python binding
   (<workspace-directory-path>\inspector_network\workspace\lib\libai_network.dll) ['network']

  Summary 'network' - ['network']
  -----------------------------------------------------------------------------------
  I[1/1] 'input_1'    :   int8[1,28,28,1], 784 Bytes, QLinear(0.012722839,-95,int8),
                          in activations buffer
  O[1/1] 'output_1'   :   f32[1,1,1,10], 40 Bytes, in activations buffer
  n_nodes             :   9
  activations         :   32640
  weights             :   1200584
  macc                :   12052856
  hash                :   0x00f1e2478590bea3e6ed23bba954f39f
  compile_datetime    :   Nov 15 2024 12:49:14
  -----------------------------------------------------------------------------------
  protocol            :   DLL Driver v2.0 - Direct Python binding
  tools               :   ST.AI (legacy api) v2.0.0
  runtime lib         :   v10.0.0
  capabilities        :   IO_ONLY, PER_LAYER, PER_LAYER_WITH_DATA
  device.desc         :   AMD64, Intel64 Family 6 Model 165 Stepping 2, GenuineIntel,
                          Windows
  -----------------------------------------------------------------------------------

 NOTE: The duration and execution time per layer are just indications. They depend
 on the host machine's workload.

  ST.AI Profiling results v2.0 - "network"
  ------------------------------------------------------------------
  nb sample(s)       :   10
  duration           :   6.068 ms by sample (5.698/6.571/0.223)
  macc               :   12052856
  ------------------------------------------------------------------
  DEVICE duration    :   7.066 ms by sample (including callbacks)
  HOST duration      :   0.074 s (total)
  used mode          :   Mode.PER_LAYER
  number of c-node   :   9
  ------------------------------------------------------------------

   Inference time per node
   --------------------------------------------------------------------------------
   c_id    m_id   type                   dur (ms)       %    cumul     name
   --------------------------------------------------------------------------------
   0       11     Conv2D (0x103)            0.144    2.4%     2.4%     ai_node_0
   1       17     Conv2dPool (0x109)        5.142   84.7%    87.1%     ai_node_1
   2       20     Transpose (0x10a)         0.035    0.6%    87.7%     ai_node_2
   3       20     NL (0x107)                0.009    0.2%    87.8%     ai_node_3
   4       23     Dense (0x104)             0.731   12.0%    99.9%     ai_node_4
   5       26     Dense (0x104)             0.002    0.0%    99.9%     ai_node_5
   6       26     NL (0x107)                0.001    0.0%    99.9%     ai_node_6
   7       29     Softmax (0x10c)           0.002    0.0%   100.0%     ai_node_7
   8       30     NL (0x107)                0.001    0.0%   100.0%     ai_node_8
   --------------------------------------------------------------------------------
   n/a     n/a    Inter-nodal               0.001    0.0%   100.0%     n/a
   --------------------------------------------------------------------------------
   total                                    6.068
   --------------------------------------------------------------------------------

   Statistic per tensor
   ----------------------------------------------------------------------------------
   tensor   #    type[shape]:size         min      max     mean      std  name
   ----------------------------------------------------------------------------------
   I.0      10   i8[1,28,28,1]:784       -128      127   -1.681   73.679  input_1
   O.0      10   f32[1,1,1,10]:40      -7.937   -0.033   -4.356    1.900  output_1
   ----------------------------------------------------------------------------------
...

Generate command

Description

The 'generate' command is used to generate the specialized network and data C-files. According to the c-api option, the used target, and other additional options, the generated files can be different.

Generated files with “legacy” C-API option

With the 'legacy' C-API, the following files are generated:

$ stedgeai generate -m <model_file_path> --target stm32 -o <output-directory-path> [--c-api legacy]
...
Generated files (7)
-----------------------------------------------------------
<output-directory-path>\<name>_config.h
<output-directory-path>\<name>.c
<output-directory-path>\<name>_data.c
<output-directory-path>\<name>_data_params.c
<output-directory-path>\<name>.h
<output-directory-path>\<name>_data.h
<output-directory-path>\<name>_data_params.h

Creating report file <output-directory-path>\network_generate_report.txt
...
  • '<name>.c/.h' files contain the topology of the C-model (C-struct definition of the tensors and the operators), including the embedded inference client API (refer to “Embedded Inference Client API” article) to use the generated c-model on the top of the optimized inference runtime library.

  • '<name>_data_params.c/.h' files contain by default a simple C-array with the data of the weight/bias tensors. However, the '--split-weights' option allows having a C-array by tensor (refer to “Split weights buffer” section) and the '--binary' option creates a binary file with the data of the weight/bias tensors. The '--relocatable/-r' option (available only for stm32) allows generating a relocatable binary model including the topology definition, the requested kernels, and the weights in a single binary file (refer to “Relocatable binary model support” article).

  • '<name>_data.c/.h' files contain the intermediate functions requested by the specialized init function to manage the C-array with the weights.

Generated files with “st-ai” C-API option

With the 'st-ai' C-API, the following files are generated:

$ stedgeai generate -m <model_file_path> --target stellar-e -o <output-directory-path> --c-api st-ai
or
$ stedgeai generate -m <model_file_path> --target stellar-pg -o <output-directory-path> --c-api st-ai
...
Generated files (5)
-----------------------------------------------------------
<output-directory-path>\<name>.c
<output-directory-path>\<name>_data.c
<output-directory-path>\<name>.h
<output-directory-path>\<name>_data.h
<output-directory-path>\<name>_details.h

Creating report file <output-directory-path>\network_generate_report.txt
...
  • '<name>.c/.h' files contain the topology of the C-model (C-struct definition of the tensors and the operators), including the embedded inference client API (refer to “Embedded Inference Client ST Edge AI API” article) to use the generated c-model on the top of the optimized inference runtime library.
  • '<name>_data.c/.h' files contain by default a simple C-array with the data of the weight/bias tensors. However, the '--split-weights' option allows having a C-array by tensor (refer to “Split weights buffer” section)
  • '<name>_details.h' files contain the debug information about the intermediate tensors (debug/advanced purpose)

For ISPU target, the generated output also contains the runtime library and its header files and is structured in a manner to correctly populate the provided templates. For more details refer to the “Generate command extension” section of the ISPU specific documentation.

Examples

  • Generate the specialized NN C-files (default options).

    $ stedgeai generate -m <model_file_path> --target stellar-e
    or
    $ stedgeai generate -m <model_file_path> --target stellar-pg
  • Generate the specialized NN C-files for a 32b float model with compression factor.

    $ stedgeai generate -m <model_file_path> --target stm32 -c medium

Specific options

Supported-ops command

Description

The 'suppoorted-ops' command is used to display the list of the supported operators for a given deep learning framework with the '-t/--type' option. Else by default, all operators are listed.

Specific arguments

--with-report

If defined, this flag allows generating a report, txt file (Markdown format) with the list of the operators and associated constraints. - Optional

This option has been used to generate the following articles: “Keras toolbox support”, “TFLite toolbox support and “ONNX toolbox support”

Examples

  • Generate the list of the supported operators (default)

    $ stedgeai supported-ops
    ST Edge AI Core v1.0.0
    281 operators found
        Abs (ONNX), ABS (TFLITE), Acos (ONNX), Acosh (ONNX), Activation (KERAS), 
        ActivityRegularization (KERAS), Add (KERAS), Add (ONNX), ADD (TFLITE),
        AlphaDropout (KERAS), And (ONNX), ARG_MAX (TFLITE), ARG_MIN (TFLITE),
        ArgMax (ONNX), ArgMin (ONNX), ArrayFeatureExtractor (ONNX), Asin (ONNX),
        Asinh (ONNX),...
  • Generate the list of the supported Keras operators

    $ stedgeai supported-ops -t keras
    ST Edge AI Core v1.0.0
    Parsing operators for KERAS toolbox
    62 operators found
     Activation, ActivityRegularization, Add, AlphaDropout, Average, AveragePooling1D, AveragePooling2D,
     BatchNormalization, Bidirectional, Concatenate, Conv1D, Conv2D, Conv2DTranspose, Cropping1D,
     Cropping2D, Dense, DepthwiseConv2D, Dropout, ELU, Flatten, GaussianDropout, GaussianNoise,
     GlobalAveragePooling1D, GlobalAveragePooling2D, GlobalMaxPooling1D, GlobalMaxPooling2D, GRU
     InputLayer, ..
    30 custom operators found
     Abs, Acos, Acosh, Asin, Asinh, Atan, Atanh, Ceil, Clip, Cos, Exp, Fill, FloorDiv, FloorMod, Gather,
     CustomLambda, Log, Pow, Reshape, Round, Shape, Sign, Sin, Split, Sqrt, Square, Tanh, Unpack, Where,
     TFOpLambda
  • Generate the list of the supported ONNX operators

    $ stedgeai supported-ops -t onnx
  • Generate the list of the supported tflite operators

    $ stedgeai supported-ops -t tflite
  • Generate the list of the supported Keras operators with a full report

    $ stedgeai supported-ops -t keras --with-report
    ...
    Building report..
    creating file : <output-directory-path>/supported_ops_keras.md