Embedded Inference Client API (legacy)
ST Edge AI Core Technology 2.0.0
r5.2
Introduction
This article describes the embedded inference client API which
must be used by a C-application layer (AI client) to use a deployed
C-model. This API is available for STM32 and STELLAR targets. All
model-specific definitions and implementations can be found in the
generated C-files: <name>.c,
<name>.h and <name>_data.h
files. For debug, advanced use-cases and profiling purposes,
Platform observer API is available (refer to “Platform Observer API
(legacy)” article).
Above figure shows that the integration of the AI stack in an
application is simple and straightforward. There is few or standard
SW/HW dependencies with the run-time. AI client uses the generated
model through a set of well-defined ai_<name>_XXX()
functions (also called “Embedded inference client API”).
The ST Edge AI Core pack provides a compiled library (i.e. network
runtime library) by target and by supported tool-chains.
Getting started - Minimal application
The following code snippet provides a typical and minimal example
using the API for a 32b floating-point model. The pre-trained model
is generated with the default options (i.e. input and output buffers
are not allocated in the “activations” buffer and default
network c-name is used). Note that all AI requested
client resources (activations buffer and data buffers for the IO)
are allocated at compile time thanks the generated macros: AI_NETWORK_XXX_SIZE
allowing a minimalist, easier and quick integration.
#include <stdio.h>
#include "network.h"
#include "network_data.h"
/* Global handle to reference the instantiated C-model */
static ai_handle network = AI_HANDLE_NULL;
/* Global c-array to handle the activations buffer */
AI_ALIGNED(32)
static ai_u8 activations[AI_NETWORK_DATA_ACTIVATIONS_SIZE];
/* Array to store the data of the input tensor */
AI_ALIGNED(32)
static ai_float in_data[AI_NETWORK_IN_1_SIZE];
/* or static ai_u8 in_data[AI_NETWORK_IN_1_SIZE_BYTES]; */
/* c-array to store the data of the output tensor */
AI_ALIGNED(32)
static ai_float out_data[AI_NETWORK_OUT_1_SIZE];
/* static ai_u8 out_data[AI_NETWORK_OUT_1_SIZE_BYTES]; */
/* Array of pointer to manage the model's input/output tensors */
static ai_buffer *ai_input;
static ai_buffer *ai_output;
/*
* Bootstrap
*/
int aiInit(void) {
ai_error err;
/* Create and initialize the c-model */
const ai_handle acts[] = { activations };
err = ai_network_create_and_init(&network, acts, NULL);
if (err.type != AI_ERROR_NONE) { ... };
/* Reteive pointers to the model's input/output tensors */
ai_input = ai_network_inputs_get(network, NULL);
ai_output = ai_network_outputs_get(network, NULL);
return 0;
}
/*
* Run inference
*/
int aiRun(const void *in_data, void *out_data) {
ai_i32 n_batch;
ai_error err;
/* 1 - Update IO handlers with the data payload */
ai_input[0].data = AI_HANDLE_PTR(in_data);
ai_output[0].data = AI_HANDLE_PTR(out_data);
/* 2 - Perform the inference */
n_batch = ai_network_run(network, &ai_input[0], &ai_output[0]);
if (n_batch != 1) {
err = ai_network_get_error(network);
...
};
return 0;
}
/*
* Example of main loop function
*/
void main_loop() {
aiInit();
while (1) {
/* 1 - Acquire, pre-process and fill the input buffers */
acquire_and_process_data(in_data);
/* 2 - Call inference engine */
aiRun(in_data, out_data);
/* 3 - Post-process the predictions */
post_process(out_data);
}
}Only the following CFLAGS/LDFLAGS extensions
(Embedded GCC-based for ARM tool-chain) are requested to compile the
specialized c-files and to add the inference runtime library in a
STM32 Cortex-m4 based project.
CFLAGS += -mcpu=cortex-m4 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard
CFLAGS += -IMiddlewares/ST/AI/Lib/Inc
LDFLAGS += -LMiddlewares/ST/AI/Lib/Lib -l:NetworkRuntime910_CM4_GCC.aAI buffers and privileged placement
From the application/integration point of view, only three memory-related objects are considered as dimensioning for the system. They are fixed size since there is no support for the dynamic tensors i.e., all the sizes and shapes of the tensors are defined/fixed at generation time. In this way inference C run-time engine does not require to use the system heap.
- “activations” buffer is a simple contiguous memory-mapped
buffer, placed into a read-write memory segment. It is owned and
allocated by the AI client, it is passed to the network instance
(see
ai_<name>_init()function) and used as private heap (or working buffer) during the execution of the inference to store the intermediate results. Between two inferences, the associated memory segment can be reused by the application. Its size (AI_<NAME>_DATA_ACTIVATIONS_SIZE) is defined during the code generation and corresponds to the reportedRAMmetric. - “weights” buffer is a simple contiguous memory-mapped buffer (or
multiple memory-mapped buffers when the
--split-weightsoption is used). It is generally placed into a non-volatile and read-only memory device. The total size (AI_<NAME>_DATA_WEIGHTS_SIZE) is defined during the code generation and corresponds to the reportedROMmetric. - “output” and “input” buffers must be also placed in the
read-write memory-mapped buffers. By default, they are owned and
provided by the AI client. Their sizes are model dependent and known
as generation time (
AI_<NAME>_IN/OUT_SIZE_BYTES). but they can be also located in the “activations” buffer.
Note
The placement of the buffers is application linker or/and runtime dependent. Additional ROM and RAM for the network runtime library itself and for network c-files (txt/rodata/bss and data sections) can be also considered but they are generally not significant to dimension the system in comparison with the required size for the “weighs” and “activations” buffers.
Following table details the privileged placement choices to minimize the inference time for a typical STM32 target. Usually the most constrained memory object is the “activations” buffer.
| memory object type | preferably placed in |
|---|---|
| client stack | a low latency & high bandwidth device. STM32 embedded SRAM or data-TCM when available (zero wait-state memory). |
| activations, inputs/outputs | a low/medium latency & high bandwidth device. STM32 embedded SRAM when available or external RAM. The trade-off is mainly driven by the size and if the STM32 MCU has a data cache (Cortex-M7 family). If the input buffers are not allocated in the “activations” buffer, the “activations” buffer should be privileged. |
| weights | a medium latency & medium bandwidth device. STM32 embedded FLASH memory or external FLASH. The trade-off is driven by the STM32 MCU data cache availability (Cortex-M7 family), the weights can be split between different memory devices. |
I/O buffers inside the “activations” buffer
By default, the input and output buffers are allocated in the
“activations” buffer. During generation, the minimal size of the
“activations” buffer is adjusted accordingly. Please note that the
base addresses of the respective memory sub-regions depend on the
model. These addresses are not necessarily aligned with the base
address of the “activations” buffer and are pre-defined or
pre-computed at generation time. For more details, refer to the snippet code. Inside the
“activations” buffer, the reserved memory regions are 4-bytes
aligned (or 8-bytes) according the selected target. For the specific
needs, the user has the possibility to define the requested
memory-alignment for the input buffers (respectively for the output
buffers) with the --input-memory-alignment INT
option (respectively --output-memory-alignment).
- “external” input/output buffers (i.e. allocated outside the
“activations” buffer) can be always used even if
--allocate-inputsor--allocate-outputsoption is used since input and output are passed throughai_<name>_run(). --allocate-inputsoption reserves only the place for one buffer by input tensor. If a double buffer scheme should be implemented,--allocate-inputsflag should be not used.
Multiple heap support
To optimize usage of the RAM for performance reasons or because the available memory is fragmented between different memory devices (embedded in the device or externally), the activations buffer can be dispatched in different memory segments.
Thanks to the --memory-pool
option, the user has the possibility to describe the available
memories (i.e. memory pools) which can be used to place the
activation tensors (and/or scratch buffers). During the code
generation, the allocator will privilege the memory pools according
to the description order in the JSON file. If a memory pool can be
not used (insufficient size), the next will be used if available
else an error is generated. The allocator considers the first memory
pool as the privileged location to place the critical
buffers to optimize the inference time. First memory pool should be
placed in high throughput, low latency memory device.
Following figure illustrates the case where the activations
buffer is split in 3. The first part is placed in the low
latency/high throughput memory (like DTCM for STM32H7/F7 series),
the second is placed in a “normal” internal memory and the last in
an external memory. The JSON file is requested to indicate the
maximum size of each memory segment ("usable_size" key)
which can be used by the AI stack allowing to reserve a part of the
critical memory resources for other SW objects.
Following snippet code illustrates the initialization sequence.
The 'activationsX' objects will be placed in different
memory devices thanks to specific linker directives by the
end-user.
...
AI_ALIGNED(32)
static ai_u8 activations1[AI_NETWORK_DATA_ACTIVATIONS_1_SIZE];
AI_ALIGNED(32)
static ai_u8 activations2[AI_NETWORK_DATA_ACTIVATIONS_2_SIZE];
AI_ALIGNED(32)
static ai_u8 activations3[AI_NETWORK_DATA_ACTIVATIONS_3_SIZE];
...
int aiInit(void) {
ai_error err;
/* Create and initialize the c-model */
const ai_handle acts[] = { activations1, activations2, activations3 };
err = ai_network_create_and_init(&network, acts, NULL);
if (err.type != AI_ERROR_NONE) { ... };
...
}or without the helper function
...
int aiInit(void) {
ai_network_params params;
ai_network_create(&network, NULL);
ai_network_data_params_get(¶ms);
AI_BUFFER_ARRAY_ITEM_SET_ADDRESS(¶ms.map_activations, 0, activations1);
AI_BUFFER_ARRAY_ITEM_SET_ADDRESS(¶ms.map_activations, 1, activations2);
AI_BUFFER_ARRAY_ITEM_SET_ADDRESS(¶ms.map_activations, 2, activations3);
ai_network_init(network, ¶ms);
}Split weights buffer
The --split-weights option allows to place
statically tensor-by-tensor the weights in different STM32 memory
segments (on or off-chip) thanks to specific linker directives for
the end-user application.
- it relaxes the placing constraint of a large buffer into a
constrained and non-homogeneous memory sub-system.
- after profiling, it allows to improve the global inference time, by placing the critical weights into a low latency memory. Or on the contrary it can free the critical resource (i.e. internal flash) which can be used by the application.
The --split-weights option prevents the generation
of a unique c-array for the whole data of the weights/bias tensors
(<name>_data.c file). Without the options weights
are declared as:
ai_handle ai_network_data_weights_get(void)
{
AI_ALIGNED(4)
static const ai_u8 s_network_weights[ 794136 ] = {
0xcf, 0xae, 0x9d, 0x3d, 0x1b, 0x0c, 0xd1, 0xbd, 0x63, 0x99,
0x36, 0xbd, 0xdb, 0x67, 0x46, 0xbe, 0x3b, 0xe7, 0x0d, 0x3e,
...
0x41, 0xbf, 0xc6, 0x7d, 0x69, 0x3e, 0x18, 0x87, 0x37,
0xbe, 0x83, 0x63, 0x0f, 0x3f, 0x51, 0xa1, 0xdd, 0xbe
};
return AI_HANDLE_PTR(s_network_weights);
}On the contrary with --split-weights a
s_<network>_<layer_name>_[bias|weights|*]_array_weights[])
c-array is created to store the data of each weight/bias tensor. A
global map table is also built that is used by the run-time to
retrieve the addresses of the different c-arrays.
...
/* conv2d_1_weights_array - FLOAT|CONST */
AI_ALIGNED(4)
const ai_u8 s_network_conv2d_1_weights_array_weights[ 2048 ] = {
0xcf, 0xae, 0x9d, 0x3d, 0x1b, 0x0c, 0xd1, 0xbd, 0x63, 0x99,
...
}
...
/* dense_3_bias_array - FLOAT|CONST */
AI_ALIGNED(4)
const ai_u8 s_network_dense_3_bias_array_weights[ 24 ] = {
0xa2, 0x72, 0x82, 0x3e, 0x5a, 0x88, 0x41, 0xbf, 0xc6, 0x7d,
0x69, 0x3e, 0x18, 0x87, 0x37, 0xbe, 0x83, 0x63, 0x0f, 0x3f,
0x51, 0xa1, 0xdd, 0xbe
};
/* Entry point to retrieve the address of the c-arrays */
ai_handle ai_network_data_weights_get(void) {
static const ai_u8* const s_network_params_map_table[] = {
&s_conv2d_1_weights_array_weights[0],
...
&s_dense_3_bias_array_weights[0],
};
return AI_HANDLE_PTR(s_network_params_map_table);
};- without particular linker directives, these multiple c-arrays
are always placed in a
.rodatasection as for the unique c-array.
- client API is not affected by the split: the
ai_network_data_weights_get()function is used to pass the entry point of the weights buffer to theai_<name>_init()function.
- as shown in the previous figure,
constC-attribute can be manually commented to use the default C-startup behavior to copy the data in an initialized RAM data section.
Re-entrance and thread safety considerations
No internal synchronization mechanism is implemented to protect
the entry points against concurrent accesses. If the API is used in
a multi-threaded context, the protection of the instantiated NN(s)
must be guaranteed by the application layer itself. To minimize the
usage of the RAM, the same activation memory chunk
(SizeSHARED) can be used to support multiple networks.
In this case, the user must guarantee that an on-going inference
execution cannot be preempted by the execution of another
network.
SizeSHARED = MAX(AI_<name>_DATA_ACTIVATIONS_SIZE) for name = “net1” … “net2”Tip
If the preemption is expected for real-time constraint or latency reasons, each network instance must have its own and private activations buffer.
Debug support
The network runtime library must be considered as an optimized
black box object in binary format (sources files are not delivered).
There is no run-time services allowing to dump internal states.
Mapping and port of the model is guaranteed by the ST Edge AI Core
generator. Some integration issues can be highlighted by the
ai_<name>_get_error() function or by the usage of
the Platform observer API
to inspect the intermediate results.
Versioning
A dedicated <network>_config.h is generated
with the C-defines which allows to know the version of the tool used
to generated the specialized NN C-files and the versions of the
associated run-time API.
Warning
Backward or/and forward compatibility between generated code and run-time library is not fully guaranteed. If a new version of the tool is used to generate the new specialized NN c-files, it is highly recommended to update also the associated header files and network run-time library.
/* <network>_config.h file */
#define AI_TOOLS_VERSION_MAJOR 1
#define AI_TOOLS_VERSION_MINOR 0
#define AI_TOOLS_VERSION_MICRO 0
#define AI_PLATFORM_API_MAJOR 1
#define AI_PLATFORM_API_MINOR 1
#define AI_PLATFORM_API_MICRO 0
#define AI_TOOLS_API_VERSION_MAJOR 1
#define AI_TOOLS_API_VERSION_MINOR 5
#define AI_TOOLS_API_VERSION_MICRO 0| type | description |
|---|---|
| AI_TOOLS_VERSION_XX | global version of the tool package |
| AI_PLATFORM_API_XX | the version of the generated API or embedded inference client API. Can be used by the application code to check if there is a API break (source level). |
| AI_TOOLS_API_VERSION_XX | the version of the API which is used by the generated NN c-files to call the network runtime library. |
These C-defines can be used by the application code to check at
compile time that the version of the used network run-time library
is aligned with the generated NN c-files. At run-time, the network
runtime library checks strictly only the AI_TOOLS_API
versions. The following ai_error will be returned by
the ai_<network>_create()
function if the version is not respected.
.code = AI_ERROR_CODE_NETWORK
.type = AI_ERROR_TOOL_PLATFORM_API_MISMATCHAt run-time, ai_<network>_get_report()
function allows to retrieve the different versions through the
ai_network_report C-structure (see
ai_platform.h file).
.tool_version /* return compiled version of the tool - AI_TOOLS_VERSION_XX */
.tool_api_version /* return compiled version of the tool API - AI_TOOLS_API_VERSION_XX */
.api_version /* return compiled version of the embedded client API - AI_PLATFORM_API_XX */Embedded inference client API
AI_<NAME>_XXX C-defines
Different C-defines are generated in the
<name>.h and <name>_data.h
files. They can be used by the application code to allocate at
compile time or dynamically the requested buffers, or for debug
purpose. At run-time, ai_<network>_get_report()
can be used to retrieve the requested sizes.
| C-defines | description |
|---|---|
AI_<NAME>_MODEL_NAME |
C-string with the C-name of the model |
AI_<NAME>_ORIGIN_MODEL_NAME |
C-string with the original name of the model |
AI_<NAME>_IN/OUT_NUM |
the total number of input/output tensors |
AI_<NAME>_IN/OUT_SIZE |
C-table (integer type) storing the number of item by input/output tensors (= H x W x C) (see “IO tensor description” section) |
AI_<NAME>_IN/OUT_SIZE_BYTES |
C-table (integer type) storing the size in bytes of input/output tensors |
AI_<NAME>_IN/OUT_x_SIZE |
the total number of item for the x-th input/output tensor |
AI_<NAME>_IN/OUT_x_SIZE_BYTES |
the size in bytes for the x-th
input/output tensor (see ai_<name>_run()
function) |
AI_<NAME>_IN/OUT_x_HEIGHT |
the expected “height” dimension value for the x-th input/output tensor |
AI_<NAME>_IN/OUT_x_WIDTH |
the expected “width” dimension value for the x-th input/output tensor |
AI_<NAME>_IN/OUT_x_DEPTH |
the expected “depth” dimension value for the x-th input/output tensor |
AI_<NAME>_IN/OUT_x_CHANNEL |
the expected “channel” dimension value for the x-th input/output tensor |
AI_<NAME>_DATA_ACTIVATIONS_SIZE |
the minimal size in bytes which must
be provided by a client application as activations buffer (see ai_<name>_init()
function) |
AI_<NAME>_DATA_ACTIVATIONS_COUNT |
the number of activations buffers |
AI_<NAME>_DATA_ACTIVATIONS_x_SIZE |
the size in bytes of the x-th activations buffer |
AI_<NAME>_DATA_WEIGHTS_SIZE |
the size in bytes of the generated weights/bias buffer |
AI_<NAME>_INPUTS_IN_ACTIVATIONS |
if the input buffers have to be put
the activations buffer. It is only defined if the
--allocate-inputs option is used. |
AI_<NAME>_OUTPUTS_IN_ACTIVATIONS |
if the outputs buffers are stored into
activations buffer. It is only defined if the
--allocate-outputs option is used. |
ai_<name>_create()
ai_error ai_<name>_create(ai_handle* network, const ai_buffer* network_config);
ai_handle ai_<name>_destroy(ai_handle network);This mandatory function is the early
function which must be called by the application to create an
instance of the c-model. Provided ai_handle object is
updated and it references a context (opaque object) which should be
passed to the other functions.
network_configparameter is a specific network configuration buffer (opaque structure) coded as anai_buffer. It is generated by the code generator and should be not modified by the application. Currently, this object is always empty andNULLcan be passed but it is preferable to passAI_NETWORK_DATA_CONFIG(see<name>_data.hfile).
When the instance is no more used by the application,
ai_<name>_destroy() function should be called to
release the possible allocated resources.
Warning
Only one instance at a time of a c-model is supported. Returned
ai_handle references always the same object so the same
C-model can be not used in a pre-emptive runtime environment w/o
additional user synchronization
mechanism.
ai_<name>_init()
ai_bool ai_<name>_init(ai_handle network, const ai_network_params* params);This mandatory function is used by the application to initialize the internal run-time data structures and to set the activations buffer and weights buffer.
paramsparameter is a structure (ai_network_paramstype) which allows to pass the references of the weights and the activations buffers (array format)networkhandle should be a valid handle, seeai_<name>_create()function
The ai_network_data_params_get()
function must be used to retrieve an initialized object (see
network_data.c file).
'AI_BUFFER_ARRAY_ITEM_SET_ADDRESS()' C-macro can be
used to set the address of the underlying memory segment. Usage of
the ai_network_create_and_init()
helper function is privileged for the default UCs.
#include "network.h"
#include "network_data.h"
AI_ALIGNED(32)
static ai_u8 activations[AI_NETWORK_DATA_ACTIVATIONS_SIZE];
...
ai_network_params params;
ai_network_data_params_get(¶ms);
AI_BUFFER_ARRAY_ITEM_SET_ADDRESS(¶ms.map_activations, 0, activations);
ai_network_init(network, ¶ms);ai_<name>_create_and_init()
ai_error ai_<name>_create_and_init(ai_handle* network,
const ai_handle activations[], const ai_handle weights[]);This helper function aggregates the call of the create and init functions (see code in the generated
'network.c' file). It allows to pass the addresses of
the activations buffers and optionally the addresses of the weights
buffers.
#include "network.h"
#include "network_data.h"
AI_ALIGNED(32)
static ai_u8 activations[AI_NETWORK_DATA_ACTIVATIONS_SIZE];
...
const ai_handle acts[] = { activations };
ai_network_create_and_init(&network, acts, NULL);ai_<name>_get_report()
ai_bool ai_<name>_get_info(ai_handle network, ai_network_report* report);This function allows to retrieve the run-time data attributes of
an instantiated model. Refer to ai_platform.h file to
see the details of the returned ai_network_report
C-structure.
Warning
If it is called before the ai_<name>_init() (or ai_<name>_create_and_init()),
the reported information for the activations,
params, * inputs and
* outputs fields will be uncomplete since the instance
is not yet fully initialized. On the contrary, all the static
information is available..
Typical usage
#include "network.h"
...
ai_network_report report;
ai_bool res;
...
res = ai_network_get_report(network, &report)
if (res) { /* display the report */ }Example of possible reported information:
Network information
---------------------------------------------------
model_name : network
model_signature : e38d1b6095099638ae20a42e53398dd7
model_datetime : <date-time when the model has been generated>
compile_datetime : <data-time when the code has been compiled>
tool_version : 1.0.0
tool_api_version : 1.5.0
api_version : 1.2.0
n_macc : 336088
map_activations : 1
shape=(1, 1, 1, 5712) size=5712 type=2 (bits=8 fbits=0 sign=+)
map_weights : 1
shape=(1, 1, 1, 16688) size=16688 type=2 (bits=8 fbits=0 sign=+)
n_inputs : 1
shape=(1, 1, 1, 1960) size=1960 type=2 (bits=8 fbits=0 sign=-)
quantized scale=0.101716 zp=-128
n_outputs : 1
shape=(1, 1, 1, 4) size=4 type=2 (bits=8 fbits=0 sign=-)
quantized scale=0.003906 zp=-128
ai_<name>_data_params_get()
ai_bool ai_<name>_data_params_get(ai_network_params* params);This function allows to retrieve the network param configuration data structure. It should be used to update it and to pass it to the init function.
ai_<name>_[in|out]puts_get()
ai_buffer* ai_<name>_inputs_get(ai_handle* network, ai_u16 *n_buffer);
ai_buffer* ai_<name>_outputs_get(ai_handle* network, ai_u16 *n_buffer);These functions return inputs/outputs array descriptors as
ai_buffer array pointers. n_buffer is used to return
the number of inputs/outputs.
ai_<name>_run()
ai_i32 ai_<name>_run(ai_handle network, const ai_buffer* input, ai_buffer* output);This function is called to feed the neural network. The input and
output buffer parameters (ai_buffer type) allow to
provide the input tensors and to store the predicted output tensors
respectively (see “IO tensor
description” section).
- Returned value is the number of the input samples processed when
n_batches >= 1. If <=0 , an error occurs and
ai_network_get_error()should be used to detail it.
Tip
Two separate arrays of inputs and outputs ai_buffer
should be passed to use a neural network model with multiple inputs
or/and outputs. AI_NETWORK_IN_NUM and respectively
AI_NETWORK_OUT_NUM helper macro can be used to know at
compile-time the number of inputs and outputs. These values are also
included in the struct ai_network_report (see ai_<name>_get_report()
function).
Typical usages
Default Use Case is illustrated by the “Getting starting” code snippet. Following code is an example with a C-model which has one input and two output tensors. Note that the data payload of the input buffers is also used in the “activations” buffer.
#include <stdio.h>
#include "network.h"
...
/* C-table to store the @ of the input buffer */
static ai_float *in_data[AI_NETWORK_IN_NUM];
/* AI input/output handlers */
static ai_buffer *ai_inputs;
static ai_buffer *ai_outputs;
/* data buffer for the output buffers */
static ai_float out_1_data[AI_NETWORK_OUT_1_SIZE];
static ai_float out_2_data[AI_NETWORK_OUT_2_SIZE];
/* C-table to store the @ of the output buffers */
static ai_float* out_data[AI_NETWORK_OUT_NUM] = {
&out_1_data[0],
&out_2_data[0]
}
...
int aiInit(void) {
...
/* 1 - Create and initialize network */
...
/* 2 - Retrieve IO network infos */
ai_input = ai_network_inputs_get(network);
ai_ouput = ai_network_outputs_get(network);
/* 3 - retrieve the effective @ of the input buffers */
for (int i=0; i < AI_NETWORK_IN_NUM; i++) {
in_data[i] = (ai_u8 *)(ai_inputs[i].data);
}
/* 4- Update the AI output handlers */
for (int i=0; i < AI_NETWORK_OUT_NUM; i++) {
ai_outputs[i].data = AI_HANDLE_PTR(&out_data[i]);
}
...
}
void main_loop()
{
while (1) {
/* 1 - Acquire, pre-process and fill the input buffers */
acquire_and_process_data(in_data);
/* 2 - Call inference engine */
ai_network_run(network, &ai_inputs[0], &ai_outputs[0]);
/* 3 - Post-process the predictions */
post_process(out_data);
}
}ai_<name>_get_error()
ai_error ai_<name>_get_error(ai_handle network);This function can be used by the client application to retrieve
the first error reported during the execution of a
ai_<name>_xxx() function.
- See
ai_platform.hfile to have the list of the returned error type (ai_error_type) and associated code (ai_error_code).
Typical AI error function handler (debug/log purpose)
#include "network.h"
...
void aiLogErr(const ai_error err)
{
printf("E: AI error - type=%d code=%d\r\n", err.type, err.code);
}IO tensor description
N-dimensional tensors are supported with a fixed format. They are
defined by a 'struct ai_buffer' C-structure object. The
referenced memory buffer ('data' field) is physically
stored and referenced in memory as a standard C-array type. Scattered
memory buffers are not supported.
ai_buffer_shape- indicates the dimensions of the tensor
format- indicates the format of the data
meta_info- extra field to reference the additional data-dependent parameters which can be requested to handle a buffer
ai_buffer C-structure
/* @file: ai_platform.h */
typedef struct ai_buffer_ {
ai_buffer_format format; /*!< buffer format */
ai_handle data; /*!< pointer to buffer data */
ai_buffer_meta_info* meta_info; /*!< pointer to buffer metadata info */
ai_flags flags; /*!< shape optional flags */
ai_size size; /*!< number of elements of the buffer
(including optional padding) */
ai_buffer_shape shape; /*!< n-dimensional shape info */
} ai_buffer;Warning
The C-tensors are always defined with minimum 4 dimensions.
The following table shows the generated mapping of the 1d, 2d and 3d-array tensor with ‘channel-last’ data placement:
| tensor shape | mapped on (B, H, W, C) |
|---|---|
| 1d-array | (-, 1, 1, c) |
| 2d-array | (-, h, 1, c) |
| 3d-array | (-, h, w, c) |
For a 5d or 6d tensor (respectively 4d-array and 5d-array), following representation is respected:
| tensor shape | mapped on |
|---|---|
| 4d-array | (-, h, w, d, c) |
| 5d-array | (-, h, w, d, e, c) |
Retrieve tensor information
Following code snippets show how to retrieve the tensor
information from a buffer descriptor. 'format' and
'meta_info' fields are described in the next
section.
#include "network.h"
{
/* Use the generated macro to set the buffer input descriptors */
const ai_buffer *ai_input = ai_network_inputs_get(network, NULL);
/* Extract format of the first input tensor (index 0) */
const ai_buffer *ai_input_1 = &ai_input[0];
/* Extract format of the tensor */
const ai_buffer_format fmt_1 = AI_BUFFER_FORMAT(ai_input_1);
/* Extract height, width and channels of the first input tensor */
const ai_u16 height_1 = AI_BUFFER_SHAPE_ELEM(ai_input_1, AI_SHAPE_HEIGHT);
const ai_u16 width_1 = AI_BUFFER_SHAPE_ELEM(ai_input_1, AI_SHAPE_WIDTH);
const ai_u16 ch_1 = AI_BUFFER_SHAPE_ELEM(ai_input_1, AI_SHAPE_CHANNEL);
const ai_u16 size_1 = AI_BUFFER_SIZE(ai_input_1); /* number of item*/
const ai_u32 size_in_bytes_1 = AI_BUFFER_BYTE_SIZE(size_1, fmt_1);
...
}or with the ai_network_info structure
#include "network.h"
{
/* Fetch run-time network descriptor */
ai_network_report report;
ai_network_get_report(network, &report);
/* Set the descriptor of the first input tensor (index 0) */
const ai_buffer *ai_input_1 = &report.inputs[0]
/* Extract format of the tensor */
const ai_buffer_format fmt_1 = AI_BUFFER_FORMAT(ai_input_1);
...
}Tensor dimension
Following macros should be used to retrieve the associated dimensions:
| macros | description |
|---|---|
AI_BUFFER_SHAPE_ELEM(buff, AI_SHAPE_WIDTH) |
the width dimension |
AI_BUFFER_SHAPE_ELEM(buff, AI_SHAPE_HEIGHT) |
the height dimension |
AI_BUFFER_SHAPE_ELEM(buff, AI_SHAPE_CHANNEL) |
the channel
dimension |
AI_BUFFER_SHAPE_ELEM(buff, AI_SHAPE_BATCH) |
the batch dimension |
AI_BUFFER_SHAPE_ELEM(buff, AI_SHAPE_DEPTH) |
the depth dimension if
available else 0 |
AI_BUFFER_SHAPE_ELEM(buff, AI_SHAPE_EXTENSION) |
the extension dimension
if available else 0 |
Tensor format
The format of the data is mainly defined by the field
format, a 32b word (ai_buffer_format
type). 3 main types are supported.
const ai_buffer_format fmt = AI_BUFFER_FORMAT(@ai_buffer_object);| type | description |
|---|---|
AI_BUFFER_FMT_TYPE_FLOAT |
floating-point data.
mapped on a 32b float C-type (ai_float or
float). |
AI_BUFFER_FMT_TYPE_Q |
quantized data, mapped on 8b signed or unsigned integer C-type. Refer to “Quantized tensors” article, to detail the used integer arithmetic. |
AI_BUFFER_FMT_TYPE_BOOL |
boolean, mapped on 8b unsigned integer C-type |
Helper C-macros
Following set of C-macros can be used with the
format field from the struct ai_buffer
C-structure object to extract the information.
| macros | description |
|---|---|
AI_BUFFER_FMT_GET_TYPE(fmt) |
returns
AI_BUFFER_FMT_TYPE_FLOAT/AI_BUFFER_FMT_TYPE_Q
or AI_BUFFER_FMT_TYPE_BOOL buffer type. |
AI_BUFFER_FMT_GET_FLOAT(fmt) |
returns 1 if the data is
a float type else 0. |
AI_BUFFER_FMT_GET_SIGN(fmt) |
returns 1 if the data is
signed else 0. |
AI_BUFFER_FMT_GET_BITS(fmt) |
returns the total number of bit which
is used to encode the data. This is M+N+sign for
AI_BUFFER_FMT_TYPE_Q type. Available values:
32 or 8. |
AI_BUFFER_FMT_GET_FBITS(fmt) |
returns the total number of bit which is used to encode the fractional part for the 8b quantized data type. |
For supported binary format (1b signed),
AI_BUFFER_FMT_TYPE_Q is returned and the total number
of bit is 1 (AI_BUFFER_FMT_GET_BITS(fmt)).
Additional macros are defined for the meta parameters:
const ai_buffer_meta_info * meta_info = AI_BUFFER_META_INFO(@ai_buffer_object);| macros | description |
|---|---|
AI_BUFFER_META_INFO_INTQ(meta_info) |
returns the scale/zero-point meta info
(reference to ai_intq_info) if available,
NULL otherwise. |
AI_BUFFER_META_INFO_INTQ_GET_SCALE(meta_info, pos) |
returns the scale value
(ai_float) at the pos-th position if available,
0 otherwise. For the IO tensor only the position 0 is
available. |
AI_BUFFER_META_INFO_INTQ_GET_ZEROPOINT(meta_info, pos) |
returns the zero-point
(ai_i8 or ai_u8) value at the pos-th
position if available, ‘0’ otherwise. Type can be deduced from the
output of the AI_BUFFER_FMT_GET_SIGN() and
AI_BUFFER_FMT_GET_BITS() macros. |
Warning
Be aware that the meta_info field is only available
through the returned ai_network_report() structure,
Otherwise the value defined by the generated
AI_<NAME>_IN/OUT C-define are
NULL.
Following code snippet shows a typical code to extract the
scale and zero_point values:
#include "network.h"
static ai_handle network;
{
/* Get the descriptor of the first input tensor (index 0) */
const ai_buffer *ai_input = ai_network_inputs_get(network, NULL);
const ai_buffer *ai_input_1 = &ai_input[0];
/* Extract format of the tensor */
const ai_buffer_format fmt_1 = AI_BUFFER_FORMAT(ai_input_1);
/* Extract the data type */
const uint32_t type = AI_BUFFER_FMT_GET_TYPE(fmt_1); /* -> AI_BUFFER_FMT_TYPE_Q */
/* Extract sign and number of bits */
const ai_size sign = AI_BUFFER_FMT_GET_SIGN(fmt_1); /* -> 1 or 0*/
const ai_size bits = AI_BUFFER_FMT_GET_BITS(fmt_1); /* -> 8 */
/* Extract scale/zero_point values (only pos=0 is currently supported, per-tensor) */
const ai_float scale = AI_BUFFER_META_INFO_INTQ_GET_SCALE(ai_input_1->meta_info, 0);
const int zero_point = AI_BUFFER_META_INFO_INTQ_GET_ZEROPOINT(ai_input_1->meta_info, 0);
...
}Floating-point case:
#include "network.h"
{
/* Get the descriptor of the first input tensor (index 0) */
const ai_buffer *ai_input = ai_network_inputs_get(network, NULL);
const ai_buffer *ai_input_1 = &ai_input[0];
/* Retrieve format of the first input tensor (index 0) */
const ai_buffer_format fmt_1 = AI_BUFFER_FORMAT(ai_input_1);
/* Retrieve the data type */
const uint32_t type = AI_BUFFER_FMT_GET_TYPE(fmt_1); /* -> AI_BUFFER_FMT_TYPE_FLOAT */
/* Retrieve sign/size values */
const ai_size sign = AI_BUFFER_FMT_GET_SIGN(fmt_1); /* -> 1 */
const ai_size bits = AI_BUFFER_FMT_GET_BITS(fmt_1); /* -> 32 */
const ai_size N = AI_BUFFER_FMT_GET_FBITS(fmt_1); /* -> 0 */
...
}Life-cycle of the IO tensors
When the input buffers and output buffers are passed to the ai_<name>_run() function,
the caller should wait the end of the inference to re-use the
associated memory segments. There is no default mechanism to notify
the application that the input tensors are released or no more used
by the c-inference engine. However, in the case where an input
buffer is allocated in the user space the Platform Observer API can be
used to be notified when the operator has finished (see “End-of-process
input buffer notification” section).
Base address of the IO buffers
Following code snippet illustrates the minimum requested
instructions to retrieve the effective address of the buffer from
the activations buffer. If the --allocate-inputs (or
--allocate-outputs) option is not used,
NULL is returned. Note that the instance should be
previously fully initialized, because
the returned address is dependent on the base address of the
activations buffer.
#include "network.h"
static ai_handle network;
#if defined(AI_NETWORK_INPUTS_IN_ACTIVATIONS)
static ai_u8 *in_data_1;
#else
/* Buffer should be allocated by the application
in this case: ai_input_1->data == NULL */
static ai_u8 in_data_1[AI_NETWORK_IN_1_SIZE_BYTES];
#endif
{
const ai_buffer *ai_input = ai_network_inputs_get(network, NULL);
const ai_buffer *ai_input_1 = &ai_input[0];
#if defined(AI_NETWORK_INPUTS_IN_ACTIVATIONS)
/* Set the descriptor of the first input tensor (index 0) */
/* Retrieve the @ of the input buffer */
in_data_1 = (ai_u8 *)ai_input_1->data;
#endif
...
}float32 to 8b data type conversion
Following code snippet illustrates the float
(ai_float) to integer
(ai_i8/ai_u8) format conversion. Input
buffer is used as destination buffer.
#include <network.h>
#define _MIN(x_, y_) \
( ((x_)<(y_)) ? (x_) : (y_) )
#define _MAX(x_, y_) \
( ((x_)>(y_)) ? (x_) : (y_) )
#define _CLAMP(x_, min_, max_, type_) \
(type_) (_MIN(_MAX(x_, min_), max_))
#define _ROUND(v_, type_) \
(type_) ( ((v_)<0) ? ((v_)-0.5f) : ((v_)+0.5f) )
const ai_buffer *get_input_desc(idx)
{
const ai_buffer *ai_input = ai_network_inputs_get(network, NULL);
return &ai_input[idx];
}
ai_float input_f[AI_<NAME>_IN_1_SIZE];
ai_i8 input_q[AI_<NAME>_IN_1_SIZE]; /* or ai_u8 */
{
const ai_buffer *input = get_input_desc(0);
ai_float scale = AI_BUFFER_META_INFO_INTQ_GET_SCALE(input->meta_info, 0);
const ai_i32 zp = AI_BUFFER_META_INFO_INTQ_GET_ZEROPOINT(input->meta_info, 0);
scale = 1.0f / scale;
/* Loop */
for (int i=0; i < AI_<NAME>_IN_1_SIZE; i++)
{
const ai_i32 tmp_ = zp + _ROUND(input_f[i] * scale, ai_i32);
/* for ai_u8 */
input_q[i] = _CLAMP(tmp_, 0, 255, ai_u8);
/* for ai_i8 */
input_q[i] = _CLAMP(tmp_, -128, 127, ai_i8);
}
...
}8b to float32 data type conversion
Following code snippet illustrates the integer
(ai_i8/ai_u8) to float
(ai_float) format conversion. The output buffer is used
as source buffer.
#include <network.h>
ai_i8 output_q[AI_<NAME>_OUT_1_SIZE]; /* or ai_u8 */
ai_float output_f[AI_<NAME>_OUT_1_SIZE];
const ai_buffer *get_output_desc(idx)
{
const ai_buffer *ai_input = ai_network_outputs_get(network, NULL);
return &ai_input[idx];
}
{
const ai_buffer *output = get_output_desc(0);
ai_float scale = AI_BUFFER_META_INFO_INTQ_GET_SCALE(output->meta_info, 0);
const ai_i32 zp = AI_BUFFER_META_INFO_INTQ_GET_ZEROPOINT(output->meta_info, 0);
/* Loop */
for (int i=0; i<AI_<NAME>_OUT_1_SIZE; i++)
{
output_f[i] = scale * ((ai_float)(output_q[i]) - zp);
}
...
}C-memory layouts
To store the elements of the different tensors, standard
C-array-of-array struct are used. For the float and
integer data-type, the associated c-type is used. For
the bool type, value is stored as uint8_t
while for binary tensor, to optimize the size, values are packed on
the 32b words (see “c-layout of the s1
type” section for more details).
Note
Note that 'BHWC' data format (or ‘channel-last’) is
used for illustration but for BCHW data format (or
‘channel-first’), C-memory layout respects the same principle.
1d-array tensor
For a 1-D tensor, standard C-array type with the following memory layout is expected to handle the input and output tensors.
#include "network.h"
#define xx_SIZE VAL /* = H * W * C = C */
ai_float xx_data[xx_SIZE]; /* n_batch = 1, height = 1,
width = 1, channels = C */
ai_float xx_data[B * xx_SIZE]; /* n_batch = B, height = 1,
width = 1, channels = C */
ai_float xx_data[B][xx_SIZE];2d-array tensor
For a 2-D tensor, standard C-array-of-array memory arrangement is used to handle the input and output tensors. 2-dim are mapped to the first two dimensions of the tensor in the original toolbox representation: e.g. H and C in Keras / Tensorflow.
#include "network.h"
#define xx_SIZE VAL /* = H * W * C = H * C */
ai_float xx_data[xx_SIZE]; /* n_batch = 1, height = H,
width = 1, channels = C */
ai_float xx_data[H][C];
ai_float xx_data[B * xx_SIZE]; /* n_batch = B, height = H,
width = 1, channels = C */
ai_float xx_data[B][H][C];3d-array tensor
For a 3D-tensor, standard C-array-of-array-of-array memory arrangement is used to handle the input and output tensors.
#include "network.h"
#define xx_SIZE VAL /* = H * W * C */
ai_float xx_data[xx_SIZE]; /* n_batch = 1, height = H,
width = W, channels = C */
ai_float xx_data[H][W][C];
ai_float xx_data[B * xx_SIZE]; /* n_batch = B, height = H,
width = W, channels = C */
ai_float xx_data[B][H][W][C];