2.0.0
ST Edge AI Core for MLC


ST Edge AI Core

ST Edge AI Core for MLC


for MLC target, based on ST Edge AI Core Technology 2.0.0




Overview

The Machine Learning Core (MLC) is an AI engine integrated into a variety of STMicroelectronics MEMS sensors that can run multiple decision trees for classification tasks using motion data (accelerometer, gyroscope) or, depending on the device, even data coming from external sources (e.g., magnetometer, vertical analog front-end, etc.).

Once a new prediction is obtained from any of the configured decision trees, the MLC can trigger an interrupt to communicate the event to a MCU/MPU that can handle it accordingly.

For more information about MLC, please explore the dedicated page available on the ST website: MEMS Sensors Ecosystem for Machine Learning.

Development flow

The flow for developing and validating AI solutions for MLC-based devices is composed of the following steps:

  1. Feature extraction: MLC feature computation from raw data logs
  2. Model training: Decision tree training using extracted features
  3. Sensor configuration: Generation of MLC sensor configuration
  4. Performance analysis: Simulation of decision tree performance
  5. Validation on target: Validation on target using ProfiMEMS evaluation board

Feature extraction

To ensure a correct model training, the features comprising the training set must be aligned 1:1 to the MLC hardware. For this reason, ST Edge AI Core enables an extra generation step for automatically extracting the features from data logs acquired using ST MEMS software tools (e.g., MEMS-Studio, Unico-GUI, Unicleo-GUI)

This is done using an MLC generation script (in .json format) containing all settings needed for extracting the features. An example of MLC generation script can be found below:

{
    "datalogs": [
        { "filename": "data/stationary.csv", "label": "stationary" },
        { "filename": "data/walking.csv",    "label": "walking"    },
        { "filename": "data/cycling.csv",    "label": "cycling"    },
        { "filename": "data/running.csv",    "label": "running"    },
        "..."
    ],
    "name": "LSM6DSV16X",
    "mlc_odr": "30 Hz",
    "input_type": "accelerometer_only",
    "accelerometer_fs": "8 g",
    "accelerometer_odr": "30 Hz",
    "decision_tree_count": 1,
    "window_length": 60,
    "filters": [
        { "filter_id": "filter_1", "filter_type": "BP", "input": "Acc_V2", "a2": "-1.66", "a3": "0.81", "gain": "0.09" },
        "..."
    ],
    "features": [
        { "feature_name": "MEAN", "input": "Acc_V2",         },
        { "feature_name": "MEAN", "input": "Acc_V2_filter_1" },
        "..."
    ],
    "arff": "features.arff"
}

For more information on the MLC generation script, please follow the link to the dedicated article: How to write an MLC generation script.

By providing the script to the generate command, ST Edge AI Core will extract all the features in .arff format:

$ stedgeai generate --target mlc --device lsm6dsv16x --json conf.json --type arff

Model training

After generating the features, the data can now be loaded inside the ML framework of choice (e.g., Python, MATLAB, Weka, etc.) for model training and or data science tasks. The following snippet of code shows how this can be achieved using Python:

# Import dependencies
import numpy as np
import pandas as pd
from scipy.io import arff
from sklearn.model_selection import train_test_split
from sklearn.tree import DecisionTreeClassifier, export_text

# Load labels and features from ARFF
arff_data = arff.loadarff("features.arff")
df = pd.DataFrame(arff_data[0])
X = df.drop("class", axis=1).values.astype(np.float32)
y = np.array([LABELS.index(label.decode()) for label in df["class"]])
feature_names = list(df.drop("class", axis=1).columns)

# Split dataset into train set and test set
X_train, X_test, y_train, y_test = train_test_split(X, y, stratify=y, test_size=0.3)

# Train decision tree classifer
clf = DecisionTreeClassifier(
    max_depth=128,
    criterion="entropy",
    min_impurity_decrease=1e-3,
    ccp_alpha=1e-2,
    class_weight="balanced",
)
clf.fit(X_train, y_train)

# Define utility function for weka format conversion
def convert_sklearn_to_weka(clf, feature_names):
    dt = re.sub(r"\|--- ", r"", export_text(clf, feature_names=feature_names)).splitlines()
    new_dt = []
    line_idx = 1
    while line_idx < len(dt):
        match = re.search(r"class: (\d+)$", dt[line_idx])
        if match is not None:
            label = LABELS[int(match.group(1))]
            new_dt.append(f"{dt[line_idx - 1]}: {label}")
            line_idx += 2
        else:
            new_dt.append(dt[line_idx - 1])
            line_idx += 1
    return "\n".join(new_dt)

# Export model to weka textual format
dectree = convert_sklearn_to_weka(clf, feature_names)
with open("dectree.txt", "w") as f:
    f.write(dectree)

After the training, to proceed with the generation of the complete configuration, the user should have one or more decision tree files in Weka format. An example can be found below:

F6_ENERGY_ACC_V2_FILTER_1 <= 7.86
|   F5_ENERGY_ACC_V2 <= 62.14: stationary
|   F5_ENERGY_ACC_V2 >  62.14
|   |   F11_PEAK_DETECTOR_ACC_V2 <= 31.00
|   |   |   F5_ENERGY_ACC_V2 <= 83.12: stationary
|   |   |   F5_ENERGY_ACC_V2 >  83.12: walking
|   |   F11_PEAK_DETECTOR_ACC_V2 >  31.00
|   |   |   F11_PEAK_DETECTOR_ACC_V2 <= 37.50
|   |   |   |   F12_PEAK_DETECTOR_ACC_V2_FILTER_1 <= 17.50: stationary
|   |   |   |   F12_PEAK_DETECTOR_ACC_V2_FILTER_1 >  17.50: cycling
|   |   |   F11_PEAK_DETECTOR_ACC_V2 >  37.50: cycling
F6_ENERGY_ACC_V2_FILTER_1 >  7.86
|   F1_MEAN_ACC_V2 <= 2.92
|   |   F9_ZERO_CROSSING_ACC_V2 <= 43.00: walking
|   |   F9_ZERO_CROSSING_ACC_V2 >  43.00: cycling
|   F1_MEAN_ACC_V2 >  2.92: running

Sensor configuration

A second, and final, generation step will now use the same MLC generation script as before with some additional fields to integrate one or more decision trees. An example of MLC generation script can be found below:

{
    "dectree_features": [
        "F1_MEAN_ACC_V2",
        "F2_MEAN_ACC_V2_FILTER_1",
        "..."
    ],
    "dectrees": [
        {
            "filename": "dectree.txt",
            "results": [
                { "label": "stationary", "value": 1  },
                { "label": "walking",    "value": 4  },
                { "label": "cycling",    "value": 8  },
                { "label": "running",    "value": 12 },
            ],
            "metaclassifier": [ 2, 2, 2, 2 ]
        },
        "..."
    ],
    "ucf": "mlc_conf.ucf"
}

For more information on the MLC generation script, please follow the link to the dedicated article: How to write an MLC generation script.

By running the generate command again with the updated script, we can now generate the .ucf file containing the register map of the sensor:

$ stedgeai generate --target mlc --device lsm6dsv16x --json conf.json --type ucf

A C header file (.h) containing the same register map is also generated in the output folder to ease the integration inside the firmware of the MCU/MPU used for configuring the sensor at runtime.

Performance analysis

By using the analyze command, ST Edge AI Core can execute the MLC logic offline by inputting features (extracted previously using the generate command) inside a given decision tree with optional metaclassifier stage to obtain the final predictions:

$ stedgeai analyze --target mlc --device lsm6dsv16x --tree dectree.txt --arff features.arff --meta meta.txt

where meta.txt configures the metaclassifier stage by specifying rows with: class name, metaclassifier end counter, and metaclassifier subgroup. For example:

stationary 2 0
walking 2 1
running 2 2
cycling 2 3

For more information on metaclassifier please refer to the MLC application note of the specific device, e.g., MLC application note for LSM6DSV16X sensor.

In addition to generating raw MLC prediction logs, a report summarizing decision tree information and predictive performance is also generated:

ST Edge AI Core v2.0.0 (MLC 1.1.0)
Created date   : YYYY-MM-DD hh:mm:ss
Parameters     : analyze --target mlc --device lsm6dsv16x --tree dectree.txt --arff features.arff --meta meta.txt

Exec/report summary (analyze)
--------------------------------------------------------------------------------
target/series  : mlc
device name    : LSM6DSV16X
decision tree  : /path/to/workspace/dectree.txt
arff features  : /path/to/workspace/features.arff
metaclassifier : /path/to/workspace/meta.txt
output dir     : /path/to/workspace/mlc_ai_output
--------------------------------------------------------------------------------

Running the simulation...

Features used:
    F1_MEAN_ACC_V2
    F5_ENERGY_ACC_V2
    F6_ENERGY_ACC_V2_FILTER_1
    F9_ZERO_CROSSING_ACC_V2
    F11_PEAK_DETECTOR_ACC_V2
    F12_PEAK_DETECTOR_ACC_V2_FILTER_1

Decision tree info:
    Nodes  : 17
    Leaves : 9
    Depth  : 6

Results before meta-classifier:
    Class "stationary" accuracy  : 98.848053 %
                       recall    : 98.504272 %
                       precision : 97.052635 %
    Class "walking"    accuracy  : 99.012619 %
                       recall    : 98.933899 %
                       precision : 97.274628 %
    Class "cycling"    accuracy  : 99.122330 %
                       recall    : 96.868011 %
                       precision : 99.540230 %
    Class "running"    accuracy  : 99.725731 %
                       recall    : 99.088837 %
                       precision : 99.770645 %

    Global accuracy : 98.354362 %

              stationary (T)    walking (T)    cycling (T)    running (T)
stationary    461               4              10             0          
walking       5                 464            4              4          
cycling       2                 0              433            0          
running       0                 1              0              435        

Results after meta-classifier:
    Class "stationary" accuracy  : 99.780342 %
                       recall    : 100.000000 %
                       precision : 99.148933 %
    Class "walking"    accuracy  : 99.615601 %
                       recall    : 99.360344 %
                       precision : 99.148933 %
    Class "cycling"    accuracy  : 99.615601 %
                       recall    : 98.434006 %
                       precision : 100.000000 %
    Class "running"    accuracy  : 99.450851 %
                       recall    : 99.088837 %
                       precision : 98.639458 %

    Global accuracy : 99.231186 %

              stationary (T)    walking (T)    cycling (T)    running (T)
stationary    466               3              1              0          
walking       0                 466            0              4          
cycling       0                 0              440            0          
running       0                 0              6              435

Validation on target

Alternatively, ST Edge AI Core also supports validation on target using ProfiMEMS Evaluation Board and DIL-24 adapters with the MLC-based sensor of choice, e.g., DIL-24 adapter for LSM6DSV16X sensor.

Before using the ProfiMEMS board for MLC validation, the user must flash the correct firmware and insert the sensor adapter into the DIL-24 slot. For these steps, please refer to the ProfiMEMS board user manual By connecting the board via USB to a PC, the validate command can be used for loading the .ucf configuration and inject any data log inside the sensor to obtain MLC predictions:

$ stedgeai validate --target mlc --device lsm6dsv16x --ucf mlc_conf.ucf --logs testset.csv --ignore-zero

Again, in addition to generating raw MLC prediction logs, a report summarizing the overall performance is also generated:

ST Edge AI Core v1.0.0-A1 (MLC 1.1.0)
Created date  : YYYY-MM-DD hh:mm:ss
Parameters    : validate --target mlc --device lsm6dsv16x --ucf mlc_conf.ucf --logs testset.csv --ignore-zero

Exec/report summary (validate)
--------------------------------------------------------------------------------
target/series : mlc
device name   : LSM6DSV16X
ucf file      : /path/to/workspace/mlc_conf.ucf
output dir    : /path/to/workspace/mlc_ai_output
logs dir/file : /path/to/workspace/testset.csv
--------------------------------------------------------------------------------

Computing the metrics...
Accuracy report for decision tree 0
--------------------------------------------------------------------------------
notes: - computed against the provided ground truth values
       - 5880 samples (4 items per sample)
       - C0 may also indicates the initial state of DT0

acc: 100.00%, rmse: 0.0, mae: 0.0, l2r: 0.0, mean: 0.0, std: 0.0, nse: 1.0, cos: 1.0

4 classes (5880 samples)
----------------------------
C1       1620   .    .    .  
C4         .  1440   .    .  
C8         .    .  1560   .  
C12        .    .    .  1260

acc  : Classification accuracy (all classes)
rmse : Root Mean Squared Error
mae  : Mean Absolute Error
l2r  : L2 relative error
nse  : Nash-Sutcliffe efficiency criteria
cos  : Cosine similarity

Command line interface

$ stedgeai --target mlc --help
usage: stedgeai [--target STR] [--output DIR] --device DEVICE [--script FILE]
                [--json FILE] [--type {arff,ucf}] [--port COM] [--ucf FILE]
                [--logs FILE | DIR] [--ignore-zero] [--tree FILE] [--arff FILE]
                [--meta FILE] [--no-report] [--help] [--version] [--tools-version]
                [--verbosity [{0,1}]]
                generate|validate|analyze

ST Edge AI Core v1.0.0-A1 (MLC 1.1.0)
...

Command

Type of command to execute, must be specified first. Available commands for MLC target:

analyze

analyze MLC model performance by inputting extracted features into a given decision tree with metaclassifier stage to compute the predictions

validate

validate MLC sensor configuration on real-hardware by using data injection (requires ProfiMEMS board with sensor adapter)

generate

extract MLC features from data logs or generate MLC sensor configuration

Common options

--target STR

target selector

--output DIR, -o DIR

folder where the generated files are saved (default: mlc_ai_output)

--device DEVICE

MLC-capable device name, choose one from:

  • ASM330LHB
  • ASM330LHBG1
  • ASM330LHHX
  • ASM330LHHXG1
  • IIS2ICLX
  • ISM330BX
  • ISM330DHCX
  • LIS2DUX12
  • LIS2DUXS12
  • LSM6DSO32X
  • LSM6DSOX
  • LSM6DSRX
  • LSM6DSV16BX
  • LSM6DSV16X
  • LSM6DSV32X
  • ST1VAFE3BX
  • ST1VAFE6AX

Specific generate options

--script FILE

generation script file (legacy)

--json FILE

generation JSON file (ignored if –script is specified)

--type {arff,ucf}

generation output type (required if –json is specified)

Specific validate options

--port COM

serial port where ProfiMEMS board is connected (default: automatic discovery)

--ucf FILE

UCF sensor configuration

--logs FILE | DIR

single log file or directory containing log files

--ignore-zero

ignore label value ‘0’ in metrics computations

Specific analyze options

--tree FILE

decision tree file in Weka format

--arff FILE

ARFF file containing extracted features

--meta FILE

loads a metaclassifier file where each row must specify:

  1. class name
  2. metaclassifier end counter
  3. metaclassifier subgroup

Additional options

--no-report

do not generate the report file

--help, -h

show this help message and exit

--version

print the version of the tool

--tools-version

print the versions of the third party packages used by the tool

--verbosity [{0,1}], --verbose [{0,1}], -v [{0,1}]

set verbosity level

Examples

$ stedgeai analyze  --target mlc --device lsm6dsv16x --tree mytree.txt --arff myfeatures.arff
$ stedgeai validate --target mlc --device lsm6dsv16x --ucf myconf.ucf --logs test_data.csv
$ stedgeai generate --target mlc --device lsm6dsv16x --json myscript.json --type arff
$ stedgeai generate --target mlc --device lsm6dsv16x --json myscript.json --type ucf -o output_dir

Application examples

A curated list of MLC application examples ready to be used in all MLC-based sensors can be found at the following GitHub repository.

This list comprises of various MLC configurations targeting: consumer, industrial, and automotive applications.