2.0.0
ST Edge AI Core for STELLAR MCUs


ST Edge AI Core

ST Edge AI Core for STELLAR MCUs


for STELLAR target, based on ST Edge AI Core Technology 2.0.0



r2.0

Overview

The article describes the specificities of the command line for the Stellar (E or P or G) target when used in the Stellar Studio environment.
A Stellar Studio AI SDK (Stellar-E or Stellar-PG) based project requires the full Stellar Studio ecosystem with the Stellar SDKs, TOOLS and the ST Edge AI software packages installation. Please refer always to the latest available versions of all the Stellar Studio ecosystem tools.

Comparison with the STELLAR STUDIO AI UI plug-in features

The stedgeai application is used as back-end by the Stellar Studio AI UI plug-in
(refer to “User manual - Getting started with Stellar Studio AI plugin for Artificial Intelligence (AI)”).

CLI as back-end

In comparison with the Stellar Studio AI UI plug-in, the following high-level features are not supported:

  • extra C-code wrapper to manage multiple models (validation refers always to only the selected network). CLI manages only one model at the time.
  • creation of a whole Stellar Studio IDE SDK based project including the optimized inference runtime library, AI headers files and the C-files related to the HW settings. CLI can be only used to generate the specialized NN C-files. However, it allows to update an initial IDE project, Stellar Studio SDK based or proprietary source tree (see “Update a stellar studio ai sdk based project” section).
  • the check to know if a model will fit, in term of memory layout in a selected Stellar memory device. CLI reports (see analyze command) only the main system level dimensioning metrics: ROM, RAM, MACC.. (refer to [[METRIC]][X_CUBE_AI_METRICS] for details)
  • for the “Validation process on target”, as a full Stellar Studio SDK based project is expected, it must be generated previously through the UI. Note that this project can be updated later (see “Update a stellar studio ai sdk based project” section). “Validation process on desktop” is fully supported through the CLI without restriction.
  • No graphic visualization of the generated c-graph. CLI provides instead a textual representation (table form) of the c-graph including a description of the tensors/operators (see analyze command).

Supported STELLAR-E series

supported series description
sr5e1 SR5 E1 line — 32 bit ARM Cortex M7 automotive electrification MCUs with FPU support enabled (double precision).

Supported STELLAR-PG series

supported series description
sr6p SR6 P line — 32 bit ARM Cortex R52+ automotive integration MCUs, Arm® v8-R compliant, with FPU support enabled (single precision). Neon™ (with SIMD, dual-precision floating point) NOT supported.

Warning

Be aware that all supported inference runtime libraries for the Stellar-E or Stellar-PG microcontrollers are compiled with the FPU enabled and the hard float EABI option for performance reasons.

Update a stellar studio ai sdk based project

For a Stellar Studio AI SDK based project, the user has the possibility to update only the generated NN C-files. In this case, the '--output' option is used to indicate the directory where to copy the new generated NN C-files.

$ stedgeai generate -m <model_path> --target stellar-e -n <name> -c low -o <nn_c_files_folder>
or
$ stedgeai generate -m <model_path> --target stellar-pg -n <name> -c low -o <nn_c_files_folder>

Generated files (7)
-----------------------------------------------------------
 <nn_c_files_folder>\inc\<name>_config.h
 <nn_c_files_folder>\inc\<name>.h
 <nn_c_files_folder>\src\<name>.c
 <nn_c_files_folder>\inc\<name>_data_params.h
 <nn_c_files_folder>\src\<name>_data_params.c
 <nn_c_files_folder>\inc\<name>_data.h
 <nn_c_files_folder>\src\<name>_data.c

Creating report file <nn_c_files_folder>\<name>_generate_report.txt

OR

$ stedgeai generate -m <model_path> --target stellar-e  --c-api st-ai -n <name> -c low -o <nn_c_files_folder>
or
$ stedgeai generate -m <model_path> --target stellar-pg  --c-api st-ai -n <name> -c low -o <nn_c_files_folder>

Generated files (5)
-----------------------------------------------------------
 <nn_c_files_folder>\inc\<name>_details.h
 <nn_c_files_folder>\inc\<name>.h
 <nn_c_files_folder>\src\<name>.c
 <nn_c_files_folder>\inc\<name>_data.h
 <nn_c_files_folder>\src\<name>_data.c

Creating report file <nn_c_files_folder>\<name>_generate_report.txt
...

For multiple networks support, the update mechanism for a particular model is the same. Users should be vigilant to use the correct name ('--name my_name') to avoid to overwrite/update an incorrect file and to be aligned with the multi-network helpers functions which are only generated by the Stellar Studio AI UI: '\app_stellar-studio-ai.c/.h' files. If the number of networks is changed, Stellar Studio AI UI should be used to update the generated c-models.