Embedded ST Neural ART API
for STM32 target, based on ST Edge AI Core Technology 2.0.0
r1.0
Overview
This article describes the embedded inference client API and
associated runtime software stack. The C-application must use this
stack to utilize the specialized or configuration files generated by
the ST Neural ART
compiler. Referred to as the 'network.c' file in
this article, it contains a series of steps (formally named epochs)
to perform inference using the ST
Neural-ART NPU as much as possible.
As descripted in the “ST Neural-ART NPU concepts” article (“Scheduling” section), each epoch is decomposed into three phases:
- Preparation of the epoch: pre-op phase
- Execution of the epoch: hw-op phase
- Cleanup of the epoch: post-op phase
The 'network.c' file contains code that outlines the
actions to be performed in each step (epoch). To make this
configuration file useful in an embedded C project, a comprehensive
and efficient NPU runtime
software stack is provided. This stack referred to as
'll_aton', supports various platforms through a simple
OSAL/port layer and offers numerous options to optimize execution
for different use cases.
This article presents the ll_aton API, and some of
the important options that can be used.
ll_aton source location
$STEDGEAI_CORE_DIR/Middlewares/ST/AI/Npu/ll_aton /* generic files */
$STEDGEAI_CORE_DIR/Middlewares/ST/AI/Npu/Devices/STM32N6XX /* STM32N6-specific files */
%STEDGEAI_CORE_DIR%indicates the root location where the ST Edge AI Core components are installed.
Layered stack
Model instance
For a given model, tracking the current status of an inference requires describing each network with an instance. This approach is crucial for efficiently managing use cases where multiple networks need to be executed.
A model instance has the following type:
typedef struct
{
const NN_Interface_TypeDef *network;
NN_Execution_State_TypeDef exec_state;
} NN_Instance_TypeDef;
// with
typedef struct
{
const char *network_name;
NN_EpochBlockItems_TypeDef epoch_block_items;
NN_Buffers_Info_TypeDef output_buffers_info;
NN_Buffers_Info_TypeDef input_buffers_info;
NN_Buffers_Info_TypeDef internal_buffers_info;
} NN_Interface_TypeDef;
// and
typedef struct
{
const EpochBlock_ItemTypeDef *volatile current_epoch_block; // pointer to current epoch block
const EpochBlock_ItemTypeDef *volatile first_epoch_block; // pointer to first epoch block in current epoch list
const EpochBlock_ItemTypeDef *volatile next_epoch_block; // pointer to epoch block to be inserted
const EpochBlock_ItemTypeDef *volatile saved_current_epoch_block; // pointer to saved current epoch list
const EpochBlock_ItemTypeDef
*volatile saved_first_epoch_block; // pointer to saved first epoch block in current epoch list
#if (LL_ATON_RT_MODE == LL_ATON_RT_ASYNC)
volatile uint32_t triggered_events; // currently triggered events/IRQs in current epoch
volatile bool current_epoch_block_started; // has current epoch block already been started
#endif // (LL_ATON_RT_MODE == LL_ATON_RT_ASYNC)
TraceEpochBlock_FuncPtr_t epoch_callback_function; // epoch callback function
} NN_Execution_State_TypeDef;In short, the instance struct is one of the main entrypoints to get information on a network and its current execution state.
Such structures are needed as arguments for most of the runtime-level functions.
How to instantiate a model
To ease definition of an instance, the
'll_aton_NN_interface.h' file provides macros to handle
all the operations to be done easily.
To use these macros, one must know the “name” of the network to
use. It has been either forced during compilation of the network
through the ST Neural-ART compiler or is “Default” by default. (In
the 'network.c' file, some symbols are suffixed by the
name of the network, for example,
'LL_ATON_EpochBlockItems_Default' describe epochs for
the “Default” network).
The use of the macros is as follows:
// "Default" should be replaced by the name of the network.
// Defines NN_Instance_Default and NN_Interface_Default with network.c informations
LL_ATON_DECLARE_NAMED_NN_INSTANCE_AND_INTERFACE(Default) Runtime layer
As already presented, this layer provides the main functions to use to perform an inference.
LL_ATON_RT_RuntimeInit()
void LL_ATON_RT_RuntimeInit(void);
void LL_ATON_RT_RuntimeDeInit(void);The init function shall always be called once whenever using this runtime, before performing any operation.
Mainly, this
- Initializes the ST Neural-ART NPU to a known-state
- Initializes the
ll_atonruntime to a known-state- Calling initialization functions if an OS should be used
- Configuring IRQ handling correctly
As obvious as it may sound, the DeInit function can be used to clean up the initializations done above.
LL_ATON_RT_Init_Network()
void LL_ATON_RT_Init_Network(NN_Instance_TypeDef *nn_instance);
void LL_ATON_RT_DeInit_Network(NN_Instance_TypeDef *nn_instance);This is again an initialization/deinitialization functions, this time used to set up the instance structures.
Here again, the init function shall be called before doing any inference to ensure that the instance is in a known state (this is the only goal of this function, make the instance clean and initialize all fields correctly). And the DeInit can be used to clear up everything done (for example, to make the instance unusable, unrunnable).
It is to be noted that the function
void LL_ATON_RT_Reset_Network(NN_Instance_TypeDef *nn_instance);
can be used to “rewind” an initialized instance. This ensures that
the instance is ready to perform a new inference.
LL_ATON_RT_RetValues_t LL_ATON_RT_RunEpochBlock()
LL_ATON_RT_RetValues_t LL_ATON_RT_RunEpochBlock(NN_Instance_TypeDef *nn_instance);Whenever an instance has been initialized, it is possible to start performing an inference with it.
LL_ATON_RT_RunEpochBlock is called to trigger
execution of the “next epoch” of the current instance.
That means that, to perform a full inference, it is needed to call
this function at least as much time as the number of epochs.
Whenever called, this function automatically updates the fields
of the instance structure passed as an argument.
It has two main roles:
- If the epoch is not started, it starts it
- If the epoch is already running, it returns the current epoch
execution status:
LL_ATON_RT_NO_WFE: The next epoch block may be started:LL_ATON_OSAL_WFE()is not called.LL_ATON_RT_WFE: Epoch block is still running:LL_ATON_OSAL_WFE()can be safely called.LL_ATON_RT_DONEInference is over.
LL_ATON_RT_Main()
void LL_ATON_RT_Main(NN_Instance_TypeDef *network_instance);This function provides a template that shows the major steps to do whenever doing an inference. As stated, the functions presented above are the main ones to use to perform an inference, this template shows how to order them correctly.
A full execution template is also provided in this article, where the major steps are also found.
void LL_ATON_RT_Main(NN_Instance_TypeDef *network_instance)
{
LL_ATON_RT_RetValues_t ll_aton_rt_ret;
/*** Start of user initialization code ***/
/*** End of user initialization code ***/
assert(network_instance != NULL);
assert(network_instance->network != NULL);
LL_ATON_RT_RuntimeInit(); // Initialize runtime
LL_ATON_RT_Init_Network(network_instance); // Initialize passed network instance object
do
{
/* Execute first/next step of Cube.AI/ATON runtime */
ll_aton_rt_ret = LL_ATON_RT_RunEpochBlock(network_instance);
/*** Start of user event handling code ***/
/*** End of user event handling code ***/
/* Wait for next event */
if (ll_aton_rt_ret == LL_ATON_RT_WFE)
{ /*** subject to change to fit also user code requirements ***/
LL_ATON_OSAL_WFE();
}
} while (ll_aton_rt_ret != LL_ATON_RT_DONE); /*** subject to change to fit also user code requirements ***/
LL_ATON_RT_DeInit_Network(network_instance); // De-initialize the network instance object
LL_ATON_RT_RuntimeDeInit(); // De-initialize runtime
/*** Start of user de-initialization code ***/
/*** End of user de-initialization code ***/
}LL_ATON_RT_SetEpochCallback()
void LL_ATON_RT_SetEpochCallback(TraceEpochBlock_FuncPtr_t epoch_block_callback, NN_Instance_TypeDef *nn_instance);
void LL_ATON_RT_SetRuntimeCallback(TraceRuntime_FuncPtr_t rt_callback);The runtime environment provides a callback mechanism that allows to follow the setup and the execution of a network; the available callbacks are the following:
- runtime callback: when enabled it is called on each runtime initialization or deinitialization operation
- epoch callback: when enabled it is called on each network, initialization, deinitialization, or execution
The default values of callback function pointers are NULL and can be set using the following functions:
LL_ATON_RT_SetRuntimeCallbackLL_ATON_RT_SetEpochCallback
In particular, the epoch callback can be useful to follow and debug the execution steps of a neural network; for example, it is possible to measure epoch timing or to dump intermediate activations. The epoch call function is called with the following parameters:
ctype: callback type. It can have the following values:LL_ATON_RT_Callbacktype_PRE_START: first in-epoch execution step (called just before epoch preparation steps)LL_ATON_RT_Callbacktype_POST_START: second in-epoch execution step (called just after epoch preparation steps)LL_ATON_RT_Callbacktype_PRE_END: third in-epoch execution step (called just before epoch cleanup steps)LL_ATON_RT_Callbacktype_POST_END: fourth (and last) in-epoch execution step (called just after epoch cleanup steps)LL_ATON_RT_Callbacktype_NN_Init: network initialization or resetLL_ATON_RT_Callbacktype_NN_DeInit: network deinitializationLL_ATON_RT_Callbacktype_RT_Init: valid only for runtime callbackLL_ATON_RT_Callbacktype_RT_Deinit: valid only for runtime callback
nn_instance: instance of the networkeb: current execution block info
The following code shows an example:
...
// Epoch callback setup
LL_ATON_RT_SetEpochCallback ( EpochBlock_TraceCallBack , nn_instance_pnt ) ;
....
void EpochBlock_TraceCallBack ( LL_ATON_RT_Callbacktype_t ctype , const NN_Instance_TypeDef *nn_instance , const EpochBlock_ItemTypeDef *eb )
{
switch ( ctype ) {
case LL_ATON_RT_Callbacktype_PRE_START :
TOGGLE_EPOCH_PIN ; // Trace epoch pin for oscilloscope
break ;
case LL_ATON_RT_Callbacktype_POST_END :
// If needed dump intermediate activations
checkEpochOutputs ( eb -> epoch_num ) ;
break ;
case LL_ATON_RT_Callbacktype_NN_Init :
// Capture network start time
inferenceBaseTime = dwtGetCycles() ;
break ;
default :
return ;
break ;
} /* endswitch */
} // end of EpochBlock_TraceCallBack() function
void checkEpochOutputs ( uint32_t epochNum )
{
for ( int idx = 0 ; idx < bufferListlen ; idx++ ) {
if ( bufferList [ idx ] -> epoch == epochNum ) {
// print the activations info and/or the activation data related to the current epoch
// It is expected that bufferList and bufferListlen have been previously initialized
printBuffer ( bufferList [ idx ] ) ;
} /* endif */
} /* endfor */
} // end of checkEpochOutputs() functionWarning
When using the epoch controller many or even all epochs are
executed in a single execution step: in this case the callback
function is not called on all epochs! If needed, the network can be
compiled (using the --ec-single-epoch option) to
generate a single execution step for each epoch thus allowing to
follow the execution also with the epoch controller.
Lower-level layers
The runtime layer operates thanks to a lot of lower-layer files.
Operating System Abstraction Layer (OSAL)
ll_aton ships with interfaces for some RTOS, easing
the integration work when working in such environments.
The supported operating systems are:
- Bare Metal (no OS)
- FreeRTOS™
- ThreadX
More detail on how to set up a project in such an environment is provided in the appropriate section.
Software library interface
A library is delivered in the middleware directory of the tool. This library is known as EmbedNets. This is a purely optimized software library based on Arm Cortex®-M55 instructions and MVE extension. > REVIEW THAT
Some epochs cannot be executed by the ST Neural-ART NPU (for example, float-point operations), and there is a need to call for functions defined in EmbedNets.
The files ll_sw_float.c and
ll_sw_integer.c handles the interface with the software
library (optimized AI runtime library for Arm Corte-M family).
Stack configuration
The ST Neural-ART compiler is platform agnostic and the code
generated can then be executed with ll_aton code. When
building a firmware for a given target, options (C-defines) must be
passed to ll_aton to configure its behavior.
(See 'll_aton_config.h' file)
Mandatory options
| C-define | Description |
|---|---|
LL_ATON_PLATFORM=LL_ATON_PLAT_STM32N6 |
Forces using of the implementation of
ll_aton specific for the STM32N6 |
LL_ATON_SW_FALLBACK |
Allows the use of software epochs (otherwise any network that requires software epochs will not compile) |
LL_ATON_RT_MODE=LL_ATON_RT_ASYNC |
Enables handling of events by
Neural-ART IRQ mechanism (the other acceptable value is
LL_ATON_RT_POLLING –IRQ not handled– but this is not
advised) |
LL_ATON_OSAL=LL_ATON_OSAL_BARE_METAL |
Enables a given OSAL (Operating System
Abstraction Layer), bare metal means “no OS”. (Other possible values
include LL_ATON_OSAL_THREADX,
LL_ATON_OSAL_FREERTOS |
Useful options
| C-define | Description |
|---|---|
LL_ATON_DBG_BUFFER_INFO_EXCLUDED=1 |
Prevents shipping all buffers information with the final code (only I/O buffers are described, this makes the final firmware lighter) |
LL_ATON_EB_DBG_INFO |
Exports extra information in epoch blocks (only for debug: consumes space on the final firmware) |
LL_ATON_DUMP_DEBUG_API |
Exports functions to ease debug (for example, printing buffers through printf statements) |
LL_ATON_ENABLE_CLOCK_GATING=1 |
Enables clock gating (this is ON by
default: ll_aton powers on only parts of the Neural-ART
IP that are needed, at epoch level. This option can be set to 0 to
power-up everything, every time. Careful on the impact on power
consumption) |
Casual operations
Getting Input/Output buffers addresses
This operation is useful in many essential use cases:
- To set data in the input buffers before an inference, one must get the address of the input buffers
- To get data from the output buffers after inference, being able to get the address of the buffers is a must-have
As stated above, the network interface (or instance) is a good place to find information about a network. It is a place of choice to find information about the I/O buffers, as shown below:
// Declare/Instantiate instance
LL_ATON_DECLARE_NAMED_NN_INSTANCE_AND_INTERFACE(Default) // NN_Instance_Default, NN_Interface_Default
...
// Input buffers information are in NN_Interface_Default->input_buffers_info()
// Get address of the first input:
const LL_Buffer_InfoTypeDef * input_infos = NN_Interface_Default.input_buffers_info();
void* i0_start_address = LL_Buffer_addr_start(&input_infos[0]);
void* i0_end_address = LL_Buffer_addr_end(&input_infos[0]);
// Get address of the first output:
const LL_Buffer_InfoTypeDef * output_infos = NN_Interface_Default.output_buffers_info();
void* o0_start_address = LL_Buffer_addr_start(&output_infos[0]);
void* o0_end_address = LL_Buffer_addr_end(&output_infos[0]);Connecting I/O buffers to the network
By default, the input and output buffers are allocated by the NPU
compiler in the provided memory pools.
As shown in the
compiler description and its interaction with STEdgeAI, it is
possible to force the compiler not to generate such buffers, and let
the user allocate them. --no-inputs-allocation (resp.
--no-outputs-allocation) let the compiler not allocate
input buffers (resp. output buffers).
When this behavior is used, the generated network.c
contains functions to be used to “connect” the user-allocated
buffers to the network.
The use of those functions is as follows (for a case where only
--no-inputs-allocation has been used for example)
LL_ATON_User_IO_Result_t res;
extern LL_ATON_User_IO_Result_t LL_ATON_Set_User_Input_Buffer_Default(uint32_t num, void* buffer, uint32_t size); // defined in network.c
extern LL_ATON_User_IO_Result_t LL_ATON_Set_User_Output_Buffer_Default(uint32_t num, void* buffer, uint32_t size); // defined in network.c
// Define buffers for Inputs (the input is an RGB image, 256 x 256 x 3 x 8 bits)
uint8_t input_buff[256 * 256 * 3];
// Connect buffer to the network first input.
res = LL_ATON_Set_User_Input_Buffer_Default(0, input_buff, 256 * 256 * 3);
assert (res == LL_ATON_User_IO_NOERROR);The user is responsible for allocating correctly the buffers:
there is no way for those functions to know if the buffers are
correctly allocated, except by trusting the user for the arguments
provided.
The types and the sizes of the buffers must match what the model
expects.
Using a Real-Time Operating System (RTOS)
ll_aton comes in RTOS-flavored versions that can be
activated through LL_ATON_OSAL c-define.
When using an RTOS, the ll_aton is mainly responsible
for protecting the ST Neural-ART NPU from concurrent accesses that
may cause issues (for example, if two threads are running an
inference). This is done by locking and releasing shared resources
using features of the OS (mutexes).
The two main supported RTOS are:
- ThreadX / Azure RTOS / Eclipse ThreadX -
LL_ATON_OSAL_THREADX - FreeRTOS™ -
LL_ATON_OSAL_FREERTOS
In all cases, the ll_aton:
- Adds OS-specific initialization routines (automatically called
by
LL_ATON_RT_RuntimeInit) - Redefines Wait For Event/Event generation using semaphores
- Adds specific toolings to handle multiple threads running inferences in parallel
- Tinker correct code to make interrupt work correctly with the OS
Minimal execution unit
When using an operating system, threads and epochs are scheduled according to the priorities and to the timing: the runtime ensures that the following minimal execution units are not interrupted:
- epochs
- When using epoch-controller: blobs. When using the epoch controller one or more epochs are packed into a “blob”, a set of instruction scheduled by the epoch controller. If all epochs of a network have been packed into a single blob the network will be executed in one shot.
ThreadX
To enable the use of ThreadX:
- Add ThreadX to the project
- Add
ll_aton_osal_threadx.cto the project - Define
LL_ATON_OSAL=LL_ATON_OSAL_THREADX - Define
TX_HAS_PARALLEL_NETWORKSsymbol:TX_HAS_PARALLEL_NETWORKS=0if only one thread is running an inference on the NPUTX_HAS_PARALLEL_NETWORKS=1if multiple threads are running an inference
- Ensure
LL_ATON_RT_MODE=LL_ATON_RT_ASYNCis set - Use the LL_ATON_OSAL_WFE macro in place of the _WFE in the network execution loop
- Use networks with separated memory spaces
FreeRTOS™
To enable the use of FreeRTOS:
- Add FreeRTOS™ suite to the project
- Add
ll_aton_osal_freertos.cto the project - Define
LL_ATON_OSAL=LL_ATON_OSAL_FREERTOS - Define
TX_HAS_PARALLEL_NETWORKSsymbol:FREERTOS_HAS_PARALLEL_NETWORKS=0if only one thread is running an inference on the NPUFREERTOS_HAS_PARALLEL_NETWORKS=1if multiple threads are running an inference
- Ensure
LL_ATON_RT_MODE=LL_ATON_RT_ASYNCis set - Use the LL_ATON_OSAL_WFE macro in place of the _WFE in the network execution loop
- Use networks with separated memory spaces
Global tips
- It is possible to implement one’s own port for a given OS, by
using
LL_ATON_OSAL=LL_ATON_OSAL_USER_IMPLand creating a filell_aton_osal_user_impl.hcontaining the custom implementations needed byll_aton. The macros to be defined are listed inll_aton_osal.h. - Careful when doing multiple inferences in parallel to ensure that activation-buffers from an ongoing network inference do not interfere with other activation-buffers from another ongoing network inference
Example
Below is an example for FreeRTOS™, running two networks in two threads.
/* Define mutex and threads attributes */
osMutexId_t mutex_id ;
const osMutexAttr_t mutex_attr = {
"myMutex", // name of the mutex
0, // attr_bits
NULL, // memory for control block
0 // size for control block
} ;
osThreadId_t Thread1Handle;
const osThreadAttr_t Thread1_attributes = {
.name = "A",
.priority = (osPriority_t) osPriorityNormal,
.stack_size = 256 * 8
};
osThreadId_t Thread2Handle;
const osThreadAttr_t Thread2_attributes = {
.name = "B",
.priority = (osPriority_t) osPriorityNormal,
.stack_size = 256 * 8
};
// Main thread
void mainthread_func(void* arg)
{
mutex_id = osMutexNew ( &mutex_attr ) ;
if ( mutex_id == NULL ) {
while ( 1 ) ;
}
Thread1Handle = osThreadNew ( thread1_func , NULL , &Thread1_attributes ) ;
Thread2Handle = osThreadNew ( thread2_func , NULL , &Thread2_attributes ) ;
while ( 1 ) ;
}
// thread 1: intialize and handle atonn_mnist network
void thread1_func(void* arg)
{
int testok ;
void* output_buffer ;
void* input_buffer ;
int output_buffer_len ;
int input_buffer_len ;
LL_ATON_RT_RetValues_t ll_aton_rt_ret ;
LL_ATON_DECLARE_NAMED_NN_INSTANCE_AND_INTERFACE ( atonn_mnist ) ; // Network instance
/* Get Input/Output buffers */
input_buffer = (void*)(inbufs[0].addr_base.i + inbufs[0].offset_start);
input_buffer_len = inbufs[0].offset_end - outbufs[0].offset_start;
output_buffer = (void*)(outbufs[0].addr_base.i + outbufs[0].offset_start);
output_buffer_len = outbufs[0].offset_end - outbufs[0].offset_start;
LL_ATON_RT_Init_Network ( &NN_Instance_atonn_mnist ) ;
testok = 1 ;
while ( testok ) {
get_atonn_mnist_features ( input_buffer , input_buffer_len ) ;
LL_ATON_RT_Reset_Network ( &NN_Instance_atonn_mnist ) ;
do {
ll_aton_rt_ret = LL_ATON_RT_RunEpochBlock ( &NN_Instance_atonn_mnist ) ;
if ( ll_aton_rt_ret == LL_ATON_RT_WFE ) {
LL_ATON_OSAL_WFE();
}
} while ( ll_aton_rt_ret != LL_ATON_RT_DONE ) ;
post_process_atonn_mnist_inference ( output_buffer , output_buffer_len ) ;
}
}
void thread2_func(void* arg)
{
int testok ;
void* output_buffer ;
void* input_buffer ;
int output_buffer_len ;
int input_buffer_len ;
LL_ATON_RT_RetValues_t ll_aton_rt_ret ;
LL_ATON_DECLARE_NAMED_NN_INSTANCE_AND_INTERFACE ( atonn_mnist5x5 ) ; // Network instance
/* Get Input/Output buffers */
const LL_Buffer_InfoTypeDef *inbufs = LL_ATON_Input_Buffers_Info_atonn_mnist5x5();
const LL_Buffer_InfoTypeDef *outbufs = LL_ATON_Output_Buffers_Info_atonn_mnist5x5();
input_buffer = (void*)(inbufs[0].addr_base.i + inbufs[0].offset_start);
input_buffer_len = inbufs[0].offset_end - outbufs[0].offset_start;
output_buffer = (void*)(outbufs[0].addr_base.i + outbufs[0].offset_start);
output_buffer_len = outbufs[0].offset_end - outbufs[0].offset_start;
LL_ATON_RT_Init_Network ( &NN_Instance_atonn_mnist5x5 ) ;
testok = 1 ;
while ( testok ) {
get_atonn_mnist5x5_features ( input_buffer , input_buffer_len ) ;
LL_ATON_RT_Reset_Network ( &NN_Instance_atonn_mnist5x5 ) ;
do {
ll_aton_rt_ret = LL_ATON_RT_RunEpochBlock ( &NN_Instance_atonn_mnist5x5 ) ;
if ( ll_aton_rt_ret == LL_ATON_RT_WFE ) {
LL_ATON_OSAL_WFE();
}
} while ( ll_aton_rt_ret != LL_ATON_RT_DONE ) ;
post_process_atonn_mnist5x5_inference ( output_buffer , output_buffer_len ) ;
}
}All reference to not-reentrant function or to shared resources need to be protected with mutex:
osMutexAcquire ( mutex_id , osWaitForever ) ;
....
osMutexRelease ( mutex_id ) ;Full simple code example for running an inference, using the “ll_aton” runtime API
// Network instance declaration
LL_ATON_DECLARE_NAMED_NN_INSTANCE_AND_INTERFACE ( Default ) ;
NN_Interface_TypeDef *NN_InterfacePnt ;
NN_Instance_TypeDef *NN_InstancePnt ;
void* input_start_address ;
void* input_end_address ;
void* output_start_address ;
void* output_end_address ;
void main ( void )
{
applicationSetup() ; // system initialization
networkSetup() ;
// Enter inference loop
while ( 1 ) {
getFeature ( input_start_address ) ; // Wait for input data from somewhere
featurePreProcess ( input_start_address ) ; // Feature pre-processing (if any)
inferenceExecute ( NN_InstancePnt ) ;
inferencePostProcess ( output_start_address ) ; // Inference post-processing (if any)
} /* endwhile */
}
void networkSetup ( void )
{
LL_ATON_RT_RuntimeInit() ; // Initialize runtime
// Set references to the network "Default"
NN_InterfacePnt = (NN_Interface_TypeDef *) &NN_Interface_Default ;
NN_InstancePnt = (NN_Instance_TypeDef *) &NN_Instance_Default ;
// Initialize network
LL_ATON_RT_Init_Network ( NN_InstancePnt ) ;
// Set call back (if any)
LL_ATON_RT_SetEpochCallback ( EpochBlock_TraceCallBack , NN_InstancePnt ) ;
// Get I/O buffers addresses
const LL_Buffer_InfoTypeDef * buffersInfos = NN_InterfacePnt -> input_buffers_info();
input_start_address = LL_Buffer_addr_start(&buffersInfos[0]);
input_end_address = LL_Buffer_addr_end(&buffersInfos[0]);
buffersInfos = NN_InterfacePnt -> output_buffers_info();
output_start_address = LL_Buffer_addr_start(&buffersInfos[0]);
output_end_address = LL_Buffer_addr_end(&buffersInfos[0]);
}
int inferenceExecute ( NN_Instance_TypeDef *networkInstancePnt )
{
LL_ATON_RT_RetValues_t ll_aton_rt_ret;
if ( networkInstancePnt == NULL ) {
return ( -1 ) ;
} /* endif */
LL_ATON_RT_Reset_Network(networkInstancePnt); // Reset the network instance object
do
{
/* Execute first/next step of Cube.AI/ATON runtime */
ll_aton_rt_ret = LL_ATON_RT_RunEpochBlock(networkInstancePnt);
/* Wait for next event */
if (ll_aton_rt_ret == LL_ATON_RT_WFE)
{ /*** subject to change to fit also user code requirements ***/
LL_ATON_OSAL_WFE();
}
} while (ll_aton_rt_ret != LL_ATON_RT_DONE);
}