Setting environment for ST Edge AI Core
ST Edge AI Core Technology 2.0.0
r1.0
Overview
The ST Edge AI Core package is mainly a complete self-contained
application package. For a given target, it is recommanded to
install the associated core tool-chain and adding the directory to
the PATH environment variable.
Note
In this article, %STEDGEAI_CORE_DIR% designates the
root path where the ST Edge AI Core
components are installed.
Example for STM32 target
For the generation of a relocatable binary network (refer to “STM32 Relocatable binary
model support” article) or to evaluate the runtime memory
size, a GNU
ARM Embedded tool-chain ('arm-none-eabi-' prefix)
should be available in the PATH.
Environment settings
Windows® 10 64-bit or newer
Open a Windows command prompt
Update system
PATHvariableset PATH=%STEDGEAI_CORE_DIR%\Utilities\windows;%PATH%[ Alternative solution ] Create an alias with
doskeycommanddoskey stedgeai="%STEDGEAI_CORE_DIR%\Utilities\windows\stedgeai.exe" $*Verify the environment (displayed versions depend on installed components)
$ stedgeai --version ST Edge AI Core v2.0.0-A1 ISPU 1.1.0 MLC 1.1.0 StellarStudioAI 2.0.0 STM32CubeAI 10.0.0 STM32MP2 1.0or to have also the version of the embedded Python modules (displayed modules depend on installed components)
$ stedgeai --tools-version stedgeai - ST Edge AI Core v1.0.0 - Python version : 3.9.13 - Numpy version : 1.23.5 - TF version : 2.15.1 - TF Keras version : 2.15.0 - ONNX version : 1.15.0 - ONNX RT version : 1.18.1
Ubuntu® 20.4 and Ubuntu® 22.4 (or derived)
Similar setting of the environment is expected. A native GCC (X86_64) tool-chain should be accessible in the system path.
export PATH=$STEDGEAI_CORE_DIR/Utilities/linux:$PATH
macOS® (x64) - Minimum version High Sierra
Similar setting of the environment is expected. A native GCC (X86_64) tool-chain should be accessible in the system path.
export PATH=$STEDGEAI_CORE_DIR/Utilities/mac:$PATH