Embedded Inference Client ST Edge AI Client APIs (Migration Guidelines)
ST Edge AI Core Technology 2.0.0
r1.0
Introduction
This article describes the main guidelines to migrate an AI Client Application from former Legacy Client APIs to the new ST Edge AI embedded inference client APIs. An example of a simple client application is presented and commented.
Overview
The ST Edge AI embedded inference client APIs have been designed to be simple, portable and unified across the majority of ST devices.
New Features of ST Edge AI Embedded Client APIs
- New
STAI_XXmacros added to build and link a model using only compile time initializations. - New stai runtime with its own local context that must be initialized / de-initialized at the beginning/end of the client application to allocate/release resources related to the AI middleware.
- Support to multiple network contexts by explicitly managing the allocation of the network context.
Migrate an Legacy Client APIs App to ST Edge AI Embedded APIs
In this section the various steps required to initialize, setup and run a network model will be shown. For each step the legacy code will be presented followed by the equivalent one using new ST Edge AI Client APIs.
- Step 1: Initial Declarations and headers inclusion
This is a typical example of a beginning of a Legacy Client APIs application:
/**
******************************************************************************
* @file ai_main_app.c
* @author AST Embedded Analytics Research Platform
* @date 2024-05-23T09:23:23+0200
******************************************************************************
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
******************************************************************************
*/
#include <inttypes.h>
#include <stdio.h>
#include <string.h>
#include "ai_platform.h" /* include ai macros, types and data structures */
#include "network_inputs.h" /* where input1 buffer is defined */
#include "network.h" /* include Legacy Client APIs generated network model files */
#include "network_data_params.h"
#define LOG_PRINT(fmt, ...) \
{ printf(fmt, ##__VA_ARGS__); fflush(stdout); }
int main(int argc, char* argv[])
{
ai_handle network = AI_HANDLE_NULL;
ai_error error;
LOG_PRINT("name:%s\n", AI_NETWORK_MODEL_NAME);
LOG_PRINT("n_inputs:%d\n", AI_NETWORK_IN_NUM);
LOG_PRINT("n_outputs:%d\n", AI_NETWORK_OUT_NUM);
LOG_PRINT("activations:%d\n", AI_NETWORK_DATA_ACTIVATIONS_SIZE);
LOG_PRINT("weights:%d\n", AI_NETWORK_DATA_WEIGHTS_SIZE);
LOG_PRINT("runtime_name:X-CUBE-AI.AI\n");And this is the equivalent section using ST Edge AI Embedded Client APIs:
/**
******************************************************************************
* @file stai_main_app.c
* @author AST Embedded Analytics Research Platform
* @date 2024-05-23T10:34:45+0200
******************************************************************************
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
******************************************************************************
*/
#include <inttypes.h>
#include <stdio.h>
#include <string.h>
#include "stai.h" /* include ST Edge AI macros, types and data structures */
#include "network_inputs.h" /* where input1 buffer is defined */
#include "network.h" /* include ST Edge AI generated network model */
#define LOG_PRINT(fmt, ...) \
{ printf(fmt, ##__VA_ARGS__); fflush(stdout); }
int main(int argc, char* argv[])
{
stai_return_code return_code = STAI_SUCCESS;
LOG_PRINT("name:%s\n", STAI_NETWORK_MODEL_NAME);
LOG_PRINT("n_inputs:%d\n", STAI_NETWORK_IN_NUM);
LOG_PRINT("n_outputs:%d\n", STAI_NETWORK_OUT_NUM);
LOG_PRINT("activations:%d\n", STAI_NETWORK_ACTIVATIONS_SIZE_BYTES);
LOG_PRINT("weights:%d\n", STAI_NETWORK_WEIGHTS_SIZE_BYTES);
LOG_PRINT("runtime_name:STM.AI\n");Changes summary:
stai.hheader instead ofai_platform.his included.- Inclusion of
network_data_params.hheader is not required anymore since defines has been moved intonetwork.h - ST Edge AI Macros are used instead of former Legacy Client API
ones. As a generic rule, ST Edge AI Macros are prefixed by
STAI_instead ofAI_.
- Step 2: Runtime, model initialization (including activations allocation)
This code section will take care of defining and initializing the network context and allocate the needed activations buffers. This example allocates two memory heaps since the model has been generated enabling the multi-heap option.
Legacy Client APIs application code snippet:
/* Get activations buffer pointers array using generated macro */
ai_handle* activation_buffers = AI_NETWORK_DATA_ACTIVATIONS_TABLE_GET();
/* Allocate and set activation buffer #1 */
AI_ALIGNED(4)
ai_u8 activation1[AI_NETWORK_ACTIVATION_1_SIZE] = {0};
activation_buffers[0] = (ai_handle)(activation1);
/* Allocate and set activation buffer #2 */
AI_ALIGNED(4)
ai_u8 activation2[AI_NETWORK_ACTIVATION_2_SIZE] = {0};
activation_buffers[1] = (ai_handle)(activation2);
/* Get weights buffer pointers array using generated macro */
ai_handle* weights_buffers = AI_NETWORK_DATA_WEIGHTS_TABLE_GET();
/* A single network context is created and initialized */
error = ai_network_create_and_init(&network, activation_buffers, weights_buffers);
if (error.type != AI_ERROR_NONE) {
LOG_PRINT(" ## Test Failed executing init: type(0x%x) code(0x%x).\n\n", error.type, error.code)
return -1;
}ST Edge AI Embedded Client APIs application equivalent code snippet:
/* !New!: Declare and allocate memory for private network context instance */
STAI_NETWORK_CONTEXT_DECLARE(network, STAI_NETWORK_CONTEXT_SIZE)
/* !New!: Runtime initialization */
return_code = stai_runtime_init();
/* Initialize network context */
return_code = stai_network_init(network);
if (return_code != STAI_SUCCESS) {
LOG_PRINT(" ## Test Failed executing stai init: 0x%x.\n\n", return_code)
return -1;
}
/* Declare activations buffer pointers array */
stai_ptr activation_buffers[STAI_NETWORK_ACTIVATIONS_NUM] = {0};
/* Allocate and set activation buffer #1 */
STAI_ALIGNED(STAI_NETWORK_ACTIVATION_1_ALIGNMENT)
uint8_t activation1[STAI_NETWORK_ACTIVATION_1_SIZE] = {0};
activation_buffers[0] = (stai_ptr)(activation1);
/* Allocate and set activation buffer #2 */
STAI_ALIGNED(STAI_NETWORK_ACTIVATION_2_ALIGNMENT)
uint8_t activation2[STAI_NETWORK_ACTIVATION_2_SIZE] = {0};
activation_buffers[1] = (stai_ptr)(activation2);
/* !New!: Set network activations buffers */
return_code = stai_network_set_activations(network, activation_buffers, STAI_NETWORK_ACTIVATIONS_NUM);
if (return_code != STAI_SUCCESS) {
LOG_PRINT(" ## Test Failed executing stai set activations: 0x%x.\n\n", return_code)
return -1;
}
/* NOTE: This step is no more required now in ST Edge AI Client APIs since weights buffers are generated and bind
directly to the C model */
#if 0
/* !New!: Declare activations buffer pointers array */
stai_ptr weight_buffers[STAI_NETWORK_WEIGHTS_NUM] = {0};
stai_size n_weights = 0;
return_code = stai_network_get_weights(network, weight_buffers, &n_weights);
if ((return_code == STAI_SUCCESS) && (n_weights==STAI_NETWORK_WEIGHTS_NUM)) {
return_code = stai_network_set_weights(network, weight_buffers, n_weights);
} else {
LOG_PRINT(" ## Test Failed executing stai set weights: 0x%x.\n\n", return_code)
return -1;
}
#endifChanges needed for this section:
- Context allocation is now explicit: the application
must always allocate a buffer thanks to the
provided
STAI_macros that will be initialized using thestai_network_init() - ST Edge AI C runtime must be initialized to
bootstrap once the AI middleware using the
stai_runtime_init() - Context initialization, activations and weights setting now are
managed thanks to three different C APIs, ideally replacing the
former
ai_network_create_and_init()API.
- Step 3: Allocation and setting of the network I/O buffers
Legacy Client APIs application code snippet:
/* Inputs Buffer Setup */
/* Retrieve pointers to the model's input tensors */
ai_buffer* ai_input = ai_network_inputs_get(network, NULL);
if (ai_input) {
ai_input[0].data = AI_HANDLE_PTR(input1) /* defined in network_inputs.h */
}
/* Outputs Buffers Setup */
/* Allocate and declare output buffer #1 */
AI_ALIGNED(4)
float output1[AI_NETWORK_OUT_1_SIZE];
/* Retrieve pointers to the model's output tensors */
ai_buffer* ai_output = ai_network_outputs_get(network, NULL);
if (ai_output) {
ai_output[0].data = AI_HANDLE_PTR(output1);
}
/* No specific I/O setters since ai_input and ai_output as passed as argument of the ai_network_run() */ST Edge AI Embedded Client APIs application equivalent code snippet:
/* Inputs Buffer Setup */
/* C-Table declaring inputs buffer pointers array and set inputs addresses */
stai_ptr input_buffers[STAI_NETWORK_IN_NUM] = {
(stai_ptr)input1 /* defined in network_inputs.h */
};
/* !New!: Set network inputs buffers */
return_code = stai_network_set_inputs(network, input_buffers, STAI_NETWORK_IN_NUM);
if (return_code != STAI_SUCCESS) {
LOG_PRINT(" ## Test Failed executing stai set inputs: 0x%x.\n\n", return_code)
return -1;
}
/* Outputs Buffers Setup */
/* Allocate and declare output buffer #1 */
STAI_ALIGNED(STAI_NETWORK_OUT_1_ALIGNMENT)
float output1[STAI_NETWORK_OUT_1_SIZE];
/* Declare outputs buffer pointers array and set outputs addresses */
stai_ptr output_buffers[STAI_NETWORK_OUT_NUM] = {
(stai_ptr)output1
};
/* Set network outputs buffers */
return_code = stai_network_set_outputs(network, output_buffers, STAI_NETWORK_OUT_NUM);
if (return_code != STAI_SUCCESS) {
LOG_PRINT(" ## Test Failed executing stai set outputs: 0x%x.\n\n", return_code)
return -1;
}Changes summary:
- The allocation of the buffers is similar between the two
snippets: what changes is the removal of
ai_bufferC struct from ST Edge AI Client APIs replaced by the concept of a C-Table of pointers. - In ST Edge AI Client APIs explicit setters are now available to
set input/output buffers pointers. In Legacy Client APIs instead an
array of type
ai_bufferrepresenting the I/O buffers is passed as argument to theai_network_run()API.
- Step 4: Logging info about generated model
Legacy Client APIs application code snippet:
ai_network_report report;
const ai_bool res = ai_network_get_report(network, &report);
if (!res) {
LOG_PRINT(" ## Test Failed executing ai get network report.\n\n")
return -1;
}
LOG_PRINT("* Runtime version : %d.%d.%d\n",
report.runtime_version.major, report.runtime_version.minor, report.runtime_version.micro)
LOG_PRINT("* Tool version : %d.%d.%d\n",
report.tool_version.major, report.tool_version.minor, report.tool_version.micro)
LOG_PRINT("* APIs version : %d.%d.%d\n",
report.api_version.major, report.api_version.minor, report.api_version.micro)
LOG_PRINT("* Network nodes : %d\n", report.n_nodes)
LOG_PRINT("* Network macc : %d\n", report.n_macc)
LOG_PRINT("* Network inputs : %d\n", report.n_inputs)
LOG_PRINT("* Network outputs : %d\n", report.n_outputs)
...ST Edge AI Embedded Client APIs application equivalent code snippet:
stai_network_info info;
return_code = stai_network_get_info(network, &info);
if (return_code != STAI_SUCCESS) {
LOG_PRINT(" ## Test Failed executing stai get network info: 0x%x.\n\n", return_code)
return -1;
}
LOG_PRINT("* Runtime version : %d.%d.%d\n",
info.runtime_version.major, info.runtime_version.minor, info.runtime_version.micro)
LOG_PRINT("* Tool version : %d.%d.%d\n",
info.tool_version.major, info.tool_version.minor, info.tool_version.micro)
LOG_PRINT("* APIs version : %d.%d.%d\n",
info.api_version.major, info.api_version.minor, info.api_version.micro)
LOG_PRINT("* Network nodes : %d\n", info.n_nodes)
LOG_PRINT("* Network macc : %d\n", info.n_macc)
LOG_PRINT("* Network inputs : %d\n", info.n_inputs)
LOG_PRINT("* Network outputs : %d\n", info.n_outputs)
...Changes summary:
- The two APIs are similar: the
ai_network_get_report()returns aai_bool, instead thestai_network_get_info()returns astai_return_codelike all thestaiAPIs. - The
stai_network_get_info()returns information about network I/O properties as an array ofstai_tensortypes, whereas former Legacy Client APIs conveys the same kind of information using theai_bufferC struct. - The
stai_network_get_info()now returns also information about activations/states/weights using always thestai_tensorC struct
- Step 5: Run of the inference (sync mode)
Legacy Client APIs application code snippet:
/* Execute network model inference on sample test (ALWAYS synchronous mode) */
LOG_PRINT("Starting inference\n");
/* The run API supports only sync mode: it is always blocking */
ai_i32 batch = ai_network_run(network, ai_input, ai_output);
LOG_PRINT("Completed inference\n");
if (batch != 1) {
LOG_PRINT(" ## Test Failed executing ai network run: %d.\n\n", batch)
return -1;
}ST Edge AI Embedded Client APIs application equivalent code snippet:
/* Execute network model inference on sample test (synchronous mode) */
LOG_PRINT("Starting inference\n");
/* The run API now supports both sync and async modes */
return_code = stai_network_run(network, STAI_MODE_SYNC);
LOG_PRINT("Completed inference\n");
if (return_code != STAI_SUCCESS) {
LOG_PRINT(" ## Test Failed executing stai network run: 0x%x.\n\n", return_code)
return -1;
}Changes summary:
- The
stai_network_run()now has only two parameters: the network handler and the mode. The informations about network I/O in ST Edge AI Client APIs are handled thanks to the setters APIs namedstai_network_set_inputs()andstai_network_set_outputs() - The return code is now homogeneous with all
staiAPIs - The
stai_network_run()now supports two modes:STAI_MODE_SYNC(default one) that is implementing a blocking API and ‘STAI_MODE_ASYNC’ (not yet supported) that is implementing a non-blocking API.
- Step 6: Dump of the output results
Legacy Client APIs application code snippet:
LOG_PRINT("__START_OUTPUT1 __\n");
for(ai_i32 o = 0; o < AI_NETWORK_OUT_1_SIZE; o++) {
const ai_float value = output1[o];
if (o != 0 && o % 10 == 0) {
LOG_PRINT("\n");
}
LOG_PRINT("%f, ", value);
}
LOG_PRINT("\n__END_OUTPUT1 __\n");ST Edge AI Embedded Client APIs application equivalent code snippet:
LOG_PRINT("__START_OUTPUT1 __\n");
for(int32_t o = 0; o < STAI_NETWORK_OUT_1_SIZE; o++) {
const float value = output1[o];
if (o != 0 && o % 10 == 0) {
LOG_PRINT("\n");
}
LOG_PRINT("%f, ", value);
}
LOG_PRINT("\n__END_OUTPUT1 __\n");Changes summary: Basically the two routines are the same except:
AI_NETWORK_OUT_1_SIZEhas been renamed inSTAI_NETWORK_OUT_1_SIZElike all the macros using theSTAI_prefix- ST Edge AI Client APis now uses types from
<stdint.h>library instead ofai_prefixed types fromai_platform.hheader
- Step 7: De-initialization of the model
Legacy Client APIs application code snippet:
/* Network de-initialization */
const ai_handle ret = ai_network_destroy(network);
return (ret == NULL) ? 0 : -1;
}ST Edge AI Embedded Client APIs application equivalent code snippet:
/* Network de-initialization */
return_code = stai_network_deinit(network);
/* Runtime de-initialization */
return_code = stai_runtime_deinit();
return (return_code == STAI_SUCCESS) ? 0 : -1;
}Changes summary:
ai_network_destroy()has been replaced bystai_network_deinit(). The return code now is always of typestai_return_codelike all the ST Edge AI Client APIs- The ST Edge AI Client APIs now has also a specific API to
de-initialize the AI Middleware named
stai_runtime_deinit()