4.0.0
Template (syntax)


ST Edge AI Core

Template (syntax)


ST Edge AI Core Technology 4.0.0




UNDER CONSTRUCTION!

About writing and formatting the articles

Formatting is mainly based on Markdown syntax with some minor extensions respecting the requested syntax to write the GitHub pages.

[1] Mardown Guide - Basic Syntax
[2] Basic writing and formatting syntax

Syntax

Headings

see section “Headings” [1] & [2]

# A first-level heading
## A second-level heading
### A third-level heading

Styling text

see section “Styling text” [1] & [2]

I just love **bold text**.
Italicized text is the *cat's meow*.
This text is ***really important***.

The rendered output looks like this:

I just love bold text. Italicized text is the cat’s meow. This text is really important.

Images

see section “Images” [1]

To add an image, add an exclamation mark (!), followed by alt text in brackets, and the path or URL to the image asset in parentheses. You can optionally add a title in quotation marks after the path or URL. By default (see css file), the images are centered.

  • Minimal syntax

    ![](./images/auto_ml_flow.png){width=40%}

    Two syntax are possible to indicate the width attribute: {width=40%} or {style="width: 40%;"}.

    The rendered output looks like this:

  • Syntax with figcaption and title

    ![Possible *AutoML*, flow with post deployment check](./images/auto_ml_flow.png "Possible AutoML flow"){style="width: 70%;"}

    The rendered output looks like this:

    Possible AutoML flow with post deployment check (figcaption)

Alert/Admonitions messages

The > [!TYPE] Github syntax and !!! TYPE Material for MkDocs syntax are supported.

Note

Highlights information that users should take into account, even when skimming.

Tip

Optional information to help a user be more successful.

Important

Crucial information necessary for users to succeed.

Warning

Critical content demanding immediate user attention due to potential risks.

Caution

Negative potential consequences of an action.

Important

Crucial information necessary for users to succeed.

Note

With list + code

  • test1
    • sub-item
  • test 2

Test suite

def helloworld(str):
    """."""
    print(str)

Footnote

@octocat :+1: This PR looks great - it’s ready to merge! :shipit:

Here is a simple footnote1.

A footnote can also have multiple lines2.

Synopsis

Task list (status)

Note

Modification of the checkbox is disabled

Status

“analyze” command

How to add a collapsible section in markdown

Collapsible section

bla, bla,…

List

  • item 1
  • item 2
    • item 2.1

Table

Rank Languages
1 JavaScript
2 Python
3 SQL

Some Javascript

function logSomething(something) {
  console.log('Something', something);
}

  1. My reference.↩︎

  2. To add line breaks within a footnote, prefix new lines with 2 spaces. This is a second line.↩︎