Neural-ART - Supported operators and limitations
for STM32 target, based on ST Edge AI Core Technology 4.1.0
r1.4
Overview
This document describes the model formats, quantization schemes, supported operators, and hardware limitations relevant to deploying neural networks on the Neural-ART™ accelerator.
Quantized Model Format
The Neural-ART compiler supports the following quantized model formats, subject to the supported data types:
- TensorFlow Lite / LiteRT models quantized using post-training quantization (PTQ) or quantization-aware training (QAT). TFLite can quantize only operators with supported quantized kernels and compatible operator patterns.
- ONNX
quantized models in QDQ format. In this format,
QuantizeLinearandDequantizeLinearoperators represent quantization and dequantization around operators in the graph. These models can be generated using ONNX Runtime quantization tools.
Only full integer static quantization is supported. It quantizes both weights and activations into integers, using representative calibration data to determine quantization parameters. Weight-only and dynamic quantization are not supported.
If a graph contains unsupported operators, the model architecture may need to be modified or those operators replaced. Where available, the compiler can use a software fallback. Mixed-precision schemes across layers or operators are supported. Unsupported hardware mappings fall back to floating-point kernels; mixed N-bit-to-M-bit activation mapping is not enabled on the hardware activation path.
Supported precision and data types
| type | weight precision | activation precision | quantization scheme | notes |
|---|---|---|---|---|
| w8a8 | int8 | int8 | full integer, scale/zero-point, ss/sa | per-channel/per-tensor for weights. Only per-tensor for activations. |
| w4a8 | int4 | int8 | full integer, scale/zero-point, ss/sa | per-channel/per-tensor for weights. Only per-tensor for activations. Convolution and dense layer type only. |
| w8a16 | int8 | int16 | full integer, fixed point number (or qmn) format only, ss/ss | per-tensor, scale factor is always a power of 2 and offset/zero point is equal to 0. Only for weights: scales can be both per-channel and per-tensor. |
- w8a16 model generation can be based on a quantization workflow that uses an enhanced version of the AMD Quark Model Optimizer library. Refer to the tutorial “How to quantize a model in 16-bits with the AMD Quark library”. Experimental static w8a16 models from LiteRT/TFLite environment is not supported.
- w4a8 models require an advanced quantization workflow that supports mixed precision, QAT, or both. Refer to the “STM32 model-zoo object-detection example”.
- For w8a8 models, refer to “Quantized model support” article, for instructions on quantizing with the TensorFlow Lite converter or ONNX Runtime.
To preserve correctness for some quantization parameters, the compiler may map individual layers to floating-point software fallback.
Inference Model Constraints
Neural-ART is a re-configurable inference-only engine capable of accelerating in hardware the quantized inference models, no training mode is supported.
- Input and output tensors must be static
- Variable-length batch dimension (i.e. (None,)) is considered as equal to 1
- Operator with un-connected output is not supported
- Mixed data operations (i.e hybrid operator) are not supported, activations and weights should be quantized
- Data type for the weights/activations tensors must be:
- int8 (scale/offset format) ss/sa scheme (see Quantized models – per-channel)
- if float32 operation is requested, it will be mapped on a SW operation
Custom Layer Support - Post-Processing
The custom operator like
TFLite_Detection_PostProcess is not supported. For
object-detection models, consider removing this operator before
quantization and retaining only the backbone and detection head.
Post-processing, including non-maximum suppression (NMS), can then
be performed by an external library on the host MCU.
TFlite Operation Mapping
The following table describes how TensorFlow Lite (TFLite) operations map to the Neural-ART stack. Only supported quantized operations in w8a8 format can be mapped directly to Neural-ART hardware. If an operation is not mapped to hardware, an int8 or float32 software fallback may be used on the host subsystem. Software quantize and dequantize operations are inserted as needed to convert between int8 and float32; these operations are deployed as software epochs.
| TFLite Operation | mapped on | precision | comment |
|---|---|---|---|
| ABS | HW | a8 | |
| ADD | HW | a8 | SW mapping if broadcasting out of HW supported broadcasting |
| ADD_N | SW_FLOAT | ||
| ARG_MAX | SW_INT | a8 | |
| ARG_MIN | SW_INT | a8 | |
| AVERAGE_POOL_2D | HW | a8 | See Pool Limitations |
| BATCH_MATMUL | HW | w8a8 | Second input should be constant else SW fallback is considered |
| CAST | HW | a8 | |
| CEIL | HW | a8 | |
| CONCATENATION | HW | a8 | |
| CONV_2D | HW | w8a8 | see Optimal Kernel Size / Stride Size and Tips. Weights tensor should be constant else SW fallback is considered. |
| COS | HW | a8 | |
| COSH | HW | a8 | |
| DEPTH_TO_SPACE | HW | a8 | with same input/output quantization |
| DEPTHWISE_CONV_2D | HW | w8a8 | |
| DEQUANTIZE | SW_FLOAT | uint8/int8/int16 -> float | |
| DIV | SW_INT | ||
| ELU | HW | a8 | |
| EXP | HW | a8 | |
| EXPAND_DIMS | HW | a8 | |
| FLOOR | SW_FLOAT | ||
| FULLY_CONNECTED | HW | w8a8 | |
| GATHER | SW_INT | a8 | |
| GELU | HW | a8 | |
| HARD_SWISH | HW | a8 | |
| L2_NORMALIZATION | SW_FLOAT | ||
| LEAKY_RELU | HW | a8 | |
| LOCAL_RESPONSE_NORMALIZATION | SW_FLOAT | ||
| LOG | SW_FLOAT | ||
| LOGISTIC | HW | a8 | |
| MAX_POOL_2D | HW | w8a8 | Decomposition in multiple operations
if kernel Height or Width are greater than 3 Horizonal and vertical strides ranging from 1 to 15 See Pool Limitations |
| MAXIMUM | HW | a8 | |
| MEAN | SW_FLOAT | ||
| MINIMUM | HW | a8 | |
| MUL | HW | a8 | SW fallback with broadcast or more than 4 dimensions. See broadcasting limitations |
| NEG | HW | a8 | |
| PACK | HW | a8 | |
| PAD | HW | a8 | Partial – according to the parameters, it can be HW-assisted with the extra epochs. |
| POW | HW | a8 | Supported in HW for 8bit Scale/Offset input and constant exponent. Otherwise, fallback to float. |
| PRELU | HW | a8 | slope attribut should be
quantized. |
| QUANTIZE | SW_FLOAT | float -> uint8/int8/int16 | |
| (RE) QUANTIZE | HW | uint8 <-> int8 | |
| REDUCE_MAX | HW | a8 | HW if it can be convered to GlobalMaxPool. No overhead if the reduced axes are the right-most ones, and the input shape.size() = number of reduced_axes+2. Additional Transposition and Reshapes might be required otherwise. SW fallback available |
| REDUCE_MIN | HW | a8 | HW if it can be convered to GlobalMinPool. No overhead if the reduced axes are the right-most ones, and the input shape.size() = number of reduced_axes+2. Additional Transposition and Reshapes might be required otherwise. SW fallback available |
| REDUCE_PROD | SW_FLOAT | ||
| RELU | HW | a8 | |
| RELU6 | HW | a8 | |
| RESHAPE | HW | a8 | |
| RESIZE_BILINEAR | SW_INT | ||
| RESIZE_NEAREST_NEIGHBOR | HW/SW_INT | a8 | HW if (coordinate_transformation_mode=‘asymmetric’ AND nearest_mode=‘floor’). SW_INT otherwise |
| ROUND | SW_FLOAT | ||
| RSQRT | HW | a8 | |
| SHAPE | HW | a8 | |
| SIN | HW | a8 | |
| SLICE | HW | a8 | |
| SOFTMAX | HW | a8 | Maximum supported dimensions: 4. There must be a leading dimension equal to 1 and up to 4 dimensions: (1, D1, D2, D3). Softmax computation dimension must be smaller or equal to 2048. The SW fallback can be enabled using the option –disable-hw-softmax. |
| SPACE_TO_DEPTH | HW | a8 | with same input/output quantization |
| SPLIT | HW/SW_INT | a8 | HW or SW_INT depends on axis |
| SPLIT_V | HW/SW_INT | HW or SW_INT depends on axis | |
| STRIDED_SLICE | HW | a8 | |
| SQUARE | HW | a8 | |
| SQUEEZE | HW | a8 | |
| SQRT | HW | a8 | |
| SUB | HW | a8 | |
| SUM | SW_FLOAT | ||
| TANH | HW | a8 | |
| TRANSPOSE | HW | a8 | Partial – according to the parameters, it can be HW-assisted with the extra epochs. |
| TRANSPOSE_CONV | HW | a8 | Partial – according to the parameters, it can be HW-assisted with the extra epochs. |
| TOPK_V2 | SW_FLOAT | a8 | |
| UNPACK | HW | a8 |
ONNX Operation Mapping
The following table describes how ONNX operations map to the Neural-ART stack. Supported quantized operations in w8a8, w4a8, or w8a16 format can be mapped directly to Neural-ART processing units. If an operation is not mapped to hardware, an int8 or float32 software fallback may be used on the host subsystem. Software quantize and dequantize operations are inserted as needed to convert between int8 and float32; these operations are deployed as software epochs.
| ONNX Operator | Pytorch Name | mapped on | precision | comment |
|---|---|---|---|---|
| Abs | abs | HW/SW_FLOAT | a8 | HW if Offset is 0, SW_FLOAT otherwise |
| Acos | acos | HW | a8 | |
| Acosh | HW | a8 | ||
| Add/sum | add | HW | a8, a16 | SW mapping if broadcasting out of HW supported broadcasting |
| And | HW | a8 | ||
| ArgMax | argmax | SW_INT | a8 | |
| ArgMin | argmin | SW_INT | a8 | |
| Asin | asin | HW | a8 | |
| Asinh | HW | a8 | ||
| Atan | atan | HW | a8 | |
| Atanh | argmin | HW | a8 | |
| AveragePool | avg_pool1d/avg_pool2d | HW | a8 | See Pool limitations |
| BatchNormalization | BatchNorm1D/BatchNorm2D | HW | w8a8, w8a16 | |
| Cast | HW | a8 | Software library mapped on DMAs or pure software | |
| Ceil | ceil | SW_FLOAT | ||
| Clip | clip/ReLU6 | HW | a8, a16 | |
| Concat | concat/concatenate | HW | a8, a16 | Mapped on HW or SW depending on the batch and concatenation axis |
| Conv | Conv1D/Conv2D | HW | w8a8, w4a8, w8a16 | see Optimal Kernel Size / Stride Size and Tips. Weights tensor should be constant else SW fallback is considered. |
| ConvTranspose | HW | w8a8, w8a16 | ||
| Cos | cos | HW | a8 | |
| Cosh | cosh | HW | a8 | |
| DepthToSpace | SW | a8, a16 | DMA is used with mode “DCR” | |
| DequantizeLinear | dequantize | SW_FLOAT | w8a8 | int8/uint8/int16 -> float32 |
| Div | div | SW_INT | a8 | HW if second operand is a constant |
| Elu | elu | HW | a8 | |
| Erf | erf | HW | a8 | |
| Exp | exp | HW | a8 | |
| Flatten | flatten | HW | a8, a16 | |
| Floor | floor | SW_FLOAT | ||
| Gather | gather | SW_INT | ||
| Gemm | HW | w8a8, w4a8, w8a16 | Params input should be constant else SW fallback is used | |
| Gelu | GELU | HW | a8 | Supported as single ONNX GELU operator and expanded version (see --GELU-recognition option) |
| GlobalAveragePool | HW | a8, a16 | Limited window. Software fallback available | |
| GlobalMaxPool | HW | a8, a16 | Limited window. Software fallback available | |
| Hardmax | SW_FLOAT | |||
| HardSigmoid | HW | a8 | ||
| HardSwitch | HW | a8 | ||
| Identity | identity | HW | a8, a16 | |
| InstanceNormalization | InstanceNorm1/InstanceNorm2 | SW_FLOAT | ||
| LeakyRelu | LeakyReLU | HW | a8, a16 | |
| LRN | LocalResponseNormalization | SW_FLOAT | ||
| Log | log | SW_FLOAT | ||
| LpNormalization | SW_FLOAT | |||
| MatMul | HW | w8a8, w8a16 | Non-constant inputs leading dimension must be equal to 1 and with up to 4 dimensions: (1, D1, D2, D3).The SW fallback can be enabled using the option –disable-hw-matmul. | |
| MaxPool | HW | a8, a16 | Decomposition in multiple operations if kernel Height or Width are greater than 3. Horizonal and vertical strides ranging from 1 to 15. See Pool limitations | |
| Max | HW | a8 | ||
| Min | HW | a8 | ||
| Mod | SW_FLOAT | |||
| Mul | mul | HW | a8, a16 | see broadcasting limitations |
| Neg | neg | HW | a8 | |
| Pad | ConstantPad1D/ConstantPad2D/ZeroPad2D | HW | a8, a16 | Mapped on ConvAcc, DMA or SW |
| Pow | HW | a8 | Supported in HW for 8bit Scale/Offset input and constant exponent. Otherwise, fallback to float. | |
| PRelu | HW | a8 | slope attribut should be
quantized. |
|
| QLinearAdd | HW | a8, a16 | Same as Add | |
| QLinearAveragePool | HW | a8 | Same as AveragePool | |
| QLinearConcat | HW | a8, a16 | Same as Concat | |
| QLinearConv | HW | w8a8, w8a16 | Same as Conv | |
| QLinearGlobalAveragePool | HW | a8, a16 | same as GlobalAveragePool | |
| QLinearMatMul | HW | w8a8, w8a16 | same as MatMul | |
| QLinearMul | HW | w8a8, w8a16 | same as Mul | |
| QuantizeLinear | quantize_per_tensor | SW_FLOAT | int8/uint8 -> float/int8 requantization supported in HW | |
| Reciprocal | reciprocal | HW | a8 | |
| ReduceLogSumExp | SW_FLOAT | a8 | ||
| ReduceMax | HW | a8 | HW if it can be convered to GlobalMaxPool. No overhead if the reduced axes are the right-most ones, and the input shape.size() = number of reduced_axes+2. Additional Transposition and Reshapes might be required otherwise. SW fallback available | |
| ReduceMean | HW/SW_INT | a8, a16 | HW if it can be convered to GlobalAveragePool. No overhead if the reduced axes are the right-most ones, and the input shape.size() = number of reduced_axes+2. Additional Transposition and Reshapes might be required otherwise. SW fallback available | |
| ReduceMin | HW | a8 | HW if it can be convered to GlobalMinPool. No overhead if the reduced axes are the right-most ones, and the input shape.size() = number of reduced_axes+2. Additional Transposition and Reshapes might be required otherwise. SW fallback available | |
| ReduceProd | SW_FLOAT | a8 | ||
| ReduceSum | HW | a8, a16 | HW if it can be convered to GlobalAveragePool. No overhead if the reduced axes are the right-most ones, and the input shape.size() = number of reduced_axes+2. Additional Transposition and Reshapes might be required otherwise. SW fallback available | |
| Relu | relu | HW | a8, a16 | |
| Reshape | shape | HW | a8, a16 | |
| Resize | upsample | SW_INT | a8, a16 | Resize Nearest Neighbor on HW if coordinate_transformation_mode=‘asymmetric’ AND nearest_mode=‘floor’ |
| Round | round | SW_FLOAT | ||
| Selu | selu | HW | a8 | |
| Shape | HW | a8, a16 | ||
| Sin | sin | HW | a8 | |
| Sinh | sinh | HW | a8 | |
| Sigmoid | sigmoid | HW | a8 | HW Acceleration available also for X*Sigmoid(X) |
| Slice | HW | a8, a16 | DMA acceleration | |
| Softmax | softmax | HW | a8 | Maximum supported dimensions: 4. There must be a leading dimension equal to 1 and up to 4 dimensions: (1, D1, D2, D3). Softmax computation dimension must be smaller or equal to 2048. The SW fallback can be enabled using the option –disable-hw-softmax. |
| Softplus | softplus | SW_FLOAT | a8 | |
| SoftSign | softsign | SW_FLOAT | a8 | |
| Split | split | HW | a8, a16 | |
| Squeeze | squeeze | HW | a8, a16 | |
| Sqrt | sqrt | HW | a8 | |
| Sub | sub | HW | a8 | |
| Swish | SiLU | SW_FLOAT / HW | a8 | Not supported as single ONNX SWISH operator, however the expanded version is supported (see --SWISH-recognition option) |
| Tan | tan | HW | a8 | |
| Tanh | tanh | HW | a8 | |
| ThresholdedRelu | HW | a8 | ||
| Tile | SW_INT | a8 | Optimized by constant folding passing through front-end, SW_INT fallback otherwise | |
| Transpose | transpose | HW | a8, a16 | |
| Topk | SW_FLOAT | |||
| Unsqueeze | unsqeeze | HW | a8, a16 | |
| Upsample | upsample | SW_FLOAT |
Neural-ART™ Processor Unit Tips and Limitations
Optimal Kernel Size / Stride Size
Maximum kernel width supported in hardware is 6 for stride 1 and 12 for stride of minimum 2. Vertical kernel size is limited to max 3. All larger kernel dimensions lead to a decomposition done by the compiler which has to be processed iteratively.
- Best use of a kernel height is 3 (using just 2 will not help)
- Best use of a kernel width is 3, 6, 12 (anything between and larger than 1 will not be better)
- Avoid horizontal strides that are not 1, 2, or 4 if possible (2 and 4 are valid but lead to less data reuse)
- Avoid vertical strides that are not 1, 2, or 4 if possible (vertical strides are in general inefficient)
- Kernel dimensions of 1 (horizontal or vertical) are special cases (e.g., 1x1, 2x1, 1x2, 2x1, 1x3, 1x6, 1x12, etc.) and can be handled efficiently. They will run a lot faster than, for example, 3x2 or 2x3
- Kernels with height 1 have no restrictions on the feature width (theoretical max is 2^16-1).
Don’t use strides larger than the kernel dimension (useless data). The compiler will have to play tricks as this is not natively supported in hardware. Note that layers with more input channels (ICH) than output channels (OCH) can often be mapped with better efficiency.
Special Case: 1x1 Kernel
1x1 kernel can be handled very efficiently if the number of input channels (ICH) is equal to N* 72…128 and the number of output channels (OCH) is equal to M(16..24) (best M24), with N, M as integers. If these numbers are larger than the amount of available CONV processing units (4 CA for STM32N6 NeuralART™), the compiler will translate this in multiple iterations.
To illustrate, three typical examples:
- ICH=128 and OCH=96 would run at the same speed as ICH=32 and OCH=96 even when there are 4 times fewer MACs as in the first one (4 CA in parallel)
- ICH=512 and OCH=24 would run at the same speed as ICH=512 and OCH=4 even when there are 6 times fewer MACs as in the first one (4 CA in series)
- ICH=256 and OCH=48 would run at the same speed as ICH=129 and OCH=25 even when there are almost 4 times fewer MACs as in the first one. (2 CA in series, 2 chains in parallel)
Zeros in the Kernel or Feature Data
They will save power (gated MAC units) but not affect the performance.
Optimal Feature Width
For 8-bit feature data, feature width multiplied by the used batch depth (input channels) must be equal to or lower than 2048. Thus, for 512 wide features, batch depth will be limited to 4 and wider feature sizes further reduce the number of input channels and may cause the compiler to even split the feature into multiple columns.
Optimal Pool Operations with up to 3x3 Pooling Windows
- Don’t use pooling windows larger than 3, else they will be decomposed by the compiler.
- The number of input channels is limited. Check that a previous operation is not generating more input channels, else chaining will not be possible.
- The line buffer of the pooling unit is limited. Avoid using data with [width x input_channels] larger than 2048 else the compiler has to split the operator into multiple columns.
Hardware supported broadcasting
- Only Unidirectional broadcasting is supported in hardware
- The best performance is achieved with a number of elements less or equal to 512.
- Broadcasting is mapped on Arithmetic Unit with best performance
in case of
- Scalar broadcasting
- Channel broadcasting (C <= 512, other dimensions =1)
- Height broadcasting (H <= 512, other dimensions =1)
- Width broadcasting (W <= 512, other dimensions =1)
- Height-Width broadcasting ((H*W) <= 512, other dimensions =1)
- DMAs supported broadcasting:
- Channel broadcasting
- Height broadcasting
- Width broadcasting
- Height-Width broadcasting
- Channel-Width broadcasting
- Channel-Height broadcasting
- When the broadcasted input is the second input of the node
- Supported only for commutative operations
Convolutions tips
- Avoid big dilation factor, big dilation factors leads to non-optimal performance.
- Avoid using prime number as number of kernels/channels, it will limit the heuristic for kernel/channel splitting.
- When using a very large kernel, use a multiple of 3 for width and height
- Horizontal strides lead to less data reuseVertical strides are in general inefficient.
- Pad <= 2, are supported without impacting performance.
- Zeros in the kernel or feature data will save power (gated MAC) but not affect the performance. Values that are almost zero cannot be used to gate the MAC units, thus no power saving.
Pool limitations
- Only 1D and 2D supported
- Kernel shape: Height and Width between 1 and 3 included
- Horizonal and vertical strides ranging from 1 to 15
- Pad
- Left, right and top padding ranging from 0 to 7
- Max bottom padding supported is up to Window Height minus 1
- input features Width <=2048 when 8 bits are used, and <=1024 when 16 bits are used.
Note that for N6 HW mapping: padded values are always included in the computation. Fallback on SW available otherwise.