4.1.0
Neural-ART compiler primer


ST Edge AI Core

Neural-ART compiler primer


for STM32 target, based on ST Edge AI Core Technology 4.1.0



r1.3

Overview

This article describes the main options and required input files for the Neural-ART compiler (also known as the neural processing unit (NPU) compiler), used to deploy artificial intelligence (AI) and deep learning (DL) models on Neural-ART-based devices.

Note that the NPU compiler is integrated as a specific back end in the ST Edge AI Core command-line interface (CLI). The CLI acts as a driver or front end. However, it is also possible to use the NPU compiler directly with the generated intermediate files (ONNX and JSON files). Only these input files representing the original model are supported. It is not possible to pass an ONNX quantization-dequantization (QDQ) or quantized TensorFlow Lite (TFLite) file directly. In this case, the options are passed directly to the compiler as arguments.

Warning

It is not recommended to use directly the atonn executable. Some features (such epoch controller support or IO data type and layout changes) are only supported via the front-end.

The main outputs are:

Tip

The NPU compiler is configurable and offers several options to modify how a network is compiled. This article covers only the main relevant options. To view the complete list of options with brief descriptions, use the --help option. Note that it is preferable to invoke the NPU compiler through the ST Edge AI Core command-line interface; in this case, the compilation profile file (json fomat) is used to pass the NPU compiler options.

atonn --help

NPU compiler location

‘atonn’ designates the name of the executable.

%STEDGEAI_CORE_DIR%\Utilities\<host_os>\atonn

%STEDGEAI_CORE_DIR% indicates the location where the ST Edge AI Core components are installed.

Options

For a STM32N6 device including an Neural-ART IP, the minimal options needed to operate properly are the following ones:

$ atonn --load-mpool my_mpool.mpool --onnx-input my_model_OE_3_1_0.onnx --json-quant-file my_model_OE_3_1_0_Q.json
  --cache-maintenance --Ocache-opt --native-float --enable-virtual-mem-pools --load-cdesc cortex-m55 --load-mdesc stm32n6

Recommended default options:

$ atonn --load-mpool my_mpool.mpool --onnx-input my_model_OE_3_1_0.onnx --json-quant-file my_model_OE_3_1_0_Q.json
  --cache-maintenance --Ocache-opt --native-float --enable-virtual-mem-pools --load-cdesc cortex-m55 --load-mdesc stm32n6
  --enable-virtual-mem-pools --enable-epoch-controller -Os

Mandatory options

Model/Platform configuration options

Option Description
-i, --onnx-input Input ONNX file path
--json-quant-file Input JSON file path (Quantization information)
-g, --c-output Output .c file path
--load-cdesc-file, --load-cdesc Specifies the MCU description file
-t, --load-mdesc, --target Specifies the target machine to use, machine description (.mdesc) file path
--load-mpool Specifies the memory pool descriptors to use, memory pool (.pool) file path
  • The NPU supports only the quantized models that have been “translated” to the ONNX+JSON format by the ST Edge AI Core CLI.
  • To enable code-generation of the compiler, the '-g' option is mandatory and sets the name of the .c output file.
  • The NPU compiler is platform-agnostic. The --load-mdesc/--target option allows to provide the configuration of the Neural ART accelerator™ which is implemented (also called machine descriptor file, the ‘stm32n6.mdesc’ file should be not modified).
  • The --load-mpool provides the description of the memory pools which can be used to implement the provided model. This file is user specific.

Specific STM32N6 device options

An additional set of mandatory options should be used when using the STM32N6 as the target:

Option Description
--native-float Consider all floats without quantization info as native floats
--load-cdesc cortex-m55 Enable the scratch buffers generation for Arm® Cortex® M55 core with MVE extension
--cache-maintenance Enable generation of cache maintenance code for both MCU & NPU caches
--Ocache-opt Enables usage of the NPU cache path for memory pools which have the attribute ‘cacheable’ set in the memory-pool description file, requires option ‘–cache-maintenance’ to be passed as well. When requested the NPU compiler emits instructions which make use the NPU cach path for the streaming engine configurations.
  • The --native-float is mandatory to bypass the check that everything should be quantized in the network given as argument. Not quantizing parts of the network results in lengthy floating operations, but this is not prevented the compiler from completing its work.

Warning

For performance reasons, it is recommended to enable the NPU cache (using the --Ocache-opt option) for the NPU memory regions stored in external memories (flash/RAM). The shared memory regions between the NPU and MCU domains, used for input/output buffers and by the software epochs, must be cacheable MCU regions. To guarantee memory coherence during inference, the --cache-maintenance option is mandatory. However, it is the application’s responsibility to use cache maintenance functions when filling or using the input/output or activations memory regions before to perform the inference.

Recommended options with possible accuracy variance or inference-time impact

The following options adjust the computation graph by fusing or expanding operations to enable more efficient hardware inference on the NPU. However, there are corner cases where clipping and rounding operations on intermediate activations may be evaluated differently compared with the original graph.

Users must evaluate and validate whether the resulting accuracy variance is acceptable for their application.

Option Description
--disable-hw-softmax Disable hardware acceleration of the softmax function
--GELU-recognition Enable GELU recognition pattern ignoring internal quantization info.
--SWISH-recognition Enable SWISH recognition pattern ignoring internal quantization info.
--disable-hw-matmul Disable MatMul hardware acceleration.
--hw-reducesum Enable ReduceSum hardware execution.

Softmax support considerations

Softmax is expanded by default into operations that can be mapped to hardware. Its implementation uses more processing units, which generally provide higher numerical precision, but can increase inference time, especially when softmax is computed on multidimensional tensors. In some cases, the overhead of configuring and using these units outweighs the latency benefit. The loss of precision can be negligible in applications where the exact softmax values are not critical. For example, in a classification model, the approximate implementation is often sufficient when only the index of the predicted class is used and no confidence threshold is applied. The user must assess whether this behavior is acceptable for the specific use case.

In all cases, neither implementation guarantees a bit-true result with respect to the original quantized model. This option is provided to allow a tradeoff between precision and performance according to application requirements. If more precision is required, the --disable-hw-softmax option is available to disable hardware mapping.

GELU support considerations

Depending on the ONNX opset, the PyTorch GELU operator can:

  • be expanded into a subgraph of basic operations (older opsets), or
  • be exported as a single ONNX GELU operator (for example, opset ≥ 20, depending on the framework).

When GELU is exported as a single ONNX operator, the ST Edge AI Core front end expands it internally into a supported form for the NPU compiler. Because no internal quantization information is available for this operator, the resulting hardware mapping is effectively equivalent to enabling the --GELU-recognition option on an expanded GELU pattern.

As a consequence:

  • The GELU mapping may slightly differ from a fully quantization‑aware, hand‑tuned expansion.
  • Users should verify accuracy when using GELU‑based models with recent ONNX opsets, particularly if GELU appears in critical parts of the network.

SWISH (or SiLU) support considerations

For SWISH (or SiLU), only the expanded version of the operator is supported by the NPU compiler.

  • When alpha = 1.0 and the intermediate values are quantized, the SWISH pattern is automatically recognized and mapped to a single hardware processing unit, with no need for additional options.
  • If alpha is not equal to 1.0, or if the intermediate values are not quantized in the standard way, the automatic pattern recognition may fail.

In these cases, the --SWISH-recognition option:

  • enables recognition of SWISH with alpha ≠ 1, and
  • ignores intermediate quantization details to still map the operation to dedicated hardware.

As with the other options, ignoring internal quantization can introduce a small accuracy variance. Users should:

  • enable –SWISH-recognition when it provides meaningful performance or power benefits, and
  • validate that the resulting accuracy remains acceptable for their application.

MatMul with dynamic inputs

MatMul lowering now handles cases where both inputs are runtime tensors (non-const tensors), with broader ONNX opset and broadcasting coverage. Hardware mapping is enabled by default; pass --disable-hw-matmul to turn it off.

Advanced options

Option Description
--ec-optimize N Epoch controller blobs optimizations.

Epoch-controller optimize

The --ec-optimize selects the blob optimizer: 0 disables optimization, 1 uses the Write Merger, 2 uses the Write Pruner without CONFCLR handling, and values above 2 enable CONFCLR handling. The default is 3. The optimizer removes or combines register writes while accounting for polling, unit resets, and register behavior.

Useful options

Option Category Description
--out-dir-prefix global The output prefix used to specify the output directory for generated files.
--network-name global Changes the generated network c-name (default: Default). This results in different symbol names in the .c file.
--options-file global Export the full command line to a .ini file for future import. This option is useful to reproduce a compilation step. The .ini file contains the full command line
--load-options global Import an exported .ini file
--onnx-output extra outputs Output ONNX filename. The NPU compiler makes manipulations/optimizations on the input ONNX file. The resulting ONNX file is then the one that is really transformed to a .c file. This intermediate ONNX file can be exported using this option.
--save-mdesc-file extra outputs Dumps machine description in use to file
--save-mpool-file extra outputs Dumps memory pools in use to file
--dot-file extra outputs Debug purpose - Dumps a .dot file showing internal behavior of the generated program. Operations done in the .c file (details of the epochs) can be exported in a .dot file that provides a graphical view of operations done in C.
--csv-file extra outputs Dumps a .csv-report file showing details for memory transfers and power consumption estimation per epoch. A report showing details of the memory transfers, and estimations of inference time/power consumption can be exported. (The values in the csv are mainly estimations and may diverge from the results in real life)
-A,--Oauto optimization Enables iterative automatic optimization options selection for all options below (increases compilation time)
--Omax-ca-pipe n optimization Where n is an int >0. Sets the maximum number of CONV_ACC used when pipelining (default is 0 meaning unlimited, max is defined in the machine descriptor file, mdesc file)
--Oalt-sched optimization Enables alternate scheduler algorithm
-O,--optimization optimization Optimization level one of [0-3](speed)
  • Each optimization can be done one-by-one. Using -A,--Oauto explores all combinations possible and assess which one seems to provide the “best” that is, fastest results
  • Adding --d-auto n (with 0<n<3: provides debug information about automatic optimization done by -A,--Oauto)
  • When using -A,--Oauto, --Omax-ca-pipe 0 should be added to ensure that the exploration of the configurations is optimal.

Experimental options

The following table presents the main experimental options available. To list all available options, type $ atonn --help.

Option Category Description
--Oconv-split-cw optimization Enable experimental optimization to split convolutions channel-wise.
--Oconv-split-kw optimization Enable experimental optimization to split convolutions kernel-wise.
--Oconv-split-kw optimization Enable experimental optimization to split convolutions stripe-wise for 1xN kernels.
--Oconv-split-stripe optimization Enable experimental optimization to split convolutions stripe-wise for 1xN kernels.
--Oconv-split-stripe-full optimization Enable experimental optimization to split convolutions stripe-wise for any kernel size.

Memory-pools

Introduction

Memory-pool descriptor files are used to give the NPU compiler a vision of the memory characteristics and mapping that is free to use for the compiler on the embedded system.

When the NPU compiler can use two memory locations to fit, for example, an activation buffer, it decides which location is ‘the best’ based on estimated data access time. For this allocation algorithm to perform well, it is then required to describe the memory with as much accuracy as possible.
The example mpool files are written for STM32N6 and contain descriptions for each internal memory cuts + external memories accessed through XSPI:

  • Disposable AXISRAM is definitely slower than NPU-RAMs. The NPU compiler prefers using NPU-RAMs to allocate buffers and uses the AXISRAM if the NPU-RAMs are full.
  • External memories are even slower than AXISRAM. NPU compiler allocates data in external memories as a last-resort.

Additional characteristics can be specified for each memory region defined in the memory pool file:

  • rights: Read/write accesses are required for each defined region. Read-only regions contain weights, while write regions contain activations and, as a last resort, weights if read-only pools are full.
  • constants_preferred: A cue can be added for each region to advise the NPU compiler to preferentially use a given pool for storing constants (weights).. This overrides speed considerations addressed above.
  • chacheable: Cacheability can be enabled for each region.

Finally, if applicable, the cache structure and characteristics should be defined in the mpool file, this gives the NPU compiler all the information it needs to optimize as much as possible the inference time.

Example

Below is an example of a memory-pool file used as a default configuration in the STEdgeaAI tool. The syntax of the mpool file is strict JSON: no comments are allowed.

This example can be used as a base for variations, as it contains the mandatory section of such a file:

  • memory: Definition of the memory characteristics described above
    • cacheinfo: cache characteristics
    • mem_file_prefix: prefix for the memory initializer files generated by the NPU compiler.
    • mempools: the memory-pools description
{
    "memory": {
        "cacheinfo": [
            {
                "nlines": 512,
                "linesize": 64,
                "associativity": 8,
                "bypass_enable": 1,
                "prop": { "rights": "ACC_WRITE",  "throughput": "MID",   "latency": "MID", "byteWidth": 8,
                          "freqRatio": 2.50, "read_power": 13.584, "write_power": 12.645 }
            }
        ],
        "mem_file_prefix": "atonbuf",
        "mempools": [
            {
                "fname": "AXIFLEXMEM",
                "name":  "flexMEM",
                "fformat": "FORMAT_RAW",
                "prop":   { "rights": "ACC_WRITE", "throughput": "MID",  "latency": "MID", "byteWidth": 8,
                            "freqRatio": 2.50, "read_power": 9.381,  "write_power": 8.569 },
                "offset": { "value": "0x34000000", "magnitude":  "BYTES" },
                "size":   { "value": "0",        "magnitude": "KBYTES" }
            },
            {
                "fname": "AXISRAM1",
                "name":  "cpuRAM1",
                "fformat": "FORMAT_RAW",
                "prop":   { "rights": "ACC_WRITE", "throughput": "MID",  "latency": "MID", "byteWidth": 8,
                            "freqRatio": 2.50, "read_power": 16.616, "write_power": 14.522 },
                "offset": { "value": "0x34064000", "magnitude":  "BYTES" },
                "size":   { "value": "0",        "magnitude": "KBYTES" }
            },
            {
                "fname": "AXISRAM2",
                "name":  "cpuRAM2",
                "fformat": "FORMAT_RAW",
                "prop":   { "rights": "ACC_WRITE", "throughput": "MID",  "latency": "MID", "byteWidth": 8,
                            "freqRatio": 2.50, "read_power": 17.324, "write_power": 15.321 },
                "offset": { "value": "0x34100000", "magnitude":  "BYTES" },
                "size":   { "value": "1024",       "magnitude": "KBYTES" }
            },
            {
                "fname": "AXISRAM3",
                "name":  "npuRAM3",
                "fformat": "FORMAT_RAW",
                "prop":   { "rights": "ACC_WRITE", "throughput": "HIGH", "latency": "LOW", "byteWidth": 8,
                            "freqRatio": 1.25, "read_power": 18.531, "write_power": 16.201 },
                "offset": { "value": "0x34200000", "magnitude":  "BYTES" },
                "size":   { "value": "448",        "magnitude": "KBYTES" }
            },
            {
                "fname": "AXISRAM4",
                "name":  "npuRAM4",
                "fformat": "FORMAT_RAW",
                "prop":   { "rights": "ACC_WRITE", "throughput": "HIGH", "latency": "LOW", "byteWidth": 8,
                            "freqRatio": 1.25, "read_power": 18.531, "write_power": 16.201 },
                "offset": { "value": "0x34270000", "magnitude":  "BYTES" },
                "size":   { "value": "448",        "magnitude": "KBYTES" }
            },
            {
                "fname": "AXISRAM5",
                "name":  "npuRAM5",
                "fformat": "FORMAT_RAW",
                "prop":   { "rights": "ACC_WRITE", "throughput": "HIGH", "latency": "LOW", "byteWidth": 8,
                            "freqRatio": 1.25, "read_power": 18.531, "write_power": 16.201 },
                "offset": { "value": "0x342e0000", "magnitude":  "BYTES" },
                "size":   { "value": "448",        "magnitude": "KBYTES" }
            },
            {
                "fname": "AXISRAM6",
                "name":  "npuRAM6",
                "fformat": "FORMAT_RAW",
                "prop":   { "rights": "ACC_WRITE", "throughput": "HIGH", "latency": "LOW", "byteWidth": 8,
                            "freqRatio": 1.25, "read_power": 19.006, "write_power": 15.790 },
                "offset": { "value": "0x34350000", "magnitude":  "BYTES" },
                "size":   { "value": "448",        "magnitude": "KBYTES" }
            },
            {
                "fname": "xSPI1",
                "name":  "hyperRAM",
                "fformat": "FORMAT_RAW",
                "prop":   { "rights": "ACC_WRITE", "throughput": "MID", "latency": "HIGH", "byteWidth": 2,
                            "freqRatio": 5.00, "cacheable": "CACHEABLE_ON","read_power": 380, "write_power": 340.0,
                            "constants_preferred": "true" },
                "offset": { "value": "0x90000000", "magnitude":  "BYTES" },
                "size":   { "value": "32",         "magnitude": "MBYTES" }
            },
            {
                "fname": "xSPI2",
                "name":  "octoFlash",
                "fformat": "FORMAT_RAW",
                "prop":   { "rights": "ACC_READ",  "throughput": "MID", "latency": "HIGH", "byteWidth": 1,
                            "freqRatio": 6.00, "cacheable": "CACHEABLE_ON", "read_power": 110, "write_power": 400.0,
                            "constants_preferred": "true" },
                "offset": { "value": "0x70000000", "magnitude":  "BYTES" },
                "size":   { "value": "64",         "magnitude": "MBYTES" }
            }
        ]
    }
}

Note

In the descriptions for “AXIFLEXMEM” and “AXISRAM1”, the sizes for the memory regions mapped after 0x34000000 have been set to 0 bytes. This is done to signal the Neural-ART compiler not to use those memory pools when allocating buffers. The reason for this is that, in the full example, the embedded firmware is placed within this range (that is, the linker script places everything in the range 0x34000000 - 0x34100000)

Tip

It is mandatory that the memory ranges available for/used by the NPU compiler and the memory ranges available for the applicative firmware are disjoint. For example, if the firmware is stored somewhere and the NPU uses this location for storing activations, then the firmware is erased during inference.

Syntax description and main options

“mempools” key

This item contains a list that describes each of the memory regions.

Each memory region is described in an object. The keys of such objects are described below, with their main associated accepted values.

  • fname (string) File name to use for the memory initializer (the final name is also prefixed by mem_file_prefix)
  • name (string) Memory Name (found in reports)
  • fformat File format used for the memory initializer. Values can be among:
    • FORMAT_RAW Raw binary format
    • FORMAT_HEX Same as raw, but easier to read for humans: hexadecimal data representation of the contents. FORMAT_HEX16, FORMAT_HEX32 can also be used.
    • FORMAT_IHEX Intel-Hex file
  • offset Memory start address. The value is an object with the following key/values
    • value (string) Start address value. Either in decimal format (for example, 805306368) or hexadecimal format (for example, 0x30000000)
    • magnitude (string) Unit to interpret the value field. Can be a value among BYTES, KBYTES, MBYTES.
  • size Memory size. The value is an object with the following key/values
    • value (string) Size of the memory. Either in decimal format (for example, 805306368) or hexadecimal format (for example, 0x30000000)
    • magnitude (string) Unit to interpret the value field. Can be a value among BYTES, KBYTES, MBYTES.
  • mode Defines whether the pool address is to be absolute or relative. For now, use USEMODE_ABSOLUTE, relative mode is explained in other documents.
  • prop Defines multiple properties of the current pool, within an object. The keys/values of this object available for the object are as follows:
    • rights States if the memory is read-only or read-write: ACC_READ, ACC_WRITE
    • throughput Memory throughput description: LOW, MID or HIGH. The description here is relative to other pools (this is not an absolute value).
    • latency Memory latency description: LOW, MID or HIGH. The description here is relative to other pools (this is not an absolute value).
    • byte_width (uint32) Memory bus access width
    • freq_ratio (float) Memory frequency ratio compared to accelerators (that is, NPU frequency) – bigger values mean slower frequency.
      • Absolute values are used for estimations available in reports
      • Relative ratios between pools are important for the NPU compiler to take decisions (that is, if the reports are not used, it is not needed to change the values when changing the NPU frequency)
    • cacheable Is the pool cacheable? ON or OFF (default is OFF)
    • read_power (float) Read power for a single byte_width access in mW (power measured at nominal frequency and voltage) – used for reports
    • write_power (float) Active write power for a single byte_width access in mW (power measured at nominal frequency and voltage) – used for reports
    • constants_preferred (bool) Preferred memory pool for constant values (for example, weights). true or false (default: false)

“cacheinfo” key

This part describes the cache architecture.

The provided memory-pools files give a good representation of the cache used in STM32N6 (CACHEAXI), and should not be modified.

Virtual mem-pools considerations

The --enable-virtual-mem-pools allows the compiler to merge contiguous memory pool into a single, virtual pool.

In the example above, the pools cpuRAM2, npuRAM3-npuRAM6 are all contiguous (that is, the end of cpuRAM2 is the start of npuRAM3). When specifying --enable-virtual-mem-pools, the NPU compiler considers all those pools as a single one, and thus will, if needed to allocate buffers that span on multiple “concrete” pools.
This is, in a way, equivalent to create only one large entry in the memory pool file that would merge all the first memory pools.

Using --enable-virtual-mem-pools enables the user to conveniently use the same .mpool file to fit different models with different memory requirements.
This, however comes at the cost that if merged memory characteristics are very different, the resulting virtual pool inherits the worst characteristics of them, and thus it may result in suboptimal allocation of buffers. (When allocating buffers to the virtual memory pool, the underlying concrete pools characteristics are not considered.)

To overcome this issue, it might be useful to add holes (for example, 1 byte) between ranges of memory that have very different characteristics, this prevents the compiler from merging heterogenous pools.

ST Edge AI Core command line interface

The ST Edge AI core CLI is the recommended way for using the NPU compiler. It facilitates the application of specific transformations and generates the intermediate representation (ONNX + JSON files). The ‘--st-neural-art’ option allows specifying a compilation profiles json file containing different sets of options named “profiles” that are directly passed to the compiler.

NPU compiler as back-end

--st-neural-art STR

Argument syntax: empty or <profile>[@<compilation-profiles-file-path>]

Set a profile from a compilation profile file. This option is mandatory to enable the passes allowing to analyze/generate a model.

Argument Description
help Print the NPU compiler help.
<empty> Use a “default” profile.
profile-<tool_profile> Use a built-in tool profile (see next section).
<profilename>@<compilation-profiles-file-path> Use the custom profiles.

Tool built-in profiles

The tool package provides a typical compilation profile file including different settings which can be selected with the 'profile-' argument of the '--st-neural-art' option. It references the memory-pool descriptor files allowing to dedicate the major part of the internal memories and external memory devices to the NPU memory subsystem.

  • Location of the compilation profile file: $STEDGEAI_CORE_DIR/Utilities/windows/targets/stm32/resources/NPU/STM32N6xx/neural_art.json.
  • Memory-pool descriptor file: $STEDGEAI_CORE_DIR/Utilities/windows/targets/stm32/resources/NPU/STM32N6xx/stm32n6.mpool.
Profile name Description
minimal Mandatory options only. No optimization. All available memories can be used ('stm32n6.mpool' file)
default Extend the minimal profile enabling the optimization options to efficiently use the memory-pools
allmems--O3 Add optimization level 3 for speed + \-\-Oauto-sched option
allmems--auto Enable auto option
internal-memories-only--default default profile, but only the internal memories are allowed ('stm32n6__internal_memories_only.mpool' file)

Note

The provided profiles are the generic setting and should be customized according to the application constraints and the imported models.

--enable-epoch-controller

Enforce generation of epoch-controller blobs when using Neural-ART compiler.
This option only works in combination with --st-neural-art.

Using this option on the command-line is equivalent to adding this option in the compiler options of the profile to be used. This allows to (some very limited extent) augment the profiles used on-the-fly with an extra argument directly from the command-line interface.

Front-end options

The following options impact the generated files.

Option Description
--name overwrite the name of the files generated by the NPU compiler (and symbols within the .c file)
--no-inputs-allocation, --no-outputs-allocation inputs/outputs buffers will not be allocated by the NPU compiler in the provided memory pools and must be allocated/“linked” at runtime by the embedded application.
--input-data-type, --output-data-type used to change the type of data of the input/output tensors for the deployed model
--inputs-ch-position, --outputs-ch-position used to change the memory layout (NHWC vs NCHW) of the input/output tensors for the deployed model

Compilation Profiles JSON File

The following JSON snippet provides a typical compilation profiles json file. This is not strict JSON format. The comments are allowed and start with //.

{
    "Globals": {
    // This section is required but can be empty
    },
    "Profiles": {
        // Minimal options required for the generated file to work
        "minimal" : {
            "memory_pool": "./mpools/stm32n6.mpool",
            "options": "--native-float --cache-maintenance --Ocache-opt"
        },
        // Advised minimal options
        "default" : {
            "memory_pool": "./mpools/stm32n6.mpool",
            "options": "--native-float --cache-maintenance --Ocache-opt --enable-virtual-mem-pools --Os"
        },
        "test" : {
            "memory_pool": "./mpools/stm32n6.mpool",
            "options": "--native-float --cache-maintenance --Ocache-opt --enable-virtual-mem-pools --optimization 1"
        },
        "test2" : {
            "memory_pool": "./my_memory_pools/stm32n6_test.mpool",
            "options": "--native-float --cache-maintenance --Ocache-opt --enable-virtual-mem-pools\
                       --optimization 1 --Oauto-sched --enable-epoch-controller"
        }
    }
}

This file has two sections: "Globals" and "Profiles".

  • The "Globals" section is used for debug purposes. It is optional, and can be removed from the profile file.
  • The "Profiles" section allows defining multiple named profiles that are selectable through the '--st-neural-art' option of the ST Edge AI CLI.

A profile is a combination of:

  • A path to a memory-pool descriptor file (.mpool file).
  • A list of options to be passed to the NPU compiler.
  • Optional: A path to a machine description file (.mdesc file) - by default, the stm32n6 description file is used.

Tips, variations around the basic use case

Generic recommendations

  • When using small-enough models, try to refrain from using external memories: any transaction with external memory is time-consuming!
  • Remember that --enable-virtual-mem-pools, though convenient, may have massive disruptive effects on inference time.
    • When in optimization steps, try to remove this option from the compiler’s parameters.

NPU compiler options

  • Experiment with options, a lot of options can be added and may provide successful (or not) effects.
  • After a successful --Oauto compilation for a model, note down the “best” options used, and report them in the arguments of the compiler at next compilation, this will save compilation time during development.

Memory-pools

Warning

Always remember to have disjoint “memory spaces” available for the NPU compiler (that will allocate buffers and constants of the network) and the firmware compiler (that will allocate space for program, variables, etc.) to prevent memory issues.

  • Carving memory for performance-improvement of a model is a time-consuming activity.
    • Start with basic memory pools with e.g. virtual memory pools enabled.
    • Check if it seems possible to fit the whole model in internal memories.
      • If the firmware is small-enough, it is possible to evolve from the example mpool by adding space before the AXISRAM2 pool (do not forget to remove this memory space in the linker script)
    • When trying to optimize memory usage/allocation for speed, try to disjoint virtually-merged-pools (by adding small holes between them).
      • Ultimately, try not to use virtual-memory-pools.
  • For development purposes
    • An external RAM can be used easily instead of an external flash (for example, by setting the size of the external flash to 0 and adding constants_preferred=true to external ram characteristics) if both types of memories are available.
    • This prevents wear of the flash, will be quicker to load weights on the board, etc.
      • Be aware that this can make the inference faster (external RAM on discovery-kit board can use hexa-SPI vs. octo-SPI for external Flash)