FAQs - ST Neural ART NPU
ST Edge AI Core Technology 2.2.0
Generic
Is it possible to deploy a model exclusively on the ARM Cortex® M55 core of an STM32N6xx device?
YES - in this case the ‘–st-neural-art [profile@conf.json]’ option should be not used. The classical flow for a STM32xx target can be used.
Is it possible to use directly the ST Neural ART compiler?
YES - When the intermediate ONNX and associated JSON files are generated, it is possible to directly call the ST Neural ART compiler.