How to upgrade a STELLAR project
for STELLAR target, based on ST Edge AI Core Technology 2.2.0
r2.2
Overview
This article describes how to upgrade a Stellar Studio AI SDK (Stellar-E or Stellar-PG) based project with a new version of the ST Edge AI Core library. The update of generated c-model files is described in the “Update a stellar studio ai sdk based project” section. For the interface between them, backward or/and forward compatibility is never considered, if the generated c-model files are updated with a new version of the Stellar Studio AI tools, the Stellar Studio AI library files should be also aligned. Without specific notification/advice, at source level, no breaking change to the embedded inference API that can break the client’s application is expected.
Typical source tree (%ROOT_PRJ_DIR%
indicates the
root AI sub-directory created in the Stellar Studio AI project after
that a generation has been done):
Command to update the c-model files with the CLI:
--target stellar-e <my_model> <my_options> -o %ROOT_PRJ_DIR%/cfg/ $ stedgeai generate or--target stellar-pg <my_model> <my_options> -o %ROOT_PRJ_DIR%/cfg/ $ stedgeai generate
Manual update
The C-header files and network runtime libraries can be directly
copied from the ST Edge AI Core installation pack of Stellar Mcus
target.
[%STELLAR_AI_DIR%
] indicates the root location where
the ST Edge AI Core installation pack of Stellar Mcus target has
been installed.
directory | contains |
---|---|
%ROOT_PRJ_DIR%/lib/ai/inc |
all C-header files requested to build the generated c-model files |
%ROOT_PRJ_DIR%/lib/ai/Lib |
the network runtime libraries for all compilers toolchain supported |
tool-chain | contains |
---|---|
IAR | the library for the IAR ARM compiler - IAR ANSI C/C++ compiler V9.30.1.335/W64 tool-chain |
GCC | the library for the GNU ARM compiler - GNU Arm embedded 10.3-2021.10 toolchain |
HT | the library for the HighTec ARM compiler - HGHTEC clang version 8.1.0 toolchain |
ARMCLANG | the library for the ARMCLNG ARM compiler - embedded 6.21 tool-chain |
In each <tool-chain>
directory, this is one
sub-directory named StellarE or StellarPG_R52 or StellarPG_M4 with
the runtime libraries for each compiler supported.
Warning
When the project source tree is updated, don’t forget to update also the associated build system to use the new library files.
Upgrading the Stellar Studio AI library for the STELLAR-E device and GCC-based build system
# remove the previous files
rm %ROOT_PRJ_DIR%/lib/ai/inc/*.h
rm %ROOT_PRJ_DIR%/lib/ai/Lib/GCC/StellarE/*.a
# copy the new files
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Inc/* %ROOT_PRJ_DIR%/lib/ai/inc/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/GCC/StellarE/NetworkRuntime1020_CM7_GCC.a %ROOT_PRJ_DIR%/lib/ai/Lib/GCC/StellarE/
Upgrading the Stellar Studio AI libraries for the STELLAR P/G devices and GCC-based build system
# remove the previous files
rm %ROOT_PRJ_DIR%/lib/ai/inc/*.h
rm %ROOT_PRJ_DIR%/lib/ai/Lib/GCC/StellarPG_R52/*.a
rm %ROOT_PRJ_DIR%/lib/ai/Lib/GCC/StellarPG_M4/*.a
# copy the new files
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Inc/* %ROOT_PRJ_DIR%/lib/ai/inc/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/GCC/StellarPG_R52/NetworkRuntime1020_CR52_GCC.a %ROOT_PRJ_DIR%/lib/ai/Lib/GCC/StellarPG_R52/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/GCC/StellarPG_R52/NetworkRuntime1020_CR52_GCC_NEON.a %ROOT_PRJ_DIR%/lib/ai/Lib/GCC/StellarPG_R52/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/GCC/StellarPG_M4/NetworkRuntime1020_CM4_GCC.a %ROOT_PRJ_DIR%/lib/ai/Lib/GCC/StellarPG_M4/
Upgrading the Stellar Studio AI library for the STELLAR-E device and HIGHTEC-based build system
# remove the previous files
rm %ROOT_PRJ_DIR%/lib/ai/inc/*.h
rm %ROOT_PRJ_DIR%/lib/ai/Lib/HT/StellarE/*.a
# copy the new files
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Inc/* %ROOT_PRJ_DIR%/lib/ai/inc/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/HT/StellarE/NetworkRuntime1020_CM7_HT.a %ROOT_PRJ_DIR%/lib/ai/Lib/HT/StellarE/
Upgrading the Stellar Studio AI libraries for the STELLAR P/G devices and HIGHTEC-based build system
# remove the previous files
rm %ROOT_PRJ_DIR%/lib/ai/inc/*.h
rm %ROOT_PRJ_DIR%/lib/ai/Lib/HT/StellarPG_R52/*.a
rm %ROOT_PRJ_DIR%/lib/ai/Lib/HT/StellarPG_M4/*.a
# copy the new files
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Inc/* %ROOT_PRJ_DIR%/lib/ai/inc/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/HT/StellarPG_R52/NetworkRuntime1020_CR52_HT.a %ROOT_PRJ_DIR%/lib/ai/Lib/HT/StellarPG_R52/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/HT/StellarPG_R52/NetworkRuntime1020_CR52_HT_NEON.a %ROOT_PRJ_DIR%/lib/ai/Lib/HT/StellarPG_R52/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/HT/StellarPG_M4/NetworkRuntime1020_CM4_HT.a %ROOT_PRJ_DIR%/lib/ai/Lib/HT/StellarPG_M4/
Upgrading the Stellar Studio AI library for the STELLAR-E device and ARMCLANG-based build system
# remove the previous files
rm %ROOT_PRJ_DIR%/lib/ai/inc/*.h
rm %ROOT_PRJ_DIR%/lib/ai/Lib/ARMCLANG/StellarE/*.a
# copy the new files
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Inc/* %ROOT_PRJ_DIR%/lib/ai/inc/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/ARMCLANG/StellarE/NetworkRuntime1020_CM7_ARMCLANG.a %ROOT_PRJ_DIR%/lib/ai/Lib/ARMCLANG/StellarE/
Upgrading the Stellar Studio AI libraries for the STELLAR P/G devices and ARMCLANG-based build system
# remove the previous files
rm %ROOT_PRJ_DIR%/lib/ai/inc/*.h
rm %ROOT_PRJ_DIR%/lib/ai/Lib/ARMCLANG/StellarPG_R52/*.a
rm %ROOT_PRJ_DIR%/lib/ai/Lib/ARMCLANG/StellarPG_M4/*.a
# copy the new files
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Inc/* %ROOT_PRJ_DIR%/lib/ai/inc/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/ARMCLANG/StellarPG_R52/NetworkRuntime1020_CR52_ARMCLANG.a %ROOT_PRJ_DIR%/lib/ai/Lib/ARMCLANG/StellarPG_R52/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/ARMCLANG/StellarPG_R52/NetworkRuntime1020_CR52_ARMCLANG_NEON.a %ROOT_PRJ_DIR%/lib/ai/Lib/ARMCLANG/StellarPG_R52/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/ARMCLANG/StellarPG_M4/NetworkRuntime1020_CM4_ARMCLANG.a %ROOT_PRJ_DIR%/lib/ai/Lib/ARMCLANG/StellarPG_M4/
Upgrading the Stellar Studio AI library for the STELLAR-E device and IAR-based build system
# remove the previous files
rm %ROOT_PRJ_DIR%/lib/ai/inc/*.h
rm %ROOT_PRJ_DIR%/lib/ai/Lib/IAR/StellarE/*.a
# copy the new files
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Inc/* %ROOT_PRJ_DIR%/lib/ai/inc/
cp %STELLAR_AI_DIR%/Middlewares/ST/AI/Lib/IAR/StellarE/NetworkRuntime1020_CM7_IAR.a %ROOT_PRJ_DIR%/lib/ai/Lib/IAR/StellarE/