Deep Quantized Neural Network (DQNN) support
ST Edge AI Core Technology 4.1.0
r2.0
Overview
ST Edge AI Core can be used to deploy a pre-trained Deep Quantized Neural Network (DQNN) model designed and trained with the QKeras library when targeting STM32, STELLAR, and ISPU. The purpose of this article is to describe the supported configurations and limitations for deploying an efficient, optimized C-inference model on ST targets. For detailed explanations and recommendations on designing a DQNN model, see the corresponding user guide or notebook.
Deep Quantized Neural Network
Quantized models generally refer to models that use an 8-bit signed or unsigned integer data format to encode each weight and activation. After an optimization/quantization process (Post-Training Quantization, PTQ, or Quantization-Aware Training, QAT), this makes it possible to deploy a floating-point network using smaller integer arithmetic, improving computational resources. DQNN denotes models where bit width used in some weight and/or activation is smaller than 8 bits. Mixed data types (hybrid layers) can also be used for a given operator, for example, binary weights with 8-bit signed-integer or 32-bit floating-point activations. This allows a trade-off between accuracy, precision, and peak memory usage. To ensure performance, QKeras trains only in quantization-aware mode (QAT).
Each library is designed as an extension of the high-level (custom layer) Keras API that provides an easy way to create a deeply quantized version of an original Keras network. As shown in the left part of the following figure, based on the concept of quantized layers and quantizers, the user can transform a full-precision layer by describing how to quantize incoming and outgoing activations and weights. Note that the quantized layers are fully compatible with the Keras API so they can be used with Keras Layers interchangeably. This property allows the user to design the mixed models with layers which are kept in float.
After using a classical quantized model (8-bit format only), a DQNN model can be considered an advanced optimization approach for deploying a model in resource-constrained environments such as ST devices, without significant accuracy loss. It is considered advanced because designing this type of model is not a direct process.
1-bit and 8-bit signed-format support
Arm Cortex-M and ISPU instructions, together with the required data manipulations (such as packing and unpacking during memory transfers), do not allow an efficient implementation for every combination of data types. The ST Edge AI Core focuses primarily on implementations to improve memory peak usage (Flash and/or RAM) and reduce latency (execution time), which means that optimization for size is not supported. Therefore, only the 32b-float, 8-bit signed and binary signed (1-bit) data types are considered by the code generator when deploying optimized C kernels (see the next “Optimized C-kernels” section). Otherwise, if possible, a fallback to 32-bit floating point C kernel is used with quantization and dequantization operations before and after the operator.
- The data type of the input tensors is inferred from the data type of the previous operator.
- The data type of the output tensors is inferred from the downstream operator chain.
- In the case where the input/output and weight tensors are quantized with a classical 8-b integer scheme (like for the TFlite quantized models), the respective optimized int8 c-kernel implementations will be used.
QKeras library
QKeras is a
quantization extension framework developed by Google on top of
Keras. It provides drop-in replacements for selected Keras layers,
particularly computational layers such as convolution, dense, and
nonlinear layers. This allows developers to create deeply quantized
Keras networks quickly. QKeras extends Keras according to Keras
design principles: it is user-friendly, modular, and extensible
while remaining minimally intrusive to native Keras functionality.
It also provides the QTools and AutoQKeras
tools to help users deploy quantized models on specific hardware or
treat quantization as a hyperparameter in a Keras Tuner search.
import tensorflow as tf
import qkeras
...
x = tf.keras.Input(shape=(28, 28, 1))
y = qkeras.QActivation(qkeras.quantized_relu(bits=8, alpha=1))(x)
y = qkeras.QConv2D(16, (3, 3),
kernel_quantizer=qkeras.binary(alpha=1),
bias_quantizer=qkeras.binary(alpha=1),
use_bias=False,
name="conv2d_0")(y)
y = tf.keras.layers.MaxPooling2D(pool_size=(2,2))(y)
y = tf.keras.layers.BatchNormalization()(y)
y = qkeras.QActivation(qkeras.binary(alpha=1))(y)
...
model = tf.keras.Model(inputs=x, outputs=y)Supported QKeras quantizers/layers
QActivation
QBatchNormalization
QConv2D
QConv2DTranspose'padding'parameter should be'valid'
'stride'must be'(1, 1)'
QDense- Only 2D input shape is supported:
[batch_size, input_dim]. A rank greater than 2 is not supported,Flattenlayer before the QuantDense/QDense operator should be added
- Only 2D input shape is supported:
QDepthwiseConv2D
The following quantizers and associated configurations are supported:
| Quantizer | Comments and limitations |
|---|---|
quantized_bits() |
Only 8-bit quantization
(bits=8) is supported. |
quantized_relu() |
Only 8-bit quantization
(bits=8) is supported. |
quantized_tanh() |
Only 8-bit quantization
(bits=8) is supported. |
binary() |
Supported only in signed mode
(use_01=False) and without scaling
(alpha=1). |
stochastic_binary() |
Supported only in signed mode
(use_01=False) and without scaling
(alpha=1). |
Typically,
'quantized_relu()'quantizer can be used to quantize the inputs which are normalized between'0.0'and'1.0'. Note that'quantized_relu(bits=8, integer=8, keep_negative=False)'can be considered if the range of the input values are between'0.0'and'256.0'.x = tf.keras.Input(shape=(..)) y = qkeras.QActivation(qkeras.quantized_relu(bits=8, integer=0))(x) y = qkeras.QConv2D(..) ...The
'quantized_bits()'quantizer can also be used to quantize the inputs which are normalized between'-1.0'and'1.0'. Note that'quantized_bits(bits=8, integer=7)'can be considered if the range of the input values are between'-128.0'and'127.0'.x = tf.keras.Input(shape=(..)) y = qkeras.QActivation(qkeras.quantized_bits(bits=8, integer=0, symmetric=0, alpha=1))(x) y = qkeras.QConv2D(..) ...To have a fully binarized operation without bias and a normalized and binarized output:
... y = qkeras.QActivation(qkeras.binary(alpha=1))(y) y = qkeras.QConv2D(.. kernel_quantizer="binary(alpha=1)", bias_quantizer=qkeras.binary(alpha=1), use_bias=False, )(y) y = keras.MaxPooling2D(...)(y) y = keras.BatchNormalization()(y) y = qkeras.QActivation(qkeras.binary(alpha=1))(y) ...
Optimized C-kernel configurations
Implementation conventions
This section lists the optimized data-type combinations using the following naming convention:
f32identifies the absence of quantization (that is, 32-bit floating point).s8identifies 8-bit signed quantization.s1identifies binary signed quantization.
c-layout of the s1 type
Elements of binary activation tensors are packed into 32-bit
words along the last dimension ('axis=-1') according to
the following rules:
- Bit order: little-endian or most-significant bit first.
- Padding value:
'0b'. - Positive values are encoded as
'0b', while negative values are encoded as'1b'.
Note
The number of channels should preferably be a multiple of 32 to optimize Flash/RAM usage and MAC/cycle performance, but this is not required.
Quantized Dense layers
| input format | output format | weight format | bias format (1) | notes |
|---|---|---|---|---|
| s1 | s1 | s1 | s1 | (2) |
| s1 | s1 | s1 | f32 | (2) |
| s1 | s1 | s8 | s1 | (2) |
| s1 | s8 | s1 | s8 | (2) |
| s1 | s8 | s8 | s8 | (2) |
| s1 | f32 | s1 | s1 | (2) |
| s1 | f32 | s1 | f32 | (2) |
| s1 | f32 | s8 | s8 | (2) |
| s1 | f32 | f32 | f32 | (2) |
| s8 | s1 | s1 | s1 | (2) |
| s8 | s8 | s1 | s1 | (2) |
| s8 | f32 | s1 | s1 | (2) |
| s8 | s8 | s8 | s8 | (2), bias are stored as s32 format |
| s8 | s8 | s8 | s32 | (2), int8-tflite kernels |
| s8 | f32 | s1 | s1 | (2) |
| f32 | s1 | s1 | s1 | (2) |
| f32 | s1 | s1 | f32 | (2) |
| f32 | f32 | s1 | s1 | (2) |
| f32 | f32 | s1 | f32 | (2) |
(1) usage of the bias is optional
(2) batch-normalization can be fused
Optimized Convolution layers
| input format | output format | weight format | bias format (1) | notes |
|---|---|---|---|---|
| s1 | s1 | s1 | s1 | (2), (3), including pointwise and depthwise version |
| s1 | s8 | s1 | s8 | (2), including pointwise version |
| s1 | s8 | s1 | f32 | (2), including pointwise version |
| s1 | f32 | s1 | f32 | (2), including pointwise version |
| s8 | s1 | s8 | ||
| s8 (Dorefa) | s1 | s8 (Dorefa) | (2), use_bias=False | |
| s8 | s8 | s8 | s8 | (2) bias are stored as s32 format |
| s8 | s8 | s8 | s32 | (2) int8-tflite kernels |
(1) usage of the bias is optional
(2) batch-normalization can be fused
(3) maxpool can be inserted between the convolution and the
batch-normalization operators
Misc layers
The following layers are also available to support more complex topologies, such as networks with residual connections.
| input format | input format | output format | notes |
|---|---|---|---|
| maxpool | s1 | s1 | s8/f32 data type is also supported by the “standard” C-kernels |
| concat | s1 | s1 | s8/f32 data type is also supported by the “standard” C-kernels |
Evidence of efficient code generation
Similar to the 'qkeras.print_qstats()' function, the
“analyze”
command reports the number of operations used by each generated C
layer according to its data type. It also reports the operation
counts for the entire generated C-model, making it possible to
determine whether the deployed model is fully or partially based on
optimized binary or quantized C kernels.
Note
For the size of the deployed weights, the 'ROM'/'weights (ro)'
metric indicates the expected size for storing the
quantized weights on the target. The reported value is
compared with the size required to store the weights in the original
format (32-bit floating point). Detailed information for each C
layer and its associated tensors is available in the generated
reports.
Following example shows that 90% of the operations are the binary
operations provided by the main contributor:
"quant_conv2d_1_conv2d" layer.
$ stedgeai -m <model_file.h5> --target stm32
...
params # : 93,556 items (365.45 KiB)
macc : 2,865,718
weights (ro) : 14,496 B (14.16 KiB) (1 segment) / -359,728(-96.1%) vs float model
activations (rw) : 86,528 B (84.50 KiB) (1 segment)
ram (total) : 89,704 B (87.60 KiB) = 86,528 + 3,136 + 40
...
Number of operations and param per c-layer
-------------------------------------------------------------------------------------------
c_id m_id name (type) #op (type)
-------------------------------------------------------------------------------------------
0 2 quant_conv2d_conv2d (conv2d) 194,720 (smul_f32_f32)
1 3 quant_conv2d_1_conv (conv) 43,264 (conv_f32_s1)
2 1 max_pooling2d (pool) 21,632 (op_s1_s1)
3 3 quant_conv2d_1_conv2d (conv2d_dqnn) 2,230,272 (sxor_s1_s1)
4 5 max_pooling2d_1 (pool) 6,400 (op_s1_s1)
5 7 quant_conv2d_2_conv2d (conv2d_dqnn) 331,776 (sxor_s1_s1)
6 10 quant_dense_quantdense (dense_dqnn_dqnn) 36,864 (sxor_s1_s1)
7 13 quant_dense_1_quantdense (dense_dqnn_dqnn) 640 (sxor_s1_s1)
8 15 activation (nl) 150 (op_f32_f32)
-------------------------------------------------------------------------------------------
total 2,865,718
Number of operation types
---------------------------------------------
smul_f32_f32 194,720 6.8%
conv_f32_s1 43,264 1.5%
op_s1_s1 28,032 1.0%
sxor_s1_s1 2,599,552 90.7%
op_f32_f32 150 0.0%
Example of supported patterns
As already mentioned in the overview, the ST Edge AI Core infers the data-type of the input and output tensors from the data-type of the incoming and outcome chains respectively. This section illustrates the typical patterns which are considered to deploy an optimized c-kernel.
Activation layer
Activation layer (including the QActivation layer)
is mainly supported by fusing it in the previous or following layer.
Supported arguments are the supported quantizer configurations.
x = tf.keras.Input(shape=(..))
y = qkeras.QActivation(qkeras.binary(alpha=1))(x)
y = qkeras.QConv2D(..)(y)
...Quantized dense layer
Dense layer patterns are a sequence of layers composed of:
- an optional
QActivationto specify the input format. If missing the input format is f32
- the
QDenselayer, use of bias is optional
- an optional other layer:
e.g.
(Q)BatchNormalizationwhich can be merged info the previous dense layer
- an optional
QActivationto specify the output format. If missing the output format is f32
The first example illustrates the case where 8-b quantized input
(s8: symmetric with 7-bit fractional part) is used for
the QDense layer exploiting 1-b quantized (or binary)
weights with bias. The output is normalized and in f32.
import qkeras
import tensorflow as tf
shape_in = (128, 128)
x = tf.keras.Input(shape=shape_in)
y = qkeras.QActivation(qkeras.quantized_bits(bits=8, integer=7))(x)
y = tf.keras.layers.Flatten()(y)
y = qkeras.QDense(16,
kernel_quantizer=qkeras.binary(alpha=1),
bias_quantizer=qkeras.binary(alpha=1),
use_bias=True,
name="dense_0")(y)
y = tf.keras.layers.BatchNormalization()(y)
y = tf.keras.layers.Activation("softmax")(y)
model = tf.keras.Model(inputs=x, outputs=y)
Number of operations per c-layer
------- ------ --------------------------- --------- ------------
c_id m_id name (type) #op type
------- ------ --------------------------- --------- ------------
0 3 dense_0 (Dense) 262,144 smul_s8_s1
1 5 activation (Nonlinearity) 240 op_f32_f32
------- ------ --------------------------- --------- ------------
total 262,384
Number of operation types
---------------- --------- -----------
operation type # %
---------------- --------- -----------
smul_s8_s1 262,144 99.9%
op_f32_f32 240 0.1%
Second example shows the case, where two dense layers are used. The
first uses the binary weights with a 8-b quantized input to compute
the binary output. Second layer uses the binary weights and the
previous binary output to compute the f32 output.
x = tf.keras.Input(shape=shape_in)
y = tf.keras.layers.Flatten()(x)
y = qkeras.QActivation(qkeras.quantized_bits(bits=8, integer=7))(y)
y = qkeras.QDense(64,
kernel_quantizer=qkeras.binary(alpha=1),
bias_quantizer=qkeras.binary(alpha=1),
use_bias=True,
name="dense_0")(y)
y = tf.keras.layers.BatchNormalization()(y)
y = qkeras.QActivation(qkeras.binary(alpha=1))(y)
y = qkeras.QDense(10,
kernel_quantizer=qkeras.binary(alpha=1),
bias_quantizer=qkeras.binary(alpha=1),
use_bias=True,
name="dense_1")(y)
y = tf.keras.layers.Activation("softmax")(y) Number of operations and param per c-layer
-------------------------------------------------------------------------------
c_id m_id name (type) #op (type)
-------------------------------------------------------------------------------
0 3 dense_0_qdense (dense_dqnn_dqnn) 50,176 (smul_s8_s1)
1 6 dense_1_qdense (dense_dqnn_dqnn) 650 (sxor_s1_s1)
2 7 activation (nl) 150 (op_f32_f32)
-------------------------------------------------------------------------------
total 50,976
Number of operation types
---------------------------------------------
smul_s8_s1 50,176 98.4%
sxor_s1_s1 650 1.3%
op_f32_f32 150 0.3%Quantized Convolution layer
For the quantized convolution layer, the pattern is similar to the quantized dense layer.
Following example shows the case where the binary input/weight
are used to compute a normalized binary output.
MaxPooling2D layer allows to compact the
activations.
x = tf.keras.Input(shape=shape_in)
y = qkeras.QActivation(qkeras.binary(alpha=1))(x)
y = qkeras.QConv2D(filters=16, kernel_size=(3, 3),
kernel_quantizer=qkeras.binary(alpha=1),
bias_quantizer=qkeras.binary(alpha=1),
use_bias=False,
padding="same",
name="dense_0")(y)
y = tf.keras.layers.MaxPooling2D(pool_size=(2, 2))(y)
y = tf.keras.layers.BatchNormalization()(y)
y = qkeras.QActivation(qkeras.binary(alpha=1))(y)
model = tf.keras.Model(inputs=x, outputs=y)
Variation with 'stride' argument can be used to avoid
to use the MaxPooling2D layer.
x = tf.keras.Input(shape=shape_in)
y = qkeras.QActivation(qkeras.binary(alpha=1))(x)
y = qkeras.QConv2D(filters=16, kernel_size=(3, 3),
kernel_quantizer=qkeras.binary(alpha=1),
bias_quantizer=qkeras.binary(alpha=1),
use_bias=False,
strides=(2, 2),
padding="same",
name="dense_0")(y)
y = tf.keras.layers.BatchNormalization()(y)
y = qkeras.QActivation(qkeras.binary(alpha=1))(y)
model = tf.keras.Model(inputs=x, outputs=y) Residual connections case
The following model shows how residual connections can be created to concatenate the activations. Particular attention shall be given to the shapes to be concatenated since must be the same with the exception of the size along the concatenation axis.
...
Number of operations and param per c-layer
--------------------------------------------------------------------------------------------
c_id m_id name (type) #op (type)
--------------------------------------------------------------------------------------------
0 1 quant_conv2d_5_conv2d (conv2d_dqnn) 819,200 (sxor_s1_s1)
1 2 max_pooling2d (pool) 12,800 (op_s1_s1)
2 4 quant_depthwise_conv2d_2_conv2d (conv2d_dqnn) 28,800 (sxor_s1_s1)
3 6 concatenate_2 (concat) 0 (op_s1_s1)
--------------------------------------------------------------------------------------------
total 860,800
Number of operation types
---------------------------------------------
sxor_s1_s1 848,000 98.5%
op_s1_s1 12,800 1.5%
...Fallback to 32b floating point kernels
Following code shows the case where the requested configuration:
's8xs1->s8' is not supported and the fallback is
applied. This is a typical case where the user has the opportunity
to modify its model (after a pre-analyze step of the model), to
keep this layer in float limiting the possible loss of
precision.
x = tf.keras.Input(shape=shape_in)
y = qkeras.QActivation(qkeras.quantized_bits(bits=8, integer=7))(x)
y = qkeras.QConv2D(filters=16, kernel_size=(3, 3), strides=(2, 2),
kernel_quantizer=qkeras.binary(alpha=1),
bias_quantizer=qkeras.binary(alpha=1),
use_bias=True,
padding="same",
name="dense_0")(y)
y = tf.keras.layers.BatchNormalization()(y)
y = qkeras.QActivation(qkeras.quantized_bits(bits=8, integer=7))(y)
model = tf.keras.Model(inputs=x, outputs=y) Number of operations and param per c-layer
----------------------------------------------------------------------------
c_id m_id name (type) #op (type)
----------------------------------------------------------------------------
0 0 input_1_0_conversion (conv) 1,568 (conv_s8_f32)
1 3 dense_0_conv2d (conv2d) 28,240 (smul_f32_f32)
2 4 q_activation_1 (conv) 6,272 (conv_f32_s8)
----------------------------------------------------------------------------
total 36,080
Number of operation types
---------------------------------------------
conv_s8_f32 1,568 4.3%
smul_f32_f32 28,240 78.3%
conv_f32_s8 6,272 17.4%Building an efficient DQNN/BNN model for ST Edge AI Core
All highlighted recommendations from the QKeras notebooks (https://github.com/google/qkeras/blob/master/notebook/QKerasTutorial.ipynb or https://notebook.community/google/qkeras/notebook/QKerasTutorial) should be considered to design an efficient DQNN/BNN model for ST series. In particular:
- It is preferable to leave the first layer and the last layer in
higher precision:
's8'or'f32'
- Usage of the
'BatchNormailzation'layer
- Placement of the
'MaxPool'layer before the'BatchNormailzation'
- Due to the way to encode the binary tensors (see “c-layout of the s1 type” section), it is recommended to have the number of channels as a multiple of 32 to optimize Flash/RAM size, and MAC/Cycle, but it is not a must have.
Pre-analyze step
It is recommended to execute regurlarly the “analyze” during the design of the DQNN/BNN model to know if it will be efficiently deployed (fallback not used) before to perform a complete training. This will avoid to use a quantized layer not supported or without gain in term of memory usage when it will deploy on a ST target.
FAQ
Is it possible to mix the quantized QKeras layers?
From the ST Edge AI Core point of view, yes, when importing the model, it is translated into an independent internal representation before applying the different optimization passes and the rendering stage. However, this is not recommended, even though each library (QKeras) is based on the Keras API, they are designed independently. There is no guarantee to converge with a good level of precision during the training phase.